Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Help. I need the reverse of zero crossing
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 4 answers
  • Subscribers 415 subscribers
  • Views 1865 views
  • Users 0 members are here
  • inrush
  • programing
  • arduino
Related

Help. I need the reverse of zero crossing

phoenixcomm
phoenixcomm over 8 years ago

Ok, I need some hunk of code to detect the peek not the zero crossing. ( this is the solution).

Problem: Toroid based power supply have inrush current problems. As when you turn on the power switch,

it is a random chance where on the sine wave it will be.

You can not start this a zero crossing as that is the Imax and will blow your fuse. image

This solution must be only a primary side problem. I was thinking of a relay but a small triac is much faster.

Thanks

Cris

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago +3 suggested
    Why do you need code - the simplest trick is to use an NTC current limiter. These people have a lovely web site: https://www.ametherm.com/ If you have to do it in code it might be easier to detect zero…
  • abrain
    abrain over 7 years ago in reply to phoenixcomm +3 verified
    Yes, sorry Cris, I don’t think I explained it very well. If you’re measuring the voltage (which I think you must be to find the zero crossing) then work out how much that voltage changed from the last…
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to michaelkellett +1 suggested
    I have seen current limiters like Ametherms before. But the problem is that I have three toroidal power transformers, and for the first 20ms or so they draw I max so the idea is to turn them on one at…
Parents
  • abrain
    0 abrain over 7 years ago

    Hi Cris, don't these things always turn out more interesting than you expect when you have a look at them?!

     

    Here's what I've come up with....

     

    My idea was basically to sample the voltage quite quickly (I think you're looking at 60Hz mains), so we get a good number of readings, and work out the difference between the latest reading and the previous one, effectively differentiating the signal. For a sine wave inout, that would give us something like the samples in the graph below (assuming you've got your input scaled nicely in the middle of the Arduino's 5V range).

     

    image

    From the orange dots showing the delta, you can then see that you're effectively after the zero crossing of the delta signal to get at the peak.

     

    When I came to try it, I got quite a lot of noisy triggering when there was no signal there, so I've added an extra check to make sure the ADC reading is above 800 before triggering, which is about a 3.9V input signal.

     

    The (moderately) interesting bit is that to get some good sampling, I set up an interrupt routine using Timer1, so we've got 2kHz sampling out of an Arduino! It's based on some other code I found on a forum some time ago, hopefully it'll be of use!

     

    // Interrupt-driven ADC sampling from Jack Christensen 13 Jun 2013
    // http://forum.arduino.cc/index.php?topic=171226.msg1276869#msg1276869
    
    
    #define BAUD_RATE 9600
    #define ADC_THRESHOLD 800      // if the actual voltage isn't above this, don't trigger
    
    
    int timerCount = 0;            // use to flash the LED at a sensible 2Hz rate
    volatile int oldAdcVal;        // keep the last reading so we can calculate a delta
    volatile int lastDelta;        // keep the old delta, so we can look for a zero crossing in that
    boolean justPeaked = false;    // flag to our main loop when we've just reached a peak
    
    
    void setup(void)
    {
        delay(1000);
        Serial.begin(BAUD_RATE);
        Serial.println("Setup...");
    
    
        //set up the timer
        TCCR1B = 0;                //stop the timer
        TCCR1A = 0;
        TIFR1 = 0xFF;              //ensure all interrupt flags are cleared
        OCR1A = 999;               //timer runs at 16MHz / 1000 / 8 (prescaler) = 2000Hz (500us between samples)
        OCR1B = 999;
        cli();
        TCNT1 = 0;                 //clear the timer
        TIMSK1 = _BV(OCIE1B);      //enable timer interrupts
        sei();
        TCCR1B = _BV(WGM12) | _BV(CS11);    //start the timer, ctc mode, prescaler 8
    
    
        //set up the adc
        ADMUX = _BV(REFS0);                                //use AVcc as reference
        ADCSRA  = _BV(ADEN)  | _BV(ADATE) | _BV(ADIE);     //enable ADC, auto trigger, interrupt when conversion complete
        ADCSRA |= _BV(ADPS2) | _BV(ADPS1) | _BV(ADPS0);    //ADC prescaler: divide by 128
        ADCSRB = _BV(ADTS2) | _BV(ADTS0);                  //trigger ADC on Timer/Counter1 Compare Match B
    
    
        pinMode(LED_BUILTIN, OUTPUT);
        Serial.println("Ready to go...");
    }
    
    
    void loop(void)
    {
      if ( justPeaked ) {
        Serial.println(micros());
        Serial.flush();
        justPeaked = false;
      }
    }
    
    
    ISR(ADC_vect)
    {
      int newAdcVal = ADC;
      int newDelta = newAdcVal - oldAdcVal;
      oldAdcVal = newAdcVal;  // save the new reading to use in the next delta sum
    
    
      // we make sure our actual reading is above a threshold to prevent
      // a lot of triggering from small signal noise
      if ( newAdcVal > ADC_THRESHOLD ) {
        // if we've had a zero crossing in our delta value,
        // we've just reached the peak of the waveform
        if ( ( lastDelta > 0 ) && ( newDelta < 0 ) ) {
          justPeaked = true;
        }
      }
      
      lastDelta = newDelta; // save the new delta value for next time
    }
    
    
    ISR(TIMER1_COMPB_vect)
    {
      // this is simply to toggle the LED, the triggering of the
      // ADC happens automatically
      timerCount++;
      if ( timerCount == 500 ) {
        digitalWrite(LED_BUILTIN, HIGH);
      }
      if ( timerCount == 1000 ) {
        digitalWrite(LED_BUILTIN, LOW);
        timerCount = 0;
      }
    }

     

    I hooked this up to my Arduino Micro, with the signal generator connected between pins GND and A5, with a 3Vpk-pk sine wave signal and 2.5Vdc offset, at 60Hz.

     

    So there you go - hopefully you can replace that serial output part in the loop() function with what you need to drive your relays, and you're done!

     

    A

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • abrain
    0 abrain over 7 years ago

    Hi Cris, don't these things always turn out more interesting than you expect when you have a look at them?!

     

    Here's what I've come up with....

     

    My idea was basically to sample the voltage quite quickly (I think you're looking at 60Hz mains), so we get a good number of readings, and work out the difference between the latest reading and the previous one, effectively differentiating the signal. For a sine wave inout, that would give us something like the samples in the graph below (assuming you've got your input scaled nicely in the middle of the Arduino's 5V range).

     

    image

    From the orange dots showing the delta, you can then see that you're effectively after the zero crossing of the delta signal to get at the peak.

     

    When I came to try it, I got quite a lot of noisy triggering when there was no signal there, so I've added an extra check to make sure the ADC reading is above 800 before triggering, which is about a 3.9V input signal.

     

    The (moderately) interesting bit is that to get some good sampling, I set up an interrupt routine using Timer1, so we've got 2kHz sampling out of an Arduino! It's based on some other code I found on a forum some time ago, hopefully it'll be of use!

     

    // Interrupt-driven ADC sampling from Jack Christensen 13 Jun 2013
    // http://forum.arduino.cc/index.php?topic=171226.msg1276869#msg1276869
    
    
    #define BAUD_RATE 9600
    #define ADC_THRESHOLD 800      // if the actual voltage isn't above this, don't trigger
    
    
    int timerCount = 0;            // use to flash the LED at a sensible 2Hz rate
    volatile int oldAdcVal;        // keep the last reading so we can calculate a delta
    volatile int lastDelta;        // keep the old delta, so we can look for a zero crossing in that
    boolean justPeaked = false;    // flag to our main loop when we've just reached a peak
    
    
    void setup(void)
    {
        delay(1000);
        Serial.begin(BAUD_RATE);
        Serial.println("Setup...");
    
    
        //set up the timer
        TCCR1B = 0;                //stop the timer
        TCCR1A = 0;
        TIFR1 = 0xFF;              //ensure all interrupt flags are cleared
        OCR1A = 999;               //timer runs at 16MHz / 1000 / 8 (prescaler) = 2000Hz (500us between samples)
        OCR1B = 999;
        cli();
        TCNT1 = 0;                 //clear the timer
        TIMSK1 = _BV(OCIE1B);      //enable timer interrupts
        sei();
        TCCR1B = _BV(WGM12) | _BV(CS11);    //start the timer, ctc mode, prescaler 8
    
    
        //set up the adc
        ADMUX = _BV(REFS0);                                //use AVcc as reference
        ADCSRA  = _BV(ADEN)  | _BV(ADATE) | _BV(ADIE);     //enable ADC, auto trigger, interrupt when conversion complete
        ADCSRA |= _BV(ADPS2) | _BV(ADPS1) | _BV(ADPS0);    //ADC prescaler: divide by 128
        ADCSRB = _BV(ADTS2) | _BV(ADTS0);                  //trigger ADC on Timer/Counter1 Compare Match B
    
    
        pinMode(LED_BUILTIN, OUTPUT);
        Serial.println("Ready to go...");
    }
    
    
    void loop(void)
    {
      if ( justPeaked ) {
        Serial.println(micros());
        Serial.flush();
        justPeaked = false;
      }
    }
    
    
    ISR(ADC_vect)
    {
      int newAdcVal = ADC;
      int newDelta = newAdcVal - oldAdcVal;
      oldAdcVal = newAdcVal;  // save the new reading to use in the next delta sum
    
    
      // we make sure our actual reading is above a threshold to prevent
      // a lot of triggering from small signal noise
      if ( newAdcVal > ADC_THRESHOLD ) {
        // if we've had a zero crossing in our delta value,
        // we've just reached the peak of the waveform
        if ( ( lastDelta > 0 ) && ( newDelta < 0 ) ) {
          justPeaked = true;
        }
      }
      
      lastDelta = newDelta; // save the new delta value for next time
    }
    
    
    ISR(TIMER1_COMPB_vect)
    {
      // this is simply to toggle the LED, the triggering of the
      // ADC happens automatically
      timerCount++;
      if ( timerCount == 500 ) {
        digitalWrite(LED_BUILTIN, HIGH);
      }
      if ( timerCount == 1000 ) {
        digitalWrite(LED_BUILTIN, LOW);
        timerCount = 0;
      }
    }

     

    I hooked this up to my Arduino Micro, with the signal generator connected between pins GND and A5, with a 3Vpk-pk sine wave signal and 2.5Vdc offset, at 60Hz.

     

    So there you go - hopefully you can replace that serial output part in the loop() function with what you need to drive your relays, and you're done!

     

    A

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer