Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Circuit Helpp!!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 6 answers
  • Subscribers 419 subscribers
  • Views 1872 views
  • Users 0 members are here
Related

Circuit Helpp!!

the_future
the_future over 7 years ago

image

 

 

need help with this please making it have no idea

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago +3 suggested
    Hi there, You've two similar posts asking for help, although with different parts of what I assume is the same project. Could you please explain a little about what you think the circuits need to achieve…
  • Dudley
    Dudley over 7 years ago in reply to 14rhb +3 suggested
    I've fixed it, thanks for letting me know
  • dougw
    dougw over 7 years ago +1 suggested
    Dudley I can't see the image at all....
Parents
  • 14rhb
    0 14rhb over 7 years ago

    Hi there,

     

    You've two similar posts asking for help, although with different parts of what I assume is the same project. Could you please explain a little about what you think the circuits need to achieve, what is its purpose of the project and where you got the drawings from (e.g. an engineer scribbled them down for you or they came from a book)? It would also be useful to know a bit about your background so any help offered can be set at the right level of understanding. Looking forward to your reply.

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • the_future
    0 the_future over 7 years ago in reply to 14rhb

    Sorry my bad I am trying to cultivate my robotic engineering skills soo....

    the circuits are two different parts for the same robot but currently separated for prototyping

     

     

     

    part 1 (is a force sensor interface with signal conditioning for a robot hand):

    image

    instrumentation amp of IN126, Low pass filter (20Hz) for noise, comparators (using LM324) for force levels 0, 20%, 40%, 60% and 80%.

     

     

    part 2 (is a "sound wake-up robot"; creating a module to activate a robot from sleep-mode for power saving via a sound ‘trigger’. ):

     

    image

    powered by 12v battery......

     

    1. The sound trigger will switch on other parts of the robot circuits, which consumes a maximum of 2A continuously current.
    2. The sound trigger shall be of the level of a normal human speaking voice at a distance of 1 metre. It will be desirable to arrange to reject frequencies outside of those intended for operation.
    3. Once activated by the sound trigger, the robot shall be maintained in active mode for a pre-set period. The pre-set period shall be ‘factory selectable’ to a period of either 30 seconds or 60 seconds so that the robot will go to sleep mode again when there is no sound within the period. For testing, it would be advantageous to also select a time period of 2 seconds.

     

    just have no idea of what an exact circuit would look like for both parts

     

    sorry still new to all this......

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • the_future
    0 the_future over 7 years ago in reply to 14rhb

    Sorry my bad I am trying to cultivate my robotic engineering skills soo....

    the circuits are two different parts for the same robot but currently separated for prototyping

     

     

     

    part 1 (is a force sensor interface with signal conditioning for a robot hand):

    image

    instrumentation amp of IN126, Low pass filter (20Hz) for noise, comparators (using LM324) for force levels 0, 20%, 40%, 60% and 80%.

     

     

    part 2 (is a "sound wake-up robot"; creating a module to activate a robot from sleep-mode for power saving via a sound ‘trigger’. ):

     

    image

    powered by 12v battery......

     

    1. The sound trigger will switch on other parts of the robot circuits, which consumes a maximum of 2A continuously current.
    2. The sound trigger shall be of the level of a normal human speaking voice at a distance of 1 metre. It will be desirable to arrange to reject frequencies outside of those intended for operation.
    3. Once activated by the sound trigger, the robot shall be maintained in active mode for a pre-set period. The pre-set period shall be ‘factory selectable’ to a period of either 30 seconds or 60 seconds so that the robot will go to sleep mode again when there is no sound within the period. For testing, it would be advantageous to also select a time period of 2 seconds.

     

    just have no idea of what an exact circuit would look like for both parts

     

    sorry still new to all this......

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer