Arduino Forum Arduino Uno Rev 3 + MIT App Inventor + Bluetooth Module HC05 + Door Magnetic Switch
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
  • State Verified Answer
  • Replies 27 replies
  • Answers 22 answers
  • Subscribers 402 subscribers
  • Views 5032 views
  • Users 0 members are here
Related

Arduino Uno Rev 3 + MIT App Inventor + Bluetooth Module HC05 + Door Magnetic Switch

kikovader
kikovader over 6 years ago

Hello, so this is my first time learning on how to use a Microcontroller like Arduino Uno and currently, I am planning to do on some mini project which uses these items below:

1. Arduino Uno Rev 3

2. Bluetooth Module HC-05

3. An App to receive the data which I created using MIT App Inventor

4. Door Magnetic Switch.

 

 

To be very honest I do not know where to start but I have already designed the User Interface of the Application without the Programming Block. I want it to work in away, when the Door Magnetic Switch formed closed circuit, it will send 1 or "ON" in the App through the Arduino Uno. However, when the Door Magnetic Switch formed an open circuit, it will send "0" of "OFF" in the App.

 

Is this possible?

Please help me. I am begging you. Please imageimage


  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 6 years ago in reply to kikovader +4 suggested
    Looking at your Arduino code, I can see that you are intending to connect the HC-05 Bluetooth module directly to the hardware Rx and Tx of the Arduino. Whilst this will work, it can be unreliable. It's…
  • neilk
    neilk over 6 years ago in reply to kikovader +4 verified
    Hi Kim Here is a slightly modified version of your Arduino Sketch: //Define the pins being used. //Connect the Door Magnetic Switch or Sensor to pin 4. // int ledOpen=2; int ledClose=3; int switchReed…
  • neilk
    neilk over 6 years ago in reply to kikovader +4 suggested
    You are welcome, Kim. Very pleased that it worked for you . You can't change the colour of the text you send from the Arduino to the App. You can, however, change the colour of the text displayed in the…
Parents
  • phoenixcomm
    0 phoenixcomm over 6 years ago

    Yes but No,

    Question: How are you determining the door to be "opened" or "closed"?

    Answer: You need a door switch normally they are a mico switch activated by a magnet!

     

    and btw you can get date and time from a public time server (very easy to build one) NTP or Network Time Protocol

    if you use timestamp then this will involve some network access and the network (Ethernet Shield)

    do {

        if ( door == open ) {

            # maybe send msg door was opened @ time

            do {

                 } while( door == closed );

                   #maybe send msg door was closed @ time

            }

       else;  # fall through

    }while ( something = 0 );

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • phoenixcomm
    0 phoenixcomm over 6 years ago

    Yes but No,

    Question: How are you determining the door to be "opened" or "closed"?

    Answer: You need a door switch normally they are a mico switch activated by a magnet!

     

    and btw you can get date and time from a public time server (very easy to build one) NTP or Network Time Protocol

    if you use timestamp then this will involve some network access and the network (Ethernet Shield)

    do {

        if ( door == open ) {

            # maybe send msg door was opened @ time

            do {

                 } while( door == closed );

                   #maybe send msg door was closed @ time

            }

       else;  # fall through

    }while ( something = 0 );

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer