Arduino
  • Products
  • More
Arduino
Arduino Forum Some questions on how to wire relays
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 605 views
  • Users 0 members are here
  • transistor
  • lighting
  • diy
  • value
  • electrical
  • arduino
  • relay
Related

Some questions on how to wire relays

e14 Contributor
e14 Contributor over 15 years ago

So right now I'm working on a project where I have 3 rope lights that run on wall power and I want to control them individually with my arduino.

 

The problem I am having is I am not sure what value relay and/or transistor I should use to control it, or how to wire the circuit.

 

Any suggestions?

  • Sign in to reply
  • Cancel
  • R_Phoenix
    0 R_Phoenix over 15 years ago

    First you will need to know the amp draw of the rope light. See if you can find a rating for it, maybe in "amps per foot". If not, you should be able to messure the amp draw with a meter. BUt if it is 110volt I would suspect it's only an Amp or 2 at the most (depending how long it is).

     

    this should work;

    http://www.robotshop.com/seeedstudio-arduino-relay-shield.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fileark
    0 fileark over 15 years ago

    The Arduino is only supposed to supply about 40 milliamps on each pin so the relay you pick would have to be very small to be powered completely from the Arduino. Be sure to use diodes reversed on the relay coils to adsorb harmful spikes generated by the relay coils. I have burned up a few IC chips thinking that the diode was optional, it is not.

     

    Here is a transistor that should work, the 2N2222 is a general purpose PNP transistor

     

    http://www.newark.com/multicomp/2n2222/bipolar-transistor-npn-30v-to-18/dp/87K2254

     

    Here is a schematic I did for my door entry control, it is being ran with a 555 timer chip but you can easily see how to wire the transistor to the relay and the diode.

    http://filear.com/dnn/Portals/0/Users/001/01/RFIDKeylessEntrySchematic.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Do you just want to switch them on and off, or do you want to vary the power and change the brilliance?

    Either way, you really need to do this using Triacs, which can be switched, or controlled from a PIC/Arduino chip, via some form of electrical isolation. There are plenty of circuits on the web to find using Google, search on Triac.

    REMEMBER Mains voltages are dangerous. A special circuit breaker (ELCB or similar) in your house on the wall circuits you will be using can protect you from dangerous shocks, though it still hurts! I know, done that!!

    regards

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • terryking
    0 terryking over 15 years ago in reply to e14 Contributor

    Hi,

     

    A lot of How-To about controlling Relays and Power with Arduino is here:  http://arduino-info.wikispaces.com/ArduinoPower 

     

    There are now low-cost relay boards with 1,2,4,or 8 relays that Arduino drives quickly and easily.

     

    You can see some here: http://goo.gl/8ZEQ8  (Disclaimer: Mentioning my own shop! But you can find them on Ebay too)

     

    Regards, Terry King

    ...In The Woods In Vermont

    terry@yourduino.com