Arduino
  • Products
  • More
Arduino
Arduino Forum Programing issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 3 answers
  • Subscribers 420 subscribers
  • Views 4896 views
  • Users 0 members are here
  • programing
  • arduino
Related

Programing issue

dirtdiver
dirtdiver over 14 years ago

Hi,

so I have a dc motor and a servo each controlled with a different potentiometer.First I made two separate codes and all works fine, but when I combine the two codes the servo starts getting readings from both pots.Here are the working codes

 

int motorPin = 9;                                          

int potpin = 0;

int val;   

 

void setup()

{

  pinMode(potpin,INPUT);

pinMode(motorPin, OUTPUT);

}

 

 

void loop()

{

  val = analogRead(potpin);        

  val = map(val, 0, 1023, 0, 255);   

 

analogWrite(motorPin, val); 

  delay(15);                         

}

 

 

AND

 

 

 

#include <Servo.h>

 

Servo myservo; 

 

int potpin = 5; 

int val;   

 

void setup()

{

  myservo.attach(3); 

}

 

void loop()

{

  val = analogRead(potpin);           

  if (val<300){

  myservo.write(67);

  }else if (val<600){

  myservo.write(89);

  } else {

    myservo.write(109);

  }

 

delay(15);                          

}

 

Heres the combined code that doesnt work.If you see whats wrong please reply, couse I cant find the mistake here.

 

 

#include <Servo.h>

Servo myservo;  // create servo object to control a servo

int motorPin = 9;

int potpin1 = 5;  // GEARS

int potpin = 0;  // SPEED

int val;    // variable to read the value from the analog pin

 

 

void setup()

{

  pinMode(potpin1,INPUT);                //GEARS

  pinMode(potpin,INPUT);                 //SPEED

pinMode(motorPin, OUTPUT);

myservo.attach(3);  // attaches the servo on pin 9 to the servo object

}

 

 

void loop()

{

 

  val = analogRead(potpin);           //SPEED

  val= map(val, 0, 1023, 0, 255); 

 

 

analogWrite(motorPin, val); 

  delay(15);                         

 

  val = analogRead(potpin1);            //   GEARS

  if (val<300){

  myservo.write(130);

  }else if (val<600){

  myservo.write(110);

  } else {

    myservo.write(90);

  }

 

delay(15);

}

 

int motorPin = 9;
int potpin = 0;  // analog pin used to connect the potentiometer
int val;    // variable to read the value from the analog pin
void setup()
{
  pinMode(potpin,INPUT);
pinMode(motorPin, OUTPUT);
}
void loop()
{
  val = analogRead(potpin);        
  val = map(val, 0, 1023, 0, 255);   
analogWrite(motorPin, val); 
  delay(15);                         
}

ALSO HERES A VIDEO SHOWING THE APLICATION OF THE FIRST TWO CODES  

http://www.youtube.com/watch?v=MrHqeFmT6DU

  • Sign in to reply
  • Cancel

Top Replies

  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver +1
    Most welcome...
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    // Try this code

     

    #include <Servo.h>

     

    Servo gear;
    int pot1= A0;                  //for motor
    int pot2= A1;                  //for servo

     

    int motor = 9;
    int s,g,i;                     // variable to store analog value. s=speed, g=gear and i=intermediate;

     

    void setup()
    {
      pinMode(pot1, INPUT);
      pinMode(pot2, INPUT);
      pinMode(motor, OUTPUT);
      gear.attach(3);               
    }

     

    void loop()
    {
      g=analogRead(pot2);
      i=map(i,0,1023,0,179);              // mapping according to your 180* servo
     
      s=analogRead(pot1);
      s=map(s,0,1023,0,255);             //mapping for motor speed
     
      analogWrite(motor,s);
      delay(5);
     
          if(i<53)
          {
           gear.write(130);
          }
          else if(i<106)
          {
           gear.write(110);
          }
          else
          {
            gear.write(90);
          }
          delay(10);     
    }
     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to e14 Contributor

    here's something weird!!!
    I changed the code so that it uses only one pot for controling the servo and the motor is constantly on,
    now heres the thing- when the motor is set to 255 -its starts rotating , the servo is working like its supposed to (getting readings from the pot)
    BUT when i set the motor to say 50 or 100 the motor doesnt spin, the servo goes crazy (random positions)
    heres the code
    #include <Servo.h>
    Servo myservo;
    int motorPin = 9;
    int potpin = 1; 
    int val;   
    void setup()
    {
      myservo.attach(3);
    pinMode(motorPin, OUTPUT);
    }
    void loop()
    {
      val = analogRead(potpin);           
      if (val<300){
      myservo.write(67);
      }else if (val<600){
      myservo.write(89);
      } else {
        myservo.write(109);
      }
                     
    delay(15); 
      analogWrite(motorPin, 255);    // WHEN I SET THIS TO 50 OR 100 INSTEAD OF 255 - NOTHING SEEMS TO WORK
      delay(15);  
    }
    that is the base of my problem couse when i have a pot controling the motor and whne its sending it a value not close to 255 the servo goes crazy and the motor is unable to start (it starts at the pots max ..at full speed )
    anyone any ideas image

    here's something weird!!!

    I changed the code so that it uses only one pot for controling the servo and the motor is constantly on,

    now heres the thing- when the motor is set to 255 -its starts rotating , the servo is working like its supposed to (getting readings from the pot)

    BUT when i set the motor to say 50 or 100 the motor doesnt spin, the servo goes crazy (random positions)

    heres the code

     

    #include <Servo.h>

     

    Servo myservo;

     

    int motorPin = 9;

    int potpin = 1; 

    int val;   

     

    void setup()

    {

      myservo.attach(3);

    pinMode(motorPin, OUTPUT);

    }

     

    void loop()

    {

      val = analogRead(potpin);           

      if (val<300){

      myservo.write(67);

      }else if (val<600){

      myservo.write(89);

      } else {

        myservo.write(109);

      }

     

    delay(15); 

     

      analogWrite(motorPin, 255);    // WHEN I SET THIS TO 50 OR 100 INSTEAD OF 255 - NOTHING SEEMS TO WORK

      delay(15);  

    }

     

    that is the base of my problem couse when i have a pot controling the motor and whne its sending it a value not close to 255 the servo goes crazy and the motor is unable to start (it starts at the pots max ..at full speed )

     

    anyone any ideas image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to dirtdiver

    U missed one thing in your programme and that is pinMode(potpin,INPUT);

    Now another thing, if you put any analog pin as input mode and if you do not connect any wire/pot, by mistake, to Analog pin then it will take value 'Randomly', rectified type wave would be there...so this problem might be there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to dirtdiver

    Here is the another way to do it... using L293 Motor driver IC. Now you dont need any kind of transistor. So hardware problem reduced here....

    Just try it...i have tried this at home. make sure you have connected grounds both of the devices together.

     

    as you can see in the picture,

    1 pin of IC is PWM. Its is enable, connect arduino pwm pin here. So you can control speed also.

    2 and 7 shoud be connected to arduino digital pin. So, by putting high and low to pins, you can set the motor direction easily.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to dirtdiver

    Here is the another way to do it... using L293 Motor driver IC. Now you dont need any kind of transistor. So hardware problem reduced here....

    Just try it...i have tried this at home. make sure you have connected grounds both of the devices together.

     

    as you can see in the picture,

    1 pin of IC is PWM. Its is enable, connect arduino pwm pin here. So you can control speed also.

    2 and 7 shoud be connected to arduino digital pin. So, by putting high and low to pins, you can set the motor direction easily.