Arduino
  • Products
  • More
Arduino
Arduino Forum Programing issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 3 answers
  • Subscribers 420 subscribers
  • Views 4918 views
  • Users 0 members are here
  • programing
  • arduino
Related

Programing issue

dirtdiver
dirtdiver over 14 years ago

Hi,

so I have a dc motor and a servo each controlled with a different potentiometer.First I made two separate codes and all works fine, but when I combine the two codes the servo starts getting readings from both pots.Here are the working codes

 

int motorPin = 9;                                          

int potpin = 0;

int val;   

 

void setup()

{

  pinMode(potpin,INPUT);

pinMode(motorPin, OUTPUT);

}

 

 

void loop()

{

  val = analogRead(potpin);        

  val = map(val, 0, 1023, 0, 255);   

 

analogWrite(motorPin, val); 

  delay(15);                         

}

 

 

AND

 

 

 

#include <Servo.h>

 

Servo myservo; 

 

int potpin = 5; 

int val;   

 

void setup()

{

  myservo.attach(3); 

}

 

void loop()

{

  val = analogRead(potpin);           

  if (val<300){

  myservo.write(67);

  }else if (val<600){

  myservo.write(89);

  } else {

    myservo.write(109);

  }

 

delay(15);                          

}

 

Heres the combined code that doesnt work.If you see whats wrong please reply, couse I cant find the mistake here.

 

 

#include <Servo.h>

Servo myservo;  // create servo object to control a servo

int motorPin = 9;

int potpin1 = 5;  // GEARS

int potpin = 0;  // SPEED

int val;    // variable to read the value from the analog pin

 

 

void setup()

{

  pinMode(potpin1,INPUT);                //GEARS

  pinMode(potpin,INPUT);                 //SPEED

pinMode(motorPin, OUTPUT);

myservo.attach(3);  // attaches the servo on pin 9 to the servo object

}

 

 

void loop()

{

 

  val = analogRead(potpin);           //SPEED

  val= map(val, 0, 1023, 0, 255); 

 

 

analogWrite(motorPin, val); 

  delay(15);                         

 

  val = analogRead(potpin1);            //   GEARS

  if (val<300){

  myservo.write(130);

  }else if (val<600){

  myservo.write(110);

  } else {

    myservo.write(90);

  }

 

delay(15);

}

 

int motorPin = 9;
int potpin = 0;  // analog pin used to connect the potentiometer
int val;    // variable to read the value from the analog pin
void setup()
{
  pinMode(potpin,INPUT);
pinMode(motorPin, OUTPUT);
}
void loop()
{
  val = analogRead(potpin);        
  val = map(val, 0, 1023, 0, 255);   
analogWrite(motorPin, val); 
  delay(15);                         
}

ALSO HERES A VIDEO SHOWING THE APLICATION OF THE FIRST TWO CODES  

http://www.youtube.com/watch?v=MrHqeFmT6DU

  • Sign in to reply
  • Cancel

Top Replies

  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver +1
    Most welcome...
Parents
  • cookieglitch
    0 cookieglitch over 14 years ago

    Have you tried writing the pot values to the serial line to see what they are reading when you change them?

     

    Does the code work when the outputs are connected to LEDs rather than the servo and motor? If it works (with a couple of minor software changes for the servo), it may be that the motors are trying to draw too much power. Hard to say however  with schematics etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to cookieglitch

    "with a couple of minor software changes for the servo"

    like what , couse I want to try it, nothing else seems to work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dmaruska

    changing the motor's rotation direction

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 14 years ago in reply to dirtdiver

    This seems a bit complicated, Cool looking but just not practical.  Have you though about this?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dmaruska

    what exactly is 1-8 ,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 14 years ago in reply to dirtdiver

    This is a generic Relay.  If you use a relay, read the datasheet and see which is the COIL on the relay, same with the contact leads.  Some relays are polorized and + and - must be on specific pins.  This relay is a DPDT type, if used make sure that a BREAK before MAKE type is used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dmaruska

    How many pins do I need to controll this relay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dirtdiver

    I can controll it with 2 pins right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 14 years ago in reply to dirtdiver

    With the schematic above you can control motor with two pins and use the analogRead to set the PWM.  Remember In the default position, (called "Normally Closed" position or "NC", this is the unpowered state of the relay), you will need to have the PWM set to 0%, or the motor will be running.  You can add another control line and completely remove the power from the input side of the relay, then it will not matter what the PWM is doing until you engage the main power switch.  On the Relay, the DPDT type has a control coil that will operate the relay.  One set of contacts are always closed until you power the relay and it will change state to the "Normally Open" or NO state and supply power.  This is acting like a real cheap H Block.  In the end you have a Pot to control speed, two to three digital IO pins to control the Relay and the PWM, and the third Digital IO to control the main power to the PWM transistor.  Attached is a drawing.  You could also use Q3 to control another relay insteed of running all the Voltage and Current through both Transistors.  You also may have to adjust the Base resistors to get exactly what you what.  If you dont add the third transistor connect the power to the collector on Q1.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dmaruska

    Ok ,  that is definitely better then using a servo with a switch, so I need a DPDT relay that works on 5 volts,right

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 14 years ago in reply to dirtdiver

    Sure, they usually come in 3v3(Newer), 5, 12, 24.  You can try a 12v and see if it will operate at 9V, if not use a 5V relay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dmaruska

    ok thaks alot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dmaruska

    ok thaks alot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dmaruska
    0 dmaruska over 14 years ago in reply to dirtdiver

    Most welcome...