Arduino
  • Products
  • More
Arduino
Arduino Forum Programing issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 3 answers
  • Subscribers 420 subscribers
  • Views 4913 views
  • Users 0 members are here
  • programing
  • arduino
Related

Programing issue

dirtdiver
dirtdiver over 14 years ago

Hi,

so I have a dc motor and a servo each controlled with a different potentiometer.First I made two separate codes and all works fine, but when I combine the two codes the servo starts getting readings from both pots.Here are the working codes

 

int motorPin = 9;                                          

int potpin = 0;

int val;   

 

void setup()

{

  pinMode(potpin,INPUT);

pinMode(motorPin, OUTPUT);

}

 

 

void loop()

{

  val = analogRead(potpin);        

  val = map(val, 0, 1023, 0, 255);   

 

analogWrite(motorPin, val); 

  delay(15);                         

}

 

 

AND

 

 

 

#include <Servo.h>

 

Servo myservo; 

 

int potpin = 5; 

int val;   

 

void setup()

{

  myservo.attach(3); 

}

 

void loop()

{

  val = analogRead(potpin);           

  if (val<300){

  myservo.write(67);

  }else if (val<600){

  myservo.write(89);

  } else {

    myservo.write(109);

  }

 

delay(15);                          

}

 

Heres the combined code that doesnt work.If you see whats wrong please reply, couse I cant find the mistake here.

 

 

#include <Servo.h>

Servo myservo;  // create servo object to control a servo

int motorPin = 9;

int potpin1 = 5;  // GEARS

int potpin = 0;  // SPEED

int val;    // variable to read the value from the analog pin

 

 

void setup()

{

  pinMode(potpin1,INPUT);                //GEARS

  pinMode(potpin,INPUT);                 //SPEED

pinMode(motorPin, OUTPUT);

myservo.attach(3);  // attaches the servo on pin 9 to the servo object

}

 

 

void loop()

{

 

  val = analogRead(potpin);           //SPEED

  val= map(val, 0, 1023, 0, 255); 

 

 

analogWrite(motorPin, val); 

  delay(15);                         

 

  val = analogRead(potpin1);            //   GEARS

  if (val<300){

  myservo.write(130);

  }else if (val<600){

  myservo.write(110);

  } else {

    myservo.write(90);

  }

 

delay(15);

}

 

int motorPin = 9;
int potpin = 0;  // analog pin used to connect the potentiometer
int val;    // variable to read the value from the analog pin
void setup()
{
  pinMode(potpin,INPUT);
pinMode(motorPin, OUTPUT);
}
void loop()
{
  val = analogRead(potpin);        
  val = map(val, 0, 1023, 0, 255);   
analogWrite(motorPin, val); 
  delay(15);                         
}

ALSO HERES A VIDEO SHOWING THE APLICATION OF THE FIRST TWO CODES  

http://www.youtube.com/watch?v=MrHqeFmT6DU

  • Sign in to reply
  • Cancel

Top Replies

  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver +1
    Most welcome...
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dirtdiver

    I can controll it with 2 pins right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 14 years ago in reply to dirtdiver

    With the schematic above you can control motor with two pins and use the analogRead to set the PWM.  Remember In the default position, (called "Normally Closed" position or "NC", this is the unpowered state of the relay), you will need to have the PWM set to 0%, or the motor will be running.  You can add another control line and completely remove the power from the input side of the relay, then it will not matter what the PWM is doing until you engage the main power switch.  On the Relay, the DPDT type has a control coil that will operate the relay.  One set of contacts are always closed until you power the relay and it will change state to the "Normally Open" or NO state and supply power.  This is acting like a real cheap H Block.  In the end you have a Pot to control speed, two to three digital IO pins to control the Relay and the PWM, and the third Digital IO to control the main power to the PWM transistor.  Attached is a drawing.  You could also use Q3 to control another relay insteed of running all the Voltage and Current through both Transistors.  You also may have to adjust the Base resistors to get exactly what you what.  If you dont add the third transistor connect the power to the collector on Q1.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dmaruska

    Ok ,  that is definitely better then using a servo with a switch, so I need a DPDT relay that works on 5 volts,right

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 14 years ago in reply to dirtdiver

    Sure, they usually come in 3v3(Newer), 5, 12, 24.  You can try a 12v and see if it will operate at 9V, if not use a 5V relay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dmaruska

    ok thaks alot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 14 years ago in reply to dirtdiver

    Most welcome...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    // Try this code

     

    #include <Servo.h>

     

    Servo gear;
    int pot1= A0;                  //for motor
    int pot2= A1;                  //for servo

     

    int motor = 9;
    int s,g,i;                     // variable to store analog value. s=speed, g=gear and i=intermediate;

     

    void setup()
    {
      pinMode(pot1, INPUT);
      pinMode(pot2, INPUT);
      pinMode(motor, OUTPUT);
      gear.attach(3);               
    }

     

    void loop()
    {
      g=analogRead(pot2);
      i=map(i,0,1023,0,179);              // mapping according to your 180* servo
     
      s=analogRead(pot1);
      s=map(s,0,1023,0,255);             //mapping for motor speed
     
      analogWrite(motor,s);
      delay(5);
     
          if(i<53)
          {
           gear.write(130);
          }
          else if(i<106)
          {
           gear.write(110);
          }
          else
          {
            gear.write(90);
          }
          delay(10);     
    }
     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to e14 Contributor

    nope, the same thing , I'm beginning to think thats a hardware problem, the code looks fine

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to e14 Contributor

    here's something weird!!!
    I changed the code so that it uses only one pot for controling the servo and the motor is constantly on,
    now heres the thing- when the motor is set to 255 -its starts rotating , the servo is working like its supposed to (getting readings from the pot)
    BUT when i set the motor to say 50 or 100 the motor doesnt spin, the servo goes crazy (random positions)
    heres the code
    #include <Servo.h>
    Servo myservo;
    int motorPin = 9;
    int potpin = 1; 
    int val;   
    void setup()
    {
      myservo.attach(3);
    pinMode(motorPin, OUTPUT);
    }
    void loop()
    {
      val = analogRead(potpin);           
      if (val<300){
      myservo.write(67);
      }else if (val<600){
      myservo.write(89);
      } else {
        myservo.write(109);
      }
                     
    delay(15); 
      analogWrite(motorPin, 255);    // WHEN I SET THIS TO 50 OR 100 INSTEAD OF 255 - NOTHING SEEMS TO WORK
      delay(15);  
    }
    that is the base of my problem couse when i have a pot controling the motor and whne its sending it a value not close to 255 the servo goes crazy and the motor is unable to start (it starts at the pots max ..at full speed )
    anyone any ideas image

    here's something weird!!!

    I changed the code so that it uses only one pot for controling the servo and the motor is constantly on,

    now heres the thing- when the motor is set to 255 -its starts rotating , the servo is working like its supposed to (getting readings from the pot)

    BUT when i set the motor to say 50 or 100 the motor doesnt spin, the servo goes crazy (random positions)

    heres the code

     

    #include <Servo.h>

     

    Servo myservo;

     

    int motorPin = 9;

    int potpin = 1; 

    int val;   

     

    void setup()

    {

      myservo.attach(3);

    pinMode(motorPin, OUTPUT);

    }

     

    void loop()

    {

      val = analogRead(potpin);           

      if (val<300){

      myservo.write(67);

      }else if (val<600){

      myservo.write(89);

      } else {

        myservo.write(109);

      }

     

    delay(15); 

     

      analogWrite(motorPin, 255);    // WHEN I SET THIS TO 50 OR 100 INSTEAD OF 255 - NOTHING SEEMS TO WORK

      delay(15);  

    }

     

    that is the base of my problem couse when i have a pot controling the motor and whne its sending it a value not close to 255 the servo goes crazy and the motor is unable to start (it starts at the pots max ..at full speed )

     

    anyone any ideas image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to dirtdiver

    U missed one thing in your programme and that is pinMode(potpin,INPUT);

    Now another thing, if you put any analog pin as input mode and if you do not connect any wire/pot, by mistake, to Analog pin then it will take value 'Randomly', rectified type wave would be there...so this problem might be there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>