Arduino
  • Products
  • More
Arduino
Arduino Forum which gps shield and module for Arduino Uno
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 2 answers
  • Subscribers 420 subscribers
  • Views 3647 views
  • Users 0 members are here
  • robot
  • arduino_uno
  • gps_antenna
  • gps_shield
  • arduino
  • gps_module
Related

which gps shield and module for Arduino Uno

EmreKon1
EmreKon1 over 14 years ago

i wanna make gps quided car with Arduino Uno R3. which gps shield, module and antenna may i buy?

  • Sign in to reply
  • Cancel

Top Replies

  • Lupo
    Lupo over 13 years ago in reply to EmreKon1 +1
    There is also this one, very interesting: http://www.open-electronics.org/gsm-gps-shield-for-arduino/
Parents
  • fustini
    0 fustini over 14 years ago

    I've heard good things about Adafruit's Ultimate GPS breakout board: http://adafruit.com/products/746

     

    They have nice tutorial for it, too: http://learn.adafruit.com/adafruit-ultimate-gps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 14 years ago in reply to fustini

    is that shield suitable for Arduino??     26.40$   +   free shipping

     

    http://dx.com/cn-06-gps-receiver-super-u-blox-gps-module-w-active-ceramic-antenna-mwc-149340?item=1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 14 years ago in reply to simon.monk

    Power supply voltage (VCC)                  Min:2.7V      Typ:3.0V      Max:3.6V

    Supply voltage USB (VDDUSB)             Min:3.0V      Typ:3.3V      Max:3.6V

     

    can i conntect arduino's  3.7 V pin ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • simon.monk
    0 simon.monk over 14 years ago in reply to EmreKon1

    Ah, okay, well the Uno can supply 50mA at 3.3V, how many mA does the module need?

     

    If you connect the Tx of the module to the Rx of the Uno and DO NOTwire the Tx of the Uno to the Rx of the module, then the 5V Arduino will be able to read the 3.3v serial signal from the gps module. It will mean you have to take the default settings of the GPS module as far as baud rate etc goes. Its probably 9600 8N1 so you should be okay.

     

    If you do decide you need to send data from the Uno to the GPS, you will have to use a level converter. Buts lets cross that bridge if we come to it image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 14 years ago in reply to simon.monk

    Condition :      VCC=3.0V

     

    Icc Acquisition : 47mA

    Icc Tracking (Max Performance mode) : 40mA

    Icc Tracking (Eco mode) : 37mA

    Icc Tracking (Power Save mode / 1 Hz) : 11mA

     

    UARTBaud rate : 9600 (USB powered)

     

     

     

    http://www.u-blox.com/images/downloads/Product_Docs/NEO-6_DataSheet_%28GPS.G6-HW-09005%29.pdf

     

    datasheet for neo-6 gps module

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • simon.monk
    0 simon.monk over 14 years ago in reply to EmreKon1

    Looks like it should be just okay image

     

    Anything I haven't thought of anyone?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 14 years ago in reply to simon.monk

    Thank you too much:) i will buy and try than i will write here :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • simon.monk
    0 simon.monk over 14 years ago in reply to EmreKon1

    No problem. Please do post back - if they are any good, I'll probably get one too. image

     

    Did you see the brushless quadcopter motors for $13 on that web page? Amazingly cheap.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 14 years ago in reply to simon.monk

    dealextreme is my nu 1 :) so cheap and free shipping :) i strongly reccomend.

     

    I will also ask you about quadrocopter parts but not that time becouse im not at that level:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 14 years ago in reply to simon.monk

    http://www.AeroQuadStore.com/Logic_Level_Converter_p/bob-08745.htm

    Can i use  "logic level converter" to  convert 5.0V of arduino to gps's 3.6V

     

    Or

     

    Is arduino's 3,7V pin enough?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • simon.monk
    0 simon.monk over 14 years ago in reply to EmreKon1

    You can power it from the Arduino 3.3V power connection.

     

    Remember do not connect the Arduino Tx to the GPS Rx - that will quite likely kill it.

     

    Only connect the Arduino Rx to the GPS Tx,

    GND to GND

    and Arduiono 3.3V to GPS VCC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 14 years ago in reply to simon.monk

    Thank you again:) i bought it. It will be my hand 15 daysy later than i will post my experiences with you:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • EmreKon1
    0 EmreKon1 over 14 years ago in reply to simon.monk

    Thank you again:) i bought it. It will be my hand 15 daysy later than i will post my experiences with you:)