Arduino Forum Series 2 Coordinator and End Devices not responding to Andrew Rapp's Xbee-Arduino Library--- need help
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
  • State Suggested Answer
  • Replies 6 replies
  • Answers 6 answers
  • Subscribers 401 subscribers
  • Views 693 views
  • Users 0 members are here
  • xbee_series_2
  • wireless_sensor_network
Related

Series 2 Coordinator and End Devices not responding to Andrew Rapp's Xbee-Arduino Library--- need help

Former Member
Former Member over 12 years ago

I want to build a Wireless Sensor Network with a XB24-B Series 2 XBee connected to Arduino Mega 2560 acting as a Coordinator and three XB24-B Series 2 XBees connected to three Arduino Uno boards respectively, acting as End Devices. To each Uno board at end is connected a temperature sensor. I have configured my XBees using X-CTU in the following ways:

 

 

Coordinator Xbee (ZNET2.5 COORDINATOR API) ->

PAN ID = 200

DH=0

Dl=0

NI=COORD

AP=2


End node_0 Xbee (ZNET2.5 ROUTER/END DEVICE API) ->


PAN ID =200

DH=0013A200 (High byte of Coordinator)

DL= 4060647B (Low byte of Coordinator)

JV = 1

NI = R1

AP=2

 


My Coordinator side Sketch is as follows :-

 

#include <XBee.h>

 


XBee xbee = XBee();

ZBRxResponse zbRx = ZBRxResponse();


uint8_t payload[5] = {0,0,0,0,0};  //initialises the data array with 0s



void setup(){

  delay(1000);

  xbee.setSerial(Serial3);

  xbee.begin(9600);

  Serial.begin(9600);

  Serial.println("Ready");

}


void loop(){

  xbee.readPacket();

  if(xbee.getResponse().isAvailable()){

    if(xbee.getResponse().getApiId() == ZB_RX_RESPONSE){

      xbee.getResponse().getZBRxResponse(zbRx);

      for(int i = 0; i < zbRx.getDataLength(); i++){

        payload [i] = zbRx.getData(i);

      }

      uint8_t analogHi = payload[0];

      uint8_t analogLo = payload[1];

      int value = analogLo + (analogHi*256);

     

     

      int A = value;

      int C = payload[3];

      int E = payload[4];

      int flag = payload[2];

     

      if(E == 0){

        Serial.print("BOARD IDENTIFIER -> ");

        Serial.println(E);

        Serial.print("Temperature ");

        Serial.println(A);

        if (flag == 0){

          Serial.print("-");

          Serial.println(C);

        }

        else{

          Serial.println(C);

        }

      }

       else if (E == 1){

        Serial.print("BOARD IDENTIFIER -> ");

        Serial.println(E);

        Serial.print("Temperature " );

        Serial.println(A);

        if (flag == 0){

          Serial.print("-");

          Serial.println(C);

        }

        else{

          Serial.println(C);

        }

       }

       else{

         Serial.println("ERROR IDENTIFYING BOARD");

       }

       delay(1000);

    }

  }

  // Serial.println("Inside loop");

   //delay(1000);

}

My Router Side Sketch is as follows :-

 

#include <XBee.h>

 


uint8_t payload[5] = {0,0,0,0,0};

XBee xbee = XBee();

XBeeAddress64 remoteAddress = XBeeAddress64(0x0013A200 ,0x4060647B);


ZBTxRequest zbTx = ZBTxRequest(remoteAddress,payload,sizeof(payload));


int tempPin =0; //Analog pin 0

int ledPin = 13;

int tempReading;

int flag;

int ID =0;                            //change this accordingly to you node


void setup(){

  Serial.begin(9600);

  pinMode(ledPin,OUTPUT);

  pinMode(tempPin,OUTPUT);

  analogReference(INTERNAL);

 

}


void loop(){

  tempReading = analogRead(tempPin);

  Serial.println(tempReading);

  int celcius = getTemp(tempReading);

  Serial.print("Temperature in celcius");

  Serial.println(celcius);

  delay(100);

  digitalWrite(ledPin,HIGH);

  delay(1000);

  digitalWrite(ledPin,LOW);

  delay(1000);

 

  payload[0] = tempReading >> 8 & 0xff;

  payload[1] = tempReading & 0xff;

 

  if(celcius<0){

    flag=0;

  }

  else{

    flag=1;

  }

 

  payload[2] = flag;

  payload[3] = celcius;

  payload [4] = ID;

 

  xbee.send(zbTx);

  delay(60000); 

}


float getTemp(float k){

 

  k = (k * 110)/1024.0;

  float celcius = k;

  return celcius;

 

}

 

I have connected the Dout of XBee coordinator to Rx3 of Mega and Din of XBee coordinator to Tx3 of Mega

.

Now , when I open serial terminals in both the sides I could see nothing on the Coordinator Side serial window , except ready which I have printed statically.However, I could see the temperature readings being printed on the serial terminal on the end device side followed by a frame of random numbers.


Can anybody tell me where have I gone wrong? I am eagerly waiting for your advices.

 

image

 

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago in reply to Former Member +1 suggested
    Hello Sriramreddy, You have to use X-CTU itself.But you have to put the arduino in RESET mode while configuring the XBee. This is done by connecting the RESET pin of the Arduino to its GND pin. From the…
Parents
  • Former Member
    0 Former Member over 12 years ago

    hai again have you done this to The remote radio must have IR > 0 and at least one digital or analog input enabled.if you want to make your arduino as a usb serial port uhave to connect arduino pin 8 to Tx of usb serial device and arduino pin 9 to rx of usb serial device

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    hai again have you done this to The remote radio must have IR > 0 and at least one digital or analog input enabled.if you want to make your arduino as a usb serial port uhave to connect arduino pin 8 to Tx of usb serial device and arduino pin 9 to rx of usb serial device

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer