Arduino
  • Products
  • More
Arduino
Arduino Forum Simple circuiting question, using Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 30 replies
  • Answers 2 answers
  • Subscribers 420 subscribers
  • Views 3152 views
  • Users 0 members are here
Related

Simple circuiting question, using Arduino

e14 Contributor
e14 Contributor over 13 years ago

I want to control a 24v DC circuit with a my arduino, what would be the proper component and roughly how would I use it. Basically when I set a pin to high, I want it to switch the 24V on, and turn it off when set to low. From what I can gather, I need a MOSFET, but I have minimal knowledge on what to look for in one. Would someone be able to assist me?

 

(p.s. This is my first discussion, sorry if I am doing this incorrectly)

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 13 years ago in reply to ntewinkel +2
    Nico teWinkel wrote: You should probably at least have a resistor between the Arduino pin and the mosfet. [I've never designed with Arduino, so these are comments that apply to most microcontrollers.]…
  • ntewinkel
    ntewinkel over 13 years ago +1 suggested
    Hi Mason, You should probably at least have a resistor between the Arduino pin and the mosfet. Oomlout has a circuit example using a smaller transistor: http://www.oomlout.com/oom.php/products/ardx/circ…
  • ntewinkel
    ntewinkel over 13 years ago +1
    ps, this Instructable might also help: http://www.instructables.com/id/Use-Arduino-with-TIP120-transistor-to-control-moto/
Parents
  • billabott
    0 billabott over 13 years ago

    May I suggest the following:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to billabott

    I think the OP wanted to control a 24v item.

    This is a very good referemce for anyone wanting to measure a 24v voltage.

     

     

    One thing that you might see on some circuits is a diode at the pin of the micro that has its anode connected to the supply.

    This makes sure the voltage at the pin can never be more tha 0.5v higher than the supply  ...which strangely fits within most IC specs.

     

    Of course this theory is only any good if the series resitor is in place otherwise the supply could get driven upwards.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago in reply to billabott

    I think the OP wanted to control a 24v item.

    This is a very good referemce for anyone wanting to measure a 24v voltage.

     

     

    One thing that you might see on some circuits is a diode at the pin of the micro that has its anode connected to the supply.

    This makes sure the voltage at the pin can never be more tha 0.5v higher than the supply  ...which strangely fits within most IC specs.

     

    Of course this theory is only any good if the series resitor is in place otherwise the supply could get driven upwards.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billabott
    0 billabott over 13 years ago in reply to mcb1

    You are talking over my head with that diode idea.   The senario as I understood it was that how best to safeguard the microC in case the NFET shorted out completely.  So, Mark, are you saying that there are good reasons to also add the diode you mentioned in addition to the voltage divider in my illustration?  Most NFETs need very little V+I  at the gate to turm them on, but, I aslo believe opto-isolators are a great way to go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to billabott

    William

    If you're simply wanting to stop a large voltage coming back from the 'failed' transistor/mosfet then a simple resistor between the pin and the base/gate with a 5.1v zener between the base/gate to ground should be  enough.

     

    Most NPN configured transistors that fail due to excess voltage, tend to go short circuit between the base and collector.

    This then tends to make the base and emitter conduct, which drops the voltage to around 0.6v.

    Depending on the load on the collector, the base junction either survives and carries the current, or it self destructs.

     

    For input voltages being applied to a pin, having a series resistor between the input voltage and the controller pin is good practice/essential.

    If you have a diode that has its anode to +5v (or supply) and the cathode connected to the input pin (ie in reverse bias) the voltage on the pin cannot exceed the supply (+0.6v).

    The difference is 'lost' across the resistor.

     

     

    Mason

    Your datasheet doesn't attach.

    Can you supply details of the transistor you have used and we can help.

     

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    Its a MJE3055T, a quick google search of the part number brought up the datasheet. I originally was looking for a IRF744N MOSFET, but all the radioshacks in my area seem to be out of almost all electrical components so I went with the NPN transitor because I thought I knew what I was doing haha.