Arduino
  • Products
  • More
Arduino
Arduino Forum xbee question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 1211 views
  • Users 0 members are here
Related

xbee question

e14 Contributor
e14 Contributor over 13 years ago

HI there guys,

 

My project is to connect one transmitting xbee to arduino 

 

I also have a  receiving xbee (both series 1) I want that the receiving Xbee will show up a "hello world" that got sent from the transmitter XBee and display it on an LCD 16X2 screen

 

I'm quite baffled how am I supposed to do that? code wise,wiring wise...I've searched the web and couldn't find an answer maybe you could help me out plz?

 

 

thanks from advance chen (or grace its the same in Hebrew image )

  • Sign in to reply
  • Cancel

Top Replies

  • fidelsalinas
    fidelsalinas over 13 years ago +1
    you'll need the following http://www.digi.com/support/kbase/kbasperesultdetl?id=2125 to update and program your xbees https://code.google.com/p/xbee-arduino/ the xbee arduino library http://arduino.cc…
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor +1
    Chen I might be wrong but you could try this. I suspect your lcd.print(Serial.read()); is treating what it reads as an integer, rather than a character, so when you print its simply a number rather than…
Parents
  • billabott
    0 billabott over 13 years ago

    By hyper terminal, do you mean the serial monitor?  Simply stated, instead of doing the Serial.writeln(" Hello World ") you would myLCD.writeln(" Hello World ").  The myLCD library is created using the techniques and library provided by the vendor/distributor/manufacturer of the LCD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    HI there i finally had some time to work on my project yayiii

     

    anywho what I did 

     

    1.connected xbee to the xctu (he is the transmitter one) with xbee explorer (direct connection to the usb entrence in my laptop)

    2.connected the second xbee to arduino

    3.connected the lcd to the arduino also

    4. my program is such :

     

    /*

     

    the circuit  :

    LCD -

    * LCD RS pin to digital pin 12

    * LCD Enable pin to digital pin 11

    * LCD D4 pin to digital pin 5

    * LCD D5 pin to digital pin 4

    * LCD D6 pin to digital pin 3

    * LCD D7 pin to digital pin 2

    * LCD R/W pin to ground

    * 10K resistor:

    * ends to +5V and ground

    * wiper to LCD VO pin (pin 3)

     

    */

     

    //includes

    #include <LiquidCrystal.h>   //LCD library

     

    // initialize the library with the numbers of the interface pins

    LiquidCrystal lcd(12, 11, 5, 4, 3, 2);

     

    void setup() {

     

      // set up the LCD's number of columns and rows:

                  lcd.begin(16, 2);

                Serial.begin(9600);

                lcd.setCursor(0,0);

     

    }

     

    void loop() {

     

     

     

      if(Serial.available( ) > 0 ) {

         

          lcd.print(Serial.read());

         

     

    }

     

    }

     

    I've tried to run in on the arduino and type something on the terminal and xctu and it doesnt come up on my lcd screen

     

    any ideas why and what should i do?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    HI there i finally had some time to work on my project yayiii

     

    anywho what I did 

     

    1.connected xbee to the xctu (he is the transmitter one) with xbee explorer (direct connection to the usb entrence in my laptop)

    2.connected the second xbee to arduino

    3.connected the lcd to the arduino also

    4. my program is such :

     

    /*

     

    the circuit  :

    LCD -

    * LCD RS pin to digital pin 12

    * LCD Enable pin to digital pin 11

    * LCD D4 pin to digital pin 5

    * LCD D5 pin to digital pin 4

    * LCD D6 pin to digital pin 3

    * LCD D7 pin to digital pin 2

    * LCD R/W pin to ground

    * 10K resistor:

    * ends to +5V and ground

    * wiper to LCD VO pin (pin 3)

     

    */

     

    //includes

    #include <LiquidCrystal.h>   //LCD library

     

    // initialize the library with the numbers of the interface pins

    LiquidCrystal lcd(12, 11, 5, 4, 3, 2);

     

    void setup() {

     

      // set up the LCD's number of columns and rows:

                  lcd.begin(16, 2);

                Serial.begin(9600);

                lcd.setCursor(0,0);

     

    }

     

    void loop() {

     

     

     

      if(Serial.available( ) > 0 ) {

         

          lcd.print(Serial.read());

         

     

    }

     

    }

     

    I've tried to run in on the arduino and type something on the terminal and xctu and it doesnt come up on my lcd screen

     

    any ideas why and what should i do?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    ok apperantly it does work however one problem when I type anything on the keyboard in order to transmit then instead of the the letter i get the ascii tabke number of it (for example if I type j on the keyboard instead of j  appear on the screen I get an 106 which is the ascii value for j )

     

    how to fix this problem in my code?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    Chen

    I might be wrong but you could try this.

     

    I suspect your

    lcd.print(Serial.read());

    is treating what it reads as an integer, rather than a character, so when you print its simply a number rather than the ascii equivalent of the character j.

     

    try

      if(Serial.available( ) > 0 ) {

      char input = Serial.read();

          lcd.print(input);

      }

     

    and see if it fixes it.

     

     

    Mark