Arduino
  • Products
  • More
Arduino
Arduino Forum xbee question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 1209 views
  • Users 0 members are here
Related

xbee question

e14 Contributor
e14 Contributor over 13 years ago

HI there guys,

 

My project is to connect one transmitting xbee to arduino 

 

I also have a  receiving xbee (both series 1) I want that the receiving Xbee will show up a "hello world" that got sent from the transmitter XBee and display it on an LCD 16X2 screen

 

I'm quite baffled how am I supposed to do that? code wise,wiring wise...I've searched the web and couldn't find an answer maybe you could help me out plz?

 

 

thanks from advance chen (or grace its the same in Hebrew image )

  • Sign in to reply
  • Cancel

Top Replies

  • fidelsalinas
    fidelsalinas over 13 years ago +1
    you'll need the following http://www.digi.com/support/kbase/kbasperesultdetl?id=2125 to update and program your xbees https://code.google.com/p/xbee-arduino/ the xbee arduino library http://arduino.cc…
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor +1
    Chen I might be wrong but you could try this. I suspect your lcd.print(Serial.read()); is treating what it reads as an integer, rather than a character, so when you print its simply a number rather than…
  • fidelsalinas
    0 fidelsalinas over 13 years ago

    you'll need the following

    http://www.digi.com/support/kbase/kbasperesultdetl?id=2125 to update and program your xbees

    https://code.google.com/p/xbee-arduino/ the xbee arduino library

    http://arduino.cc/en/Reference/LiquidCrystal?from=Tutorial.LCDLibrary the LCD library tutorial

    http://www.ladyada.net/make/xbee/arduino.html xbee tutorial

    with the info and librarys from those sites you shouldn't have a problem. but if you run into more trouble i'll be more then willing to help.

     

    F/S

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to fidelsalinas

    Thanks for the quick response I can see you put your heart into it with all the links I want to try and explain my situation

     

    well I did configured the Xbee's in the X-CTU all that is fine i also have the LCD libraray and I've read the tutorial in the ladyada website

     

    but that's not the problem...I have a functioning network of the xbee's (I made a program that sends a "Hello World" from the transmitter to the receiver and watch it on the hyper terminal)

    now i want instead of watch the receiving msg on the hyper terminal to watch it on a LCD screen ...but I don't know how to connect the system and write the code to perform this...

     

    and that's what I'm asking...

     

    (I'm at work now but I will upload pictures when I get back from work and maybe it will be more clearer so You could answer me exactly what I'm asking)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago

    By hyper terminal, do you mean the serial monitor?  Simply stated, instead of doing the Serial.writeln(" Hello World ") you would myLCD.writeln(" Hello World ").  The myLCD library is created using the techniques and library provided by the vendor/distributor/manufacturer of the LCD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    I'm using arduino interface ...myLCD is another library? (I know the liquidcrystal libraray)

     

    but anyway I think I understand what you mean

     

    I understand that anyway's that the LCD have to be attached to an arduino and I only have 1 (mega2560 r3) so what i will try to do is other way around (connect the transmitter xbee to the pc and send a msg from the XCTU and try and display it to the receiver connected to lcd screen (and the two of them will be connected to the arduino) and order another board and then try again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to billabott

    chen

     

    When you find answers useful, can you please select the helpful or correct answer icons and slect the appropriate one/ones.

    (Sorry I haven't seen how these occur since I haven't started a question)

     

    I note the responders did resolve your last query help resolve the issue, but the query is not marked answered.

     

     

    Thanks

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    where? i dont know how to do it...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    i dont know where ...i cant dind a button that says that..sorry...where is it? i will gladly press it or whatever i just dont know how to 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    sorry mark i dont see any button that says (helpful or answered...if i had seen it surely i would press it i still dont realy understand how this forum works..i will try and look it up in the next couple of days and if i will find how to do so i will promise xxoxo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    HI there i finally had some time to work on my project yayiii

     

    anywho what I did 

     

    1.connected xbee to the xctu (he is the transmitter one) with xbee explorer (direct connection to the usb entrence in my laptop)

    2.connected the second xbee to arduino

    3.connected the lcd to the arduino also

    4. my program is such :

     

    /*

     

    the circuit  :

    LCD -

    * LCD RS pin to digital pin 12

    * LCD Enable pin to digital pin 11

    * LCD D4 pin to digital pin 5

    * LCD D5 pin to digital pin 4

    * LCD D6 pin to digital pin 3

    * LCD D7 pin to digital pin 2

    * LCD R/W pin to ground

    * 10K resistor:

    * ends to +5V and ground

    * wiper to LCD VO pin (pin 3)

     

    */

     

    //includes

    #include <LiquidCrystal.h>   //LCD library

     

    // initialize the library with the numbers of the interface pins

    LiquidCrystal lcd(12, 11, 5, 4, 3, 2);

     

    void setup() {

     

      // set up the LCD's number of columns and rows:

                  lcd.begin(16, 2);

                Serial.begin(9600);

                lcd.setCursor(0,0);

     

    }

     

    void loop() {

     

     

     

      if(Serial.available( ) > 0 ) {

         

          lcd.print(Serial.read());

         

     

    }

     

    }

     

    I've tried to run in on the arduino and type something on the terminal and xctu and it doesnt come up on my lcd screen

     

    any ideas why and what should i do?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    ok apperantly it does work however one problem when I type anything on the keyboard in order to transmit then instead of the the letter i get the ascii tabke number of it (for example if I type j on the keyboard instead of j  appear on the screen I get an 106 which is the ascii value for j )

     

    how to fix this problem in my code?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>