Arduino Forum Arduino resets when solenoid shuts off
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
  • State Suggested Answer
  • Replies 54 replies
  • Answers 16 answers
  • Subscribers 396 subscribers
  • Views 8629 views
  • Users 0 members are here
  • emi_protection
  • arduino
Related

Arduino resets when solenoid shuts off

Former Member
Former Member over 11 years ago

I have an arduino hooked to a 2 relay board. Each relay is opto-isolated. The arduino and board each have their own 5V power feed. The relays are switching 12V to controll a motor and a solenoid valve.

Sometimes when the solenoid turns off, the arduino resets. From what I've read, it's likely an EMI problem caused by the solenoid. If I disconnect the solenoid, I don't see the problem.

I've seen various suggestions about using a varistor or a diode, but I don't know which is better or what values to try. Any recommendations?

I'm assuming that the varistor or diode should be as close to the solenoid as possible, shorting the power and ground lines, is this correct?

 

Thanks,

Chris

  • Sign in to reply
  • Cancel

Top Replies

  • c4m4ch0
    c4m4ch0 over 8 years ago in reply to maranatha +3 suggested
    Hello maranatha, you just need to connect the diode as it is in this image
  • Former Member
    Former Member over 11 years ago in reply to michaelkellett +2 suggested
    I put an IN4004 Rectifier Diode across the terminals of the solenoid and that seems to have solved the problem. I also found this page pretty educational: http://en.wikipedia.org/wiki/Flyback_diode
  • maranatha
    maranatha over 8 years ago in reply to Former Member +1
    Hi Chris Do you happen to have the connection diagram? I am facing similar problem and it would be really helpful if you could share a connection diagram (basically how you connect the rectifier diode…
Parents
  • D_Hersey
    0 D_Hersey over 8 years ago

    You may also want to use some ferrite beads on your power feed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago in reply to D_Hersey

    Trying to find the root cause first.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • maranatha
    0 maranatha over 8 years ago in reply to mcb1

    Hi Mark

     

    Thank you!!!

     

    I have to confess that I had been ignoring some basic principles.  I almost went to cry when the 1F didn't resolve the issue. Desperately, I just connected the grounds of the raspberry pi and the arduino...and it worked. I said desperately, because I had the GNDs of both Arduino and RPi connected when I started the project. It was working. But then, somewhere on the internet I read that connecting the GNDs of two separate circuits can be dangerous. So, I removed it. Removing that common GND didn't affect the operation until I decided to run the RPi headless. I removed the HDMI display and I start to have this ugly problem for more than a month. I should have tested removing the HDMI display in my original setup where both GNDs are connected.

     

    I hope this fixes the problem permanently! I will just keep this 1F capacitor for decoupling. I have also soldered ferrite beads for extra protection.

     

    I would be more than happy if somebody could explain me about the relevance of connecting the GNDs of both

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago in reply to maranatha

    Your diagram of your set up is incorrect. The most vital bit of information was missing - the input feed to the Arduino from the Rpi.

     

    If you want to keep both boards electrically isolated you'll need to use an optocoupler or a relay set in in reverse to drive the Arduino input pin to it's own gnd.

    You've got plenty of relays so it should be an issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago in reply to COMPACT

    I'd remove the capacitor and ferrite beads for the moment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to maranatha

    Removing that common GND didn't affect the operation until I decided to run the RPi headless

     

    Are you using wireless or ethernet to connect ot the RPi.?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maranatha
    0 maranatha over 8 years ago in reply to mcb1

    I am using WiFi. RPi-3 provides integrated WiFi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maranatha
    0 maranatha over 8 years ago in reply to COMPACT

    Hi COMPACT

     

    This is a preliminary test setup. I will have a pin feed from the RPi to the arduino for status check.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to maranatha

    I asked because the ethernet could result in the RPi flaoting up.

     

    The input pins on an Arduino are very sensitive and would likely float high when the RPi was powered up.

    While this shouldn't matter as far as the program is concerned, it's most likely that it was causing an issue on the supply side, resulting in it crashing the controller and the program.

     

    The fact it didn't do it while the HDMI lead was plugged in supports this.

     

     

    Various supplies can be used for the different items, however connecting the grounds ensures they all work relative to one another.

     

     

    Your 1F cap is a bit over the top, and maybe a 10,000 uF aor even somethign in between 1000 and 10,000uF would ehlp ensure any relay switching is not going to cause issues.

    Personally I would have used a 2,200 or 4,700uF on that board.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • maranatha
    0 maranatha over 8 years ago in reply to mcb1

    Hi Mark

     

    Thanks for the nice explanation.

     

    I was dubious about whether or not the arduino was resetting when I was experiencing the relay unlatching problem with the HDMI unplugged on the RPi. I was checking using multi-meter the pins of the arduino which goes to the relay (Vcc and pin 4, as in my program). When PIR/pin 8 is active/HIGH, pin 4 goes HIGH and latches the relay, but few seconds later pin 4 goes LOW(irrespective of my program code) and relay unlatches. The Vcc pin was not however changing during the incident (may be it had changed. But couldn't see that on the multi-meter. Oscilloscope would have been nice for checking that ).  If the Arduino was not resetting, so may be, as you said, the pin was floating.

     

    I will replace the 1F capacitor with 2200uF. It worked with 100uF when I check it after connecting the GNDs together.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago in reply to maranatha

    Room 101 - Tie unused input pins to a known stable state.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • maranatha
    0 maranatha over 8 years ago in reply to COMPACT

    Thanks COMPACT

     

    I will do that

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • maranatha
    0 maranatha over 8 years ago in reply to COMPACT

    Thanks COMPACT

     

    I will do that