Arduino Forum I Want To Make My Own Arduino Uno Board Is There Any Way To Make One At Home ??
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 10 answers
  • Subscribers 398 subscribers
  • Views 1103 views
  • Users 0 members are here
  • board
  • own
  • uno
  • my
  • arduino
Related

I Want To Make My Own Arduino Uno Board Is There Any Way To Make One At Home ??

saurocksall
saurocksall over 11 years ago

hi to all, i want to make my own arduino uno board, is it possible to make one at home ?? i have a arduino uno r3 and have made many fun projects with it i wanted to know can i make one at home as is is open sourced it would not be that difficult to do, has any one here done that ??  would like some help ...

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 11 years ago +3 suggested
    Hey Saurabh There are many documents/websites out there that show how to make Arduinos. Here is just one doing a quick google search How to make your own Arduino board . I have also made this one that…
  • bwelsby
    bwelsby over 8 years ago +3 suggested
    Here's one way to build an arduino , http://make.kosakalab.com/make/obaka-project/aruduino-skeleton_en
  • ntewinkel
    ntewinkel over 11 years ago +2 suggested
    The good folks at Oomlout put together this nice Instructable that should make it very easy: How to Breadboard Arduino Compatible. I've seen other Arduino-on-a-breadboard type Instructables there too,…
  • Nate1616
    0 Nate1616 over 11 years ago

    Hey Saurabh

    There are many documents/websites out there that show how to make Arduinos.  Here is just one doing a quick google search How to make your own Arduino board.  I have also made this one that has more of a polished look Techunboxed: Ktuluino - How to Build Your Own Arduino Clone.  Hope this helps

     

    Nate

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 11 years ago

    The good folks at Oomlout put together this nice Instructable that should make it very easy: How to Breadboard Arduino Compatible.

     

    I've seen other Arduino-on-a-breadboard type Instructables there too, but judging by other Oomlout tutorials I've seen, I would check theirs out first.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago

    Yes you can build your own Arduino and its very easy, basically you need to burn the Arduino's boot loader in New Atmega328 chip, and connect it with all the required components and 16MHz crystal oscillator, on bread board or on PCB.

    Arduino website itself has good tutorial for creating your arduino on breadboard. I would like to share one more tutorial, from which I have build my arduino, which also contains step by step video, Homemade Arduino Board.

    Further I am using this power supply from ebay to power my Homemade Arduino.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to Former Member

    Just to let you know, this is a 3 year old post. I would like to think the original poster got his answer by now image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • volly
    0 volly over 9 years ago in reply to Robert Peter Oakes

    Robert Peter Oakes, I would like to believe so myself. It would be nice if saurocksall could put us all in the picture here by letting us know whether he did and actually built

    the actual Homemade Arduino Board.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to volly

    It is actually very simple to make your own, or make enough to run your completed project as the full boards have so much redundant electronics not needed in most finished project. Probably about 6 components for the core, plus whatever your interfacing to.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to Robert Peter Oakes

    electronichamsters did a post during the Forget_me_not design challenge.

    Inexpensive & Flexible Home Automation / Wireless Sensors

     

    I thought he included a schematic somewhere on the site but I can't see to find it easily.

    The main part about this design is the 3v3 regulator to run the RFM69 module.

     

    For the cost of some of the open source boards, I don't think it's worth bothering making my own.

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Hello Saurabh!

     

    As all the other user friends says, that answer is yes you can ! There are a couple of things that maybe useful for you in the specific case. I don't know what kind of projects you have in mind (maybe a good idea to share them with us ?); We assume that it is really super-easy to make your arduino board - IMHO the absolutely easier is just the Paperduino project creating an Arduino compatibile board on a piece of paper image

    Then maybe you make things more easier for your specific projects. Instead of making the general purpose Arduino board with the advantage to be able to recycle indefinitely the board you can make for less than the cost of the commercial Arduino your own dedicated Arduino-like boards. 100% compatible with Arduino you can integrate the base circuit of the microcontroller with your dedicated components excluding all those parts that are not useful for you. The result is that you can obtain a Arduino compatible board running on your project, something original just done by you.

     

    Here are some examples I have used in past:

     

    TiltPan Micro Camera is up and running !!!

    Microcontroller Health Status Controller Board based on AVR328p

     

    The following is the schemits of another Arduino dedicated board. I hope this suggestion maybe useful, if you need more information let me know.

    Enrico

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ravi_butani
    0 ravi_butani over 8 years ago

    well u can even mk it on breadboard....what exactly you need here to mk ur own Arduino on breadboard is usb-uart converter and AtMega328 uC with arduino bootloader.... even Crystal is not compulsory...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to ravi_butani

    Hi Ravi,

     

    Yoi mean that it can work without crystal too?  Sounds very strange to me!

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>