Arduino
  • Products
  • More
Arduino
Arduino Forum Which Accelerometer Module Should I Use For My Self Balancing Robot ??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 415 subscribers
  • Views 371 views
  • Users 0 members are here
  • accelerometer
  • module
Related

Which Accelerometer Module Should I Use For My Self Balancing Robot ??

saurocksall
saurocksall over 12 years ago

Hi guys..

 

I am making a self balancing robot with Arduino UNO and i am not sure which accelerometer module should i buy, there are many options in the market, as i have not used accelerometers in the past  i am really confused, i want a cheep and easy to use one.. have any of u guys has made a Self Balancing Robot ?? Please help me !!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 12 years ago +2
    Hi Saurabh, For a 2 wheel robot, you only need a single axis accelerometer with a range of about 2 or 3 g. You need to decide if you want to use analog output signals or serial communications with the…
  • ntewinkel
    ntewinkel over 12 years ago +1
    Hi Saurabh, If you're open to using something that is not Arduino, but still very easy to use, maybe have a look at the Freescale FRDM-KL25z board . It is about $14 and includes an on board accelerometer…
Parents
  • dougw
    0 dougw over 12 years ago

    Hi Saurabh,

    For a 2 wheel robot, you only need a single axis accelerometer with a range of about 2 or 3 g.

    You need to decide if you want to use analog output signals or serial communications with the accelerometer. Analog is simpler to program, but harder to achieve accuracy, however you can achieve balance with either.

    Either way, you will need an accelerometer that has a bandwidth above 100 Hz - the output signal must be able to detect changes in acceleration faster than 100 times per second, and preferably significantly faster than this.

    As you mentioned, there are many inexpensive devices with these specifications, just pick the cheapest one that is Arduino compatible with the suitable range and bandwidth..

    Doug

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 12 years ago

    Hi Saurabh,

    For a 2 wheel robot, you only need a single axis accelerometer with a range of about 2 or 3 g.

    You need to decide if you want to use analog output signals or serial communications with the accelerometer. Analog is simpler to program, but harder to achieve accuracy, however you can achieve balance with either.

    Either way, you will need an accelerometer that has a bandwidth above 100 Hz - the output signal must be able to detect changes in acceleration faster than 100 times per second, and preferably significantly faster than this.

    As you mentioned, there are many inexpensive devices with these specifications, just pick the cheapest one that is Arduino compatible with the suitable range and bandwidth..

    Doug