Arduino
  • Products
  • More
Arduino
Arduino Forum Which Accelerometer Module Should I Use For My Self Balancing Robot ??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 415 subscribers
  • Views 370 views
  • Users 0 members are here
  • accelerometer
  • module
Related

Which Accelerometer Module Should I Use For My Self Balancing Robot ??

saurocksall
saurocksall over 12 years ago

Hi guys..

 

I am making a self balancing robot with Arduino UNO and i am not sure which accelerometer module should i buy, there are many options in the market, as i have not used accelerometers in the past  i am really confused, i want a cheep and easy to use one.. have any of u guys has made a Self Balancing Robot ?? Please help me !!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 12 years ago +2
    Hi Saurabh, For a 2 wheel robot, you only need a single axis accelerometer with a range of about 2 or 3 g. You need to decide if you want to use analog output signals or serial communications with the…
  • ntewinkel
    ntewinkel over 12 years ago +1
    Hi Saurabh, If you're open to using something that is not Arduino, but still very easy to use, maybe have a look at the Freescale FRDM-KL25z board . It is about $14 and includes an on board accelerometer…
Parents
  • ntewinkel
    0 ntewinkel over 12 years ago

    Hi Saurabh,

     

    If you're open to using something that is not Arduino, but still very easy to use, maybe have a look at the Freescale FRDM-KL25z board. It is about $14 and includes an on board accelerometer, as well as extra LEDs, capacitive touch slider, more memory and higher speed compared to the Uno.

     

    I have one here and found it very easy to work with, using mbed.org.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 12 years ago

    Hi Saurabh,

     

    If you're open to using something that is not Arduino, but still very easy to use, maybe have a look at the Freescale FRDM-KL25z board. It is about $14 and includes an on board accelerometer, as well as extra LEDs, capacitive touch slider, more memory and higher speed compared to the Uno.

     

    I have one here and found it very easy to work with, using mbed.org.

     

    Cheers,

    -Nico