Arduino
  • Products
  • More
Arduino
Arduino Forum Toggle switch to push button switch conversion (Arduino or IC logic)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 62 replies
  • Answers 13 answers
  • Subscribers 422 subscribers
  • Views 10841 views
  • Users 0 members are here
  • push
  • toggle
  • trigger
  • button
  • flight
  • switch
  • arduino
  • simulator
Related

Toggle switch to push button switch conversion (Arduino or IC logic)

silviustro
silviustro over 12 years ago

     I would like to build an interface for a flight simulator consisting on various toggle and trigger switches, unfortunately i can't just simply flip a switch to an ON state and leave the signal like that, i need to send a quick pulse every time you toggle the switch ON or OFF, as if you where to push a button on a keyboard to send that command.

 

     In simple words... i need a toggle switch that will produce one pulse when you flip the toggle switch ON. And a second pulse will be generated when the same toggle switch is flipped to OFF. Here is a GIF to better illustrate that... http://www.desktopaviator.com/Products/Model_2120/2120B.gif

 

     If there is a simpler way of doing this without using an Arduino, like an IC or a special toggle swich, I would like to know, otherwise, I plan on using an Arduino to do this.

 

 

Thank you for your time!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 12 years ago +3 suggested
    Hi Silviu, An easy method to produce pulses is to get a 'quad XOR gate' ic. Connecting one input of a gate to 0V makes a simple buffer which does nothing except delay a signal slightly. Do this with three…
  • shabaz
    shabaz over 12 years ago in reply to silviustro +2 suggested
    Hi Silviu, If you want to do it using an Arduino alone, you will need 80 pins for 40 switches and 40 outputs, so that may be unfeasible. Anyway, below is some pseudocode that will do it for (say) 4 switches…
  • jw0752
    jw0752 over 12 years ago in reply to silviustro +2 verified
    Hi Silviu; I have drawn a schematic and added some notes. . Don't worry about right answers as everyone contributes good ideas. If you have clarifying questions let me know. John
Parents
  • silviustro
    0 silviustro over 12 years ago

    Thank you for your answer Shabaz,

     

    I have to say, i did tough of using a logic gate to produce the signal, tho, when you have 40 toggles you need to wire, it becomes inefficient. A tenth of a nanosecond wouldn't be enough, i'd need something like a half second pulse to trigger the command correctly.

     

    Now, is there a way of doing this with an MCU? preferably an Arduino, (something like, if toggle on, then turn on led for one second, then if toggle off, do the same) I'd test it out with an LED, then replace it with an optocoupler. I have done the reverse, making a push button toggle a motor ON and OFF, but even then, i needed help with the code regarding the buffer of the Arduino. (i think using a delay without a loop would work, wouldn't it? the LED would turn on, and then stay off?)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago in reply to silviustro

    Hi Silviu,

    I see that you have marked this question closed but I thought I would throw an old fashioned idea at you anyway. If you are able to use DPDT toggles you could hook them up to reverse the polarity of a capacitor. In this way each time the switch is toggled the capacitor would discharge and recharge creating a current of duration depending on the size of the capacitor. I prototyped a small circuit and was able to get an LED to turn on for one second each time the switch was toggled. If this idea fits your need you could save lots of hardware and programming. If you would like a schematic for the little prototype I put together let me know.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • billpenner
    0 billpenner over 12 years ago in reply to silviustro

    adding to the comments by shabaz ;

     

    The following might of help. Since you are using many switches and apparently need them to be independent,

    you could put all the resistors,capacitors and ICs on a PC board to simplify wiring.

    The ICs are quad XOR gates so each IC will handle four switches.

    The pulse width can be adjusted with R8 and C3. Using the values shown will produce about 1/2 second. The capacitors can be ceramic, which is very small.

    The ICs are available in both the standard dual inline and small form factor.

    I don't know what you are going to drive with the output, so I am not sure if the IC will handle the necessary current.

    Could you let us know where the output of this conversion goes?

     

    Bill

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • silviustro
    0 silviustro over 12 years ago in reply to jw0752

    Hi, John

     

    Thank you very much for your answer! it worked wonderfully... not only that, but i tested it using both ON-OFF-ON and ON-ON switches, and they both worked perfectly, there was no voltage leakage. The idea of linking polarized caps together also worked really nice, thanks for the advice.

     

    I know we have turned this into a live discussion, and i'd like to add a bit of complexity to the design, do you think it would be possible to add LEDs indicating the position of the switch??

     

    I think it would be a bit complex... what do you think?

     

    Thanks, Silviu

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago in reply to silviustro

    Hi Silviu,

     

    I am glad that it worked for you. I am sure it is possible to add LED position indicators. As I mentioned in the schematic point "1" is high when the switch is in one position and low when it is in the other. All we have to do is design a little circuit to detect this and turn on the corresponding LEDS. Are you going to use On-On switches or On-Off-On? I ask since with On-On we can always have one of the two LEDs on and just toggle between them. Keep in mind we have to keep the sensing of point "1" at high impedance or you will get a constant current through your pulse circuit. I haven't done any serious thinking on this but I would guess our best bet, to keep it simple, would be to use some FET transitor switches. One would turn on when its gate is pulled high and the other would turn on when its gate is pulled low. This would involve one N FET and one P FET as well as your 2 LEDS and a couple current limiting resistors. The use of FETs would keep the impedance high enough to not bother the pulse circuit. A word of caution is that if you are pulsing an inductive load we would want to be sure to put a protector diode accross the coil to protect the FETs.  If you wait a couple days and check back here one of the other guys who are almost all better designers than me might have an even better idea.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago in reply to silviustro


    Hi Silviu,

     

    I do not know if your quest for electronics know-how is just for this project or if you have a deeper interest. I am quite old fashioned and where more modern individuals might point you to u-tube videos I would point you towards a book. For example, Practical Electronics for Inventors by Paul Scherz and Simon Monk Edition III has, starting on page 449, a section on Junction field effect transistors of the type that would be usefull for turning your LEDs for switch position on and off. I have found this book very helpful with many of my projects. There is a second edition of the book also available but you would be happier with the third edition.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • silviustro
    0 silviustro over 12 years ago in reply to jw0752

    Hi John,

     

    Thank you once again for your answer, no worries about that, I am quite old fashion myself, and a good book will always be capable of storing immense amounts of knowledge in one convenient place. I will explore ways of achieving what i want testing many methods (regarding the LEDs), but i have to say, that your method of turning the LED for a brief amount of time using the capacitor was the best one i have ever seen.Thank you for your help,


    Silviu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to billpenner

    I need this type of circuit for a pipe organ, but the stop switch is magnetic reed spst.   We need to control the stop input of a sound module which uses pulse on and pulse off.  Any mods to this circuit?  

    Chaim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 12 years ago in reply to e14 Contributor

    Hi Chaim, can you provide a drawing?  I don't know much about organs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to D_Hersey

    Hi

    The stop switch  is nothing more than a big slide switch which uses  an attached bar magnet  sliding in close proximity to a enclosed reed switch.  The switch does nothing more than to supply 12 or so volts dc to an input board which eventually will turn on the mechanics and electronics of a pipe chest.     My problem is we have a sound module where the stops are turned on and off by a momentary push button contact.  There were external terminals added to do the same function by remote wiring.   The late organs are control the stops or voices by this method even with these stop knobs.   But they are nothing more than momentary contact switchs which activate when the knob is pulled or deactivated when the knob is pushed, and is on a spring return with an indicator lamp inside.    We want to control this box with the original stop mechanisms on the organ console.  So far I cannot figure a circuit which would be able to give me 2 states--an on state and an off state.   The on state is easy, it is when the voltage is removed how does that get translated to a pulse to trigger the box to shut the stop off?  The pulse width can be 500ms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 12 years ago in reply to e14 Contributor

    Still not clear on this, could this be your ticket?

     

    http://www.fairchildsemi.com/ds/MM/MM74C221.pdf

    http://www.fairchildsemi.com/an/AN/AN-138.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to D_Hersey

    Thanks Don.  I will experiment with this also.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to D_Hersey

    Thanks Don.  I will experiment with this also.