Arduino
  • Products
  • More
Arduino
Arduino Forum Toggle switch to push button switch conversion (Arduino or IC logic)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 62 replies
  • Answers 13 answers
  • Subscribers 422 subscribers
  • Views 10913 views
  • Users 0 members are here
  • push
  • toggle
  • trigger
  • button
  • flight
  • switch
  • arduino
  • simulator
Related

Toggle switch to push button switch conversion (Arduino or IC logic)

silviustro
silviustro over 12 years ago

     I would like to build an interface for a flight simulator consisting on various toggle and trigger switches, unfortunately i can't just simply flip a switch to an ON state and leave the signal like that, i need to send a quick pulse every time you toggle the switch ON or OFF, as if you where to push a button on a keyboard to send that command.

 

     In simple words... i need a toggle switch that will produce one pulse when you flip the toggle switch ON. And a second pulse will be generated when the same toggle switch is flipped to OFF. Here is a GIF to better illustrate that... http://www.desktopaviator.com/Products/Model_2120/2120B.gif

 

     If there is a simpler way of doing this without using an Arduino, like an IC or a special toggle swich, I would like to know, otherwise, I plan on using an Arduino to do this.

 

 

Thank you for your time!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 12 years ago +3 suggested
    Hi Silviu, An easy method to produce pulses is to get a 'quad XOR gate' ic. Connecting one input of a gate to 0V makes a simple buffer which does nothing except delay a signal slightly. Do this with three…
  • shabaz
    shabaz over 12 years ago in reply to silviustro +2 suggested
    Hi Silviu, If you want to do it using an Arduino alone, you will need 80 pins for 40 switches and 40 outputs, so that may be unfeasible. Anyway, below is some pseudocode that will do it for (say) 4 switches…
  • jw0752
    jw0752 over 12 years ago in reply to silviustro +2 verified
    Hi Silviu; I have drawn a schematic and added some notes. . Don't worry about right answers as everyone contributes good ideas. If you have clarifying questions let me know. John
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    so referring to the question regarding using a simple reed switch, why cant you do this or something like it

    image

    when switch is made, then the power is applied through the LED which turns on, you get a pulse while cap charges

    when you release reed, power is removed, LED and resistor discharges quicker then the leg with Cap and therefore you get another pulse

     

    you may need to play with values to get it to the right timing but this or a variation of it should work ?

     

    you could even remove the top resistor, not sure why it is needed anyway

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    so referring to the question regarding using a simple reed switch, why cant you do this or something like it

    image

    when switch is made, then the power is applied through the LED which turns on, you get a pulse while cap charges

    when you release reed, power is removed, LED and resistor discharges quicker then the leg with Cap and therefore you get another pulse

     

    you may need to play with values to get it to the right timing but this or a variation of it should work ?

     

    you could even remove the top resistor, not sure why it is needed anyway

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • phoenixcomm
    0 phoenixcomm over 12 years ago in reply to Robert Peter Oakes

    my G-d you guys like to work..  image image

    if you are going to do a de-bounce circuit, please use something that was designed for this job!! dont rebuild the darn world!! you should look at the lowly 74xx14  http://www.ti.com/lit/ds/symlink/sn74hc14.pdf this is Schmidt trigger.. you can also use a 555 but that cost more!!  ~~ Cris H. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to phoenixcomm

    please look through the thread carefully, it is not a de-bounce circuit, it is designed to give a pulse out when you close the switch and also a pulse when you open the switch

     

    I agree if the poster wanted a de-bounce circuit then your hardware solution would work well but that is not what there looking for.

     

    Regards

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 12 years ago in reply to Robert Peter Oakes

    duh peter,  If the switch was a spdt add another trigger and or tie the outputs!!!  fin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to phoenixcomm

    Hi

    As I mentioned,  we examined the stop switch and found there are provisions to mount a reed switch midtravel, so all that is necessary is to add a pair of wires from each stop switch to its respective terminal pair on the sound module.  But in the process I have been able to tap some great minds.  I thank all of you for that.   IT may be better to go this route as the process is easily reversible when real pipes are installed, and the original stop and driver circuit is still intact.  But we will check out the devices and circuits to give our budding technician and BSEE graduate more in-depth knowledge for future application.

    Chaim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • billpenner
    0 billpenner over 12 years ago in reply to e14 Contributor

    OK but the pulse width will be determined by how fast the stop switch is moved and there will be no indication of the position(on or off stop.

    Bill

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Hi  What would be the IC needed

    CHAim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • silviustro
    0 silviustro over 12 years ago in reply to e14 Contributor

    I never expected this thread to escalate so much! it seems there are a lot of people in search for a non MCU related way of achieving the toggle switch to momentary switch conversion.

     

    For some reason, I think Bills' method (even tho rudimentary) works better than the XOR method, but it is just my opinion, as it uses basic components and it does not involve any ICs.

     

    Tho, for applications like yours, it would be best to use the XOR method, as the capacitor method would not work using a normal switch.