Arduino
  • Products
  • More
Arduino
Arduino Forum Toggle switch to push button switch conversion (Arduino or IC logic)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 62 replies
  • Answers 13 answers
  • Subscribers 422 subscribers
  • Views 10903 views
  • Users 0 members are here
  • push
  • toggle
  • trigger
  • button
  • flight
  • switch
  • arduino
  • simulator
Related

Toggle switch to push button switch conversion (Arduino or IC logic)

silviustro
silviustro over 12 years ago

     I would like to build an interface for a flight simulator consisting on various toggle and trigger switches, unfortunately i can't just simply flip a switch to an ON state and leave the signal like that, i need to send a quick pulse every time you toggle the switch ON or OFF, as if you where to push a button on a keyboard to send that command.

 

     In simple words... i need a toggle switch that will produce one pulse when you flip the toggle switch ON. And a second pulse will be generated when the same toggle switch is flipped to OFF. Here is a GIF to better illustrate that... http://www.desktopaviator.com/Products/Model_2120/2120B.gif

 

     If there is a simpler way of doing this without using an Arduino, like an IC or a special toggle swich, I would like to know, otherwise, I plan on using an Arduino to do this.

 

 

Thank you for your time!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 12 years ago +3 suggested
    Hi Silviu, An easy method to produce pulses is to get a 'quad XOR gate' ic. Connecting one input of a gate to 0V makes a simple buffer which does nothing except delay a signal slightly. Do this with three…
  • shabaz
    shabaz over 12 years ago in reply to silviustro +2 suggested
    Hi Silviu, If you want to do it using an Arduino alone, you will need 80 pins for 40 switches and 40 outputs, so that may be unfeasible. Anyway, below is some pseudocode that will do it for (say) 4 switches…
  • jw0752
    jw0752 over 12 years ago in reply to silviustro +2 verified
    Hi Silviu; I have drawn a schematic and added some notes. . Don't worry about right answers as everyone contributes good ideas. If you have clarifying questions let me know. John
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to D_Hersey

    Hi

    We will experiment with this circuit also.  However we changed the input resistors to the IC to 100k and ran 560 ohm resistor to common omitting the LED.   The output is connected to optoisolator .  The  circuit works fine   . input goes high-ouput pulse; power removed-output pulse.  We  tried it with our stock sliding stop switch with reed switch and debounce circuit and works well.   We wanted to make sure that when organ is depowered  and repowered there are no pulses generated , and that seems to be the case.   We needed to explore this as some organs now use pulsed stop switching instead of steady state; and we needed to be able to go from one format to another  as we have an upcoming project to control a sound module.

    Thanks again.   We will build this circuit provided by Don and inform you of the results

    Chaim.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to D_Hersey

    Hi

    We will experiment with this circuit also.  However we changed the input resistors to the IC to 100k and ran 560 ohm resistor to common omitting the LED.   The output is connected to optoisolator .  The  circuit works fine   . input goes high-ouput pulse; power removed-output pulse.  We  tried it with our stock sliding stop switch with reed switch and debounce circuit and works well.   We wanted to make sure that when organ is depowered  and repowered there are no pulses generated , and that seems to be the case.   We needed to explore this as some organs now use pulsed stop switching instead of steady state; and we needed to be able to go from one format to another  as we have an upcoming project to control a sound module.

    Thanks again.   We will build this circuit provided by Don and inform you of the results

    Chaim.