Arduino
  • Products
  • More
Arduino
Arduino Forum Help, my Processing code is restarting my Arduino code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 35 replies
  • Answers 1 answer
  • Subscribers 420 subscribers
  • Views 4144 views
  • Users 0 members are here
Related

Help, my Processing code is restarting my Arduino code

kjhart0133
kjhart0133 over 12 years ago

Hello all,

I'm developing some Arduino code using XBees to sense environmental data at a remote location. My Arduino code is working great and I'm now ready to upload my remotely acquired data to my computer so that I can parse the data and send it via an SMS message to my smart phone. This way I can monitor my remote location from anywhere.

I'm using a chunk of code I got from the "Getting Started with Processing" book by Reas and Fry. I am able to get the Arduino/XBee data into my computer this way, but I have a problem/issue:

The Arduino code loops continually, but each time I start the Processing Code, it restarts (resets?) the Arduino code. The Arduino code starts over from the beginning going through setup and then into the loop. I have no idea why this is happening. Here is the Processing code I'm using:

// Based on Example 11-07 from "Getting Started with Processing"

// by Reas & Fry. O'Reilly / Make 2010

// This sketch, as modified by kjh, reads data from an Arduino, stores it in an array

// then saves the data to a file on disk.

 

import processing.serial.*;

 

Serial port;                     // Create object from Serial class

int asize = 8;                 // define size of data array

byte[] val = new byte[asize];    // Data received from the serial port

                                 // representing the setting of the pot

int i = 0;                       // array index

int x;                           // scratch value

float y;

 

void setup() {

  //size(440, 220);

  // IMPORTANT NOTE:

  // The first serial port retrieved by Serial.list()

  // should be your Arduino. If not, uncomment the next

  // line by deleting the // before it. Run the sketch

  // again to see a list of serial ports. Then, change

  // the 0 in between [ and ] to the number of the port

  // that your Arduino is connected to.

  println(Serial.list());

  String arduinoPort = Serial.list()[2];

  port = new Serial(this, arduinoPort, 9600);

}

 

void draw() {

    if (port.available() > 0) {        // If data is available,

      x = port.read();        // read it and store it in val

      val[i] = byte(x);

      y =  float(x);

      //println(y);

      println(val[i]);

      //val = map(val, 0, 255, 0, height);  // Convert the value

      i++;

    }

    if (i > asize-1){

      saveBytes("arduino_data.dat", val);

      println("Data written.");

      exit();

    }

}

My Arduino code does not read data from the computer or Processing, it only sends data to Processing. The Arduino code is quite long and involved using a fair amount of XBee interface code so I didn't include it here. But, as I said, it is running fine except for being restarted each time I run the Processing code.  I'm using an Mega Arduino board connected to my PC via the USB cable. 

I greatly appreciate any assistance on this.

Thanks,

Kevin H.

  • Sign in to reply
  • Cancel

Top Replies

  • kjhart0133
    kjhart0133 over 12 years ago in reply to mcb1 +1
    Success!! After trying a number of different things without solving the problem, I finally cut the jumper on the reset line between the USART and the Mega chip and this did the trick. These forums are…
  • kjhart0133
    kjhart0133 over 12 years ago in reply to kjhart0133 +1
    To solve the problem of now not being able to upload sketches, I soldered a wire to each of the reset line solder pads and wired an SPST switch across the two solder pads. This works perfectly (so far…
  • kjhart0133
    kjhart0133 over 12 years ago in reply to Robert Peter Oakes +1
    Peter, That's great info about the ports. I'm learning a lot in this thread. Here's a block diagram of my system that shows all the components. I run Processing code in the PC that uploads data from the…
Parents
  • ipv1
    0 ipv1 over 12 years ago

    The XBee CTS pin is usually wired to the reset pin of the arduino... This has caused some havoc in my past projects...

    Lemme know if this is a possible issue.

    Cheers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • kjhart0133
    0 kjhart0133 over 12 years ago in reply to ipv1

    Mr. Singh, I think you have hit the nail on the head.  I hooked up an oscilloscope to the reset/ line on the Mega and observed that each time I started my Processing code the reset/ line was asserted low!!  Looking at the Arduino Mega schematic, it clearly shows the Mega's USART chip's CTS/ line wired to the ATmega chip's reset line.  Apparently, when the Processing code wants to read data on the Serial/USB port it sends control packets to the Mega's USART that somehow assert the Mega's CTS/ line low.  I've included a picture of the reset line being asserted when I run the Processing code.  This happens each time I start the Processing code.

     

    I guess my question now is: what do I do next?  Is there a way to 'turn off' the CTS/RTS flow control on the Mega?  The data sheet for the ATmega16u  USB controller shows a register, UCSRnD, that has a CTSEN (CTS enable) bit, but that register name is not recognized by the Arduino compiler so I don't know how to turn that enable bit off, or if that would even solve the problem.

     

    Any suggestions are appreciated.

     

    Thanks,

     

    Kevin H.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kjhart0133
    0 kjhart0133 over 12 years ago in reply to ipv1

    Mr. Singh, I think you have hit the nail on the head.  I hooked up an oscilloscope to the reset/ line on the Mega and observed that each time I started my Processing code the reset/ line was asserted low!!  Looking at the Arduino Mega schematic, it clearly shows the Mega's USART chip's CTS/ line wired to the ATmega chip's reset line.  Apparently, when the Processing code wants to read data on the Serial/USB port it sends control packets to the Mega's USART that somehow assert the Mega's CTS/ line low.  I've included a picture of the reset line being asserted when I run the Processing code.  This happens each time I start the Processing code.

     

    I guess my question now is: what do I do next?  Is there a way to 'turn off' the CTS/RTS flow control on the Mega?  The data sheet for the ATmega16u  USB controller shows a register, UCSRnD, that has a CTSEN (CTS enable) bit, but that register name is not recognized by the Arduino compiler so I don't know how to turn that enable bit off, or if that would even solve the problem.

     

    Any suggestions are appreciated.

     

    Thanks,

     

    Kevin H.