Arduino Forum Using serial communication without pc
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
  • State Suggested Answer
  • Replies 35 replies
  • Answers 5 answers
  • Subscribers 403 subscribers
  • Views 5237 views
  • Users 0 members are here
  • arduino
Related

Using serial communication without pc

Former Member
Former Member over 11 years ago

I just started using the arduino and tried to build a remote control car. I have used the 434MHz RF module for radio transmission. I made a program for both remote and the receiver in the car, it worked fine when I tested it using my pc to send and receive signals. since I used the serial communication, it didn't work when I disconnected the arduinos from my pc. Is there a way to use the serial communication even when it is not connected to the pc, if it can be done, please suggest a way to do so.

  • Sign in to reply
  • Cancel

Top Replies

  • alexev
    alexev over 11 years ago in reply to Former Member +1
    There are many considerations to take in account: -instead of using "serial.print" which is a display command, try using "serial.write" to transmit data ( http://arduino.cc/en/Serial/Print#.UyoIPIXPsvw…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to elizabethmath +1 suggested
    I just checked with a sketch The serial lights TX or RX do not flicker when the USB is not connected, you can see that the USB Controller knows when the USB is connected and also that the lights are controlled…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to elizabethmath +1 suggested
    How were yo planning on using the scanner in the original design without the PC ? Suggestions would be LCD Display either attached via I2C or even via the hardware serial port but connected to pins 0,1…
Parents
  • D_Hersey
    0 D_Hersey over 9 years ago

    Doing a moments digging on the interweb tells me that 'volatile' also retards automatic p-code optimization.  If I were to type something like:

     

    int N =0;

    while (N != Magic_Number_1){}

     

    when N is asynchronously and independently loaded by another thread or the I/O subsystem, the optomiser might be fooled into interpreting this as:

     

    while(1){}

     

    so,

     

    volatile int N =0;

     

    prevents this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 9 years ago

    Doing a moments digging on the interweb tells me that 'volatile' also retards automatic p-code optimization.  If I were to type something like:

     

    int N =0;

    while (N != Magic_Number_1){}

     

    when N is asynchronously and independently loaded by another thread or the I/O subsystem, the optomiser might be fooled into interpreting this as:

     

    while(1){}

     

    so,

     

    volatile int N =0;

     

    prevents this.