Arduino Forum Using serial communication without pc
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
  • State Suggested Answer
  • Replies 35 replies
  • Answers 5 answers
  • Subscribers 403 subscribers
  • Views 5237 views
  • Users 0 members are here
  • arduino
Related

Using serial communication without pc

Former Member
Former Member over 11 years ago

I just started using the arduino and tried to build a remote control car. I have used the 434MHz RF module for radio transmission. I made a program for both remote and the receiver in the car, it worked fine when I tested it using my pc to send and receive signals. since I used the serial communication, it didn't work when I disconnected the arduinos from my pc. Is there a way to use the serial communication even when it is not connected to the pc, if it can be done, please suggest a way to do so.

  • Sign in to reply
  • Cancel

Top Replies

  • alexev
    alexev over 11 years ago in reply to Former Member +1
    There are many considerations to take in account: -instead of using "serial.print" which is a display command, try using "serial.write" to transmit data ( http://arduino.cc/en/Serial/Print#.UyoIPIXPsvw…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to elizabethmath +1 suggested
    I just checked with a sketch The serial lights TX or RX do not flicker when the USB is not connected, you can see that the USB Controller knows when the USB is connected and also that the lights are controlled…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to elizabethmath +1 suggested
    How were yo planning on using the scanner in the original design without the PC ? Suggestions would be LCD Display either attached via I2C or even via the hardware serial port but connected to pins 0,1…
Parents
  • alexev
    0 alexev over 11 years ago

    You're a bit confusing, serial communication means sending data on a single communication channel bit by bit, hence it's name. Usb also does serial communication as rs232 but at a way faster rates and using different protocols. You want your robot to be controlled from a computer or from a remote control? If you want to get rid of your arduino's and just use the microcontrollers (atmega328), well you can either way (pc or remote), you just have to adapt the software on both microcontrollers and setup the fuses for external clock to use without arduino boards. Here's a useful link Arduino - ArduinoToBreadboard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to alexev

    Thank you sir, the link was helpful. I wanted to use my arduino as remote control and receiver on the car which works without a computer. I want my robot to be controlled by a remote control. Sorry for the confusion with the serial communication, I just wanted to tell about the Serial.print and Serial.read commands.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexev
    0 alexev over 11 years ago in reply to Former Member

    There are many considerations to take in account:

    -instead of using "serial.print" which is a display command, try using "serial.write" to transmit data (http://arduino.cc/en/Serial/Print#.UyoIPIXPsvw)

    -have you used the virtualwire library?

    -it's well known that cheap 434MHz rf modules are "what you pay is what you get" so you might aswell get delays and corrupted transmission from them even with the increase of the length of the antenna, when you have obstacles and interference. Don't expect large distances operations, these modules work in amplitude shift keying for low performance applications (http://en.wikipedia.org/wiki/Amplitude-shift_keying)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • elizabethmath
    0 elizabethmath over 9 years ago in reply to alexev

    Hi,

    Sorry, I'm quite new to the arduino( and electronic) platform, so apologies in advance if my queries seem silly.

    But does that mean i would need to replace the serial.print commands with serial.write or since I would no longer require the laptop interface, can I just get rid of all the serial.print commands in my code?

     

    I am working on getting rid of my laptop interface and just uploading the code onto my arduino board. unfortunately, even after getting rid of all the serial.print commands while retaining all the other essential parts of the code, I dont seem to have it working without the usb to pc connection.

    May I know what I'm doing wrong? Am I expected to ADD certain code now ( like the serial.write command) into my code now?

     

    Many thanks for any help with regard to me query! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • neilk
    0 neilk over 9 years ago in reply to elizabethmath

    Hi elizabethmath

     

    I think we need to know a little bit more about what you are trying to do with your Arduino program.

     

    A block diagram and/or your code would be very helpful.

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to elizabethmath

    Please provide the sketch your using,

     

    There is no reason you need the PC connected to run you sketch but there may be something in you code that will help us to help you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • elizabethmath
    0 elizabethmath over 9 years ago in reply to neilk

    Hi,

    Thank you so very much for taking time out to assist me with this. I really appreciate the help!

     

    image

    imageimageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • elizabethmath
    0 elizabethmath over 9 years ago in reply to neilk

    Hi,

    Thank you so very much for taking time out to assist me with this. I really appreciate the help!

     

    image

    imageimageimageimage