Arduino Forum Using serial communication without pc
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
  • State Suggested Answer
  • Replies 35 replies
  • Answers 5 answers
  • Subscribers 403 subscribers
  • Views 5238 views
  • Users 0 members are here
  • arduino
Related

Using serial communication without pc

Former Member
Former Member over 11 years ago

I just started using the arduino and tried to build a remote control car. I have used the 434MHz RF module for radio transmission. I made a program for both remote and the receiver in the car, it worked fine when I tested it using my pc to send and receive signals. since I used the serial communication, it didn't work when I disconnected the arduinos from my pc. Is there a way to use the serial communication even when it is not connected to the pc, if it can be done, please suggest a way to do so.

  • Sign in to reply
  • Cancel

Top Replies

  • alexev
    alexev over 11 years ago in reply to Former Member +1
    There are many considerations to take in account: -instead of using "serial.print" which is a display command, try using "serial.write" to transmit data ( http://arduino.cc/en/Serial/Print#.UyoIPIXPsvw…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to elizabethmath +1 suggested
    I just checked with a sketch The serial lights TX or RX do not flicker when the USB is not connected, you can see that the USB Controller knows when the USB is connected and also that the lights are controlled…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to elizabethmath +1 suggested
    How were yo planning on using the scanner in the original design without the PC ? Suggestions would be LCD Display either attached via I2C or even via the hardware serial port but connected to pins 0,1…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Can you provide a block diagram of what your describing, ie. do you have two arduino's one in the car and one for the remote control, both with radios , the one in the car connected to the speed and steering im assuming with PWM control. the other with buttons or something to act as user controls because without the connection to the PC there is no commands going to the transmitter.

     

    also (And sorry if this is obvious), if the one connected to the PC was powered by the PC then it wont have power once disconnected ?

     

    hence a block diagram would help us help you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Can you provide a block diagram of what your describing, ie. do you have two arduino's one in the car and one for the remote control, both with radios , the one in the car connected to the speed and steering im assuming with PWM control. the other with buttons or something to act as user controls because without the connection to the PC there is no commands going to the transmitter.

     

    also (And sorry if this is obvious), if the one connected to the PC was powered by the PC then it wont have power once disconnected ?

     

    hence a block diagram would help us help you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to Robert Peter Oakes

    image

    This is the block diagram of the system I wanted to build. the remote control contains the buttons I require and the receiver end is mounted on my car.

    I used the command Serial.print to transmit the data and the command Serial.read to receive the data. These two commands work only when the serial monitors are open. I wanted to know if there is a way to use these two commands without keeping the serial monitor open.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Former Member

    What are the radio modules and also the Arduino models, there are many alternatives but I would be reluctant  to say without knowing what your working with

     

    And to answer your original question, yes there is a way to do it without the PC connected, just need the info requested to get it right for you

     

    Thanks