Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino and Transistors Question - RE: School Musical Production
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 126 replies
  • Answers 2 answers
  • Subscribers 421 subscribers
  • Views 11040 views
  • Users 0 members are here
  • raspberry
  • transistor
  • pi
  • arduino
Related

Arduino and Transistors Question - RE: School Musical Production

wallarug
wallarug over 12 years ago

One of the directors has asked me to create a special backdrop for our college musical. This particular backdrop has a particular design (see below) that includes LED strip lighting to give the feel of a 1920s casino sign – similar to what is seen today in Las Vegas.

I  have done up a detailed design for this sign, based off the rough sketch given to me by the director and the dimensions of the backdrop.  On this diagram, the arrangement of the LED strip lighting can be seen.

image

          

The LED Strip lighting that will be bought for this project will be sourced from Jaycar – “Low Cost 5m Flexible Adhesive LED Strip Light – Warm White” (ZD0577).  According to the specifications off Jaycar’s website, these LED lights need 1.1 Amps per metre @ 12 volts.  This means that the longest segments of lights need 1.1 * 1.5 = 1.65 Amps of power (rounded up by 20% for safety: 2.0 Amps @ 12 volts).

 

This would not be an issue if I was just turning these LED Strips on and off with mains power BUT I want to control these LEDs via an Arduino, so that they can do fancy things like flash and chase.  That means that I would need a circuit to control these lights with an Arduino so that everything remains safe and does not blow up.

I have come up with this circuit (below) using a couple of NPN transistors and two power supplies.  In the diagram below, I am aware that the transistor pinouts are EBC.  The ones I am going to buy have a pinout of BCE.

 

image

 

The only problem with this is that I have very little understanding of transistor circuits.  What this circuit has to be able to do is:

  • Using the smallest amount of current from the Arduino (at 5 volts) or a Raspberry Pi (3v3 volts), turn on the circuit to allow the 12 volts that powers the LED strip lighting to flow.

 

I was thinking of using either TIP41C NPN Transistors (in a darlington Array) or TIP122 NPN transistors.

 

This circuit will be replicated 8 times over to accommodate for the number of LEDs I am controlling.

 

 

Can anyone help me:

  1. Design a circuit that will work 100% and will be safe (ie: low heat)
    1. This includes base resistance
  1. Confirm which transistors I should be using for this project.

 

Any help will be much appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Sorry the one I suggested wont work, but this one should http://www.jaycar.com.au/productView.asp?ID=ZK8821 10+ current rating and at 0.016ohms it should be good for your needs pdf here http://www.vishay…
  • mcb1
    mcb1 over 12 years ago in reply to jw0752 +1
    John If you are referring to this It means that at a gate voltage of 1.6 typ, a current of 250uA will be flowing in the Drain. If you look here, you can see that from 3 to 3.3v will give you enough to…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Solenoid Whapper:
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    If you want to drive the strips easily then using a logic level FET will work the easiest for you

     

    something like this, a few K gate resistor would be all thats needed between the Arduino and the FET

    http://canada.newark.com/fairchild-semiconductor/fdp7030bl/n-channel-mosfet-30v-60a-to-220/dp/38C7149

     

    and with your loads they will not require heat sinks as the on resistance is only 0.009ohms so even at 60Amps thats only 0.6W so at 2 Amps its only 0.02W.

     

    now you mention running and other patterns, if your using all one color strips running on 12 V then the whole strip will be on or off, or using PWM any brightness in between

     

    if you use strips that have LEDs like WS2812B then you dont need drivers, they will work on 5V and you can make any LED be any color and intensity you like (Yes, every individual LED)

     

    AdaFruit sell them under the brand of NEOPixel https://learn.adafruit.com/adafruit-neopixel-uberguide

     

    you can also get LED strips that are RGB so you can change the strip color but all the strip will be the same

     

    either way, with the exception of the strips with the WS2811/12 LEDs, the FET I linked in will work easily for you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    If you want to drive the strips easily then using a logic level FET will work the easiest for you

     

    something like this, a few K gate resistor would be all thats needed between the Arduino and the FET

    http://canada.newark.com/fairchild-semiconductor/fdp7030bl/n-channel-mosfet-30v-60a-to-220/dp/38C7149

     

    and with your loads they will not require heat sinks as the on resistance is only 0.009ohms so even at 60Amps thats only 0.6W so at 2 Amps its only 0.02W.

     

    now you mention running and other patterns, if your using all one color strips running on 12 V then the whole strip will be on or off, or using PWM any brightness in between

     

    if you use strips that have LEDs like WS2812B then you dont need drivers, they will work on 5V and you can make any LED be any color and intensity you like (Yes, every individual LED)

     

    AdaFruit sell them under the brand of NEOPixel https://learn.adafruit.com/adafruit-neopixel-uberguide

     

    you can also get LED strips that are RGB so you can change the strip color but all the strip will be the same

     

    either way, with the exception of the strips with the WS2811/12 LEDs, the FET I linked in will work easily for you