Arduino Forum Arduino and Transistors Question - RE: School Musical Production
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
  • State Verified Answer
  • Replies 126 replies
  • Answers 2 answers
  • Subscribers 402 subscribers
  • Views 7607 views
  • Users 0 members are here
  • raspberry
  • transistor
  • pi
  • arduino
Related

Arduino and Transistors Question - RE: School Musical Production

wallarug
wallarug over 11 years ago

One of the directors has asked me to create a special backdrop for our college musical. This particular backdrop has a particular design (see below) that includes LED strip lighting to give the feel of a 1920s casino sign – similar to what is seen today in Las Vegas.

I  have done up a detailed design for this sign, based off the rough sketch given to me by the director and the dimensions of the backdrop.  On this diagram, the arrangement of the LED strip lighting can be seen.

image

          

The LED Strip lighting that will be bought for this project will be sourced from Jaycar – “Low Cost 5m Flexible Adhesive LED Strip Light – Warm White” (ZD0577).  According to the specifications off Jaycar’s website, these LED lights need 1.1 Amps per metre @ 12 volts.  This means that the longest segments of lights need 1.1 * 1.5 = 1.65 Amps of power (rounded up by 20% for safety: 2.0 Amps @ 12 volts).

 

This would not be an issue if I was just turning these LED Strips on and off with mains power BUT I want to control these LEDs via an Arduino, so that they can do fancy things like flash and chase.  That means that I would need a circuit to control these lights with an Arduino so that everything remains safe and does not blow up.

I have come up with this circuit (below) using a couple of NPN transistors and two power supplies.  In the diagram below, I am aware that the transistor pinouts are EBC.  The ones I am going to buy have a pinout of BCE.

 

image

 

The only problem with this is that I have very little understanding of transistor circuits.  What this circuit has to be able to do is:

  • Using the smallest amount of current from the Arduino (at 5 volts) or a Raspberry Pi (3v3 volts), turn on the circuit to allow the 12 volts that powers the LED strip lighting to flow.

 

I was thinking of using either TIP41C NPN Transistors (in a darlington Array) or TIP122 NPN transistors.

 

This circuit will be replicated 8 times over to accommodate for the number of LEDs I am controlling.

 

 

Can anyone help me:

  1. Design a circuit that will work 100% and will be safe (ie: low heat)
    1. This includes base resistance
  1. Confirm which transistors I should be using for this project.

 

Any help will be much appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    Sorry the one I suggested wont work, but this one should http://www.jaycar.com.au/productView.asp?ID=ZK8821 10+ current rating and at 0.016ohms it should be good for your needs pdf here http://www.vishay…
  • mcb1
    mcb1 over 11 years ago in reply to jw0752 +1
    John If you are referring to this It means that at a gate voltage of 1.6 typ, a current of 250uA will be flowing in the Drain. If you look here, you can see that from 3 to 3.3v will give you enough to…
  • D_Hersey
    D_Hersey over 11 years ago +1
    Solenoid Whapper:
Parents
  • wallarug
    0 wallarug over 11 years ago

    Board is built and tested with 5 volts and 9 volts - no issues thus far.

     

    I am going to conduct further testing tomorrow.

     

    Images below:

    image

    image

    image

     

    Quick Question:

    1.  Do the LED strip sections need to have the pads shorted in order for the lights to work?

    When I first tested them, it seemed that I had to have a wire across the top + and - metallic pad to get it to work.  Yet when I tried it a second time I didn't need it?  Any ideas / experience?

     

    LED Strips: see metalic pads.

    image

     

    BTW:  I have not yet added in the NPN base resistor, I will do that tomorrow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 11 years ago in reply to wallarug

    Hey Guys!

     

    I forgot to thank you all so much for your efforts in this project.  It worked BRILLIANTLY!!  The Director and the audience were amazed at such a wonderful set backdrop.  It could not have been done without all of your help.  Special thanks goes to: John Alexander, Douglas, and Peter.

     

    Here is a video of the set backdrop while we were testing it.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    ...and one of it on the stage with the other production lights on ( 9 x 1200W pacifics + 6 x LED PARs ).  From this video you can see it was VERY VERY bright.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

     

    Once the production was complete, myself and a friend decided to attach a Raspberry Pi to it and using the 'lightshowpi' software were able to sync the LEDs to the music.  Very fun indeed.  The board did not break at any stage.  The temperature off the board (MOSFETs, etc.) was not noticeable even under such stresses put on it by the software.  The videos of that are on the same youtube channel (cmdenterprises) if you have some time to enjoy them.

     

    I hope to do a write up on this project one day so that others can do similar projects or learn by doing like I have done.

     

    Thank you again to everyone on E14 who made this happen.  You left a lot of people amazed on show night!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wallarug
    0 wallarug over 11 years ago in reply to wallarug

    Hey Guys!

     

    I forgot to thank you all so much for your efforts in this project.  It worked BRILLIANTLY!!  The Director and the audience were amazed at such a wonderful set backdrop.  It could not have been done without all of your help.  Special thanks goes to: John Alexander, Douglas, and Peter.

     

    Here is a video of the set backdrop while we were testing it.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    ...and one of it on the stage with the other production lights on ( 9 x 1200W pacifics + 6 x LED PARs ).  From this video you can see it was VERY VERY bright.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

     

    Once the production was complete, myself and a friend decided to attach a Raspberry Pi to it and using the 'lightshowpi' software were able to sync the LEDs to the music.  Very fun indeed.  The board did not break at any stage.  The temperature off the board (MOSFETs, etc.) was not noticeable even under such stresses put on it by the software.  The videos of that are on the same youtube channel (cmdenterprises) if you have some time to enjoy them.

     

    I hope to do a write up on this project one day so that others can do similar projects or learn by doing like I have done.

     

    Thank you again to everyone on E14 who made this happen.  You left a lot of people amazed on show night!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to wallarug

    Wow, nice show

     

    I am so glad it all worked out for you and everyone was happy with the result

     

    Only too happy to have been able to assist you with this, you know where we are for the next one

     

    Regards and Congrats

     

    Peter