Arduino
  • Products
  • More
Arduino
Arduino Forum Handheld transmitter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 421 subscribers
  • Views 1858 views
  • Users 0 members are here
Related

Handheld transmitter

royston02
royston02 over 12 years ago

I see many people build wireless reciver for electric skateboards and wanted to build one which could be controlled by a phone(android) and a handheld reciver. A few questions:

-How to make one like this(wireless)?

https://s3.amazonaws.com/ksr/assets/002/032/858/34c0fa6478a0d319f5b712b27be07e5d_large.jpg?1400567936

-Can I use a bluethoot module for the handheld reciver or will it intefere with the signals send to the phone(one will be on the skateboard)?

It's my diy project because I like skateboardsimage.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    An example of a very simple transmitter / receiver could be based on the TI Booster Pack (CC110L Booster sub 1GHz radio) http://www.ti.com/tool/430boost-cc110l this has a simple to use transmitter on a…
Parents
  • gihu
    0 gihu over 12 years ago

    Hi,

     

    I am not sure if I get the idea. But I think you could use bluetooth, so a module like RN42XV could be conected to the arduino in the skate. Then through an app in an Android phone you will be able to control the skate.

     

    Just as an example:

    http://forcetronic.blogspot.com.es/2014/04/building-bluetooth-remote-control-car.html

    You could adapt the receiver part for your skate instead for an RC car.

    And for the transmitter just an app in an Android phone.

     

    Does it fit the idea?

     

    In fact, in this case, there is no receiver neither transmitter, both sides are transceiver, so you can get parameters, as for example, speed, battery status... from the skate to the app.

     

    One big inconvenience, do not fall down and hurt your mobile... image

     

    Hope that helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gihu
    0 gihu over 12 years ago

    Hi,

     

    I am not sure if I get the idea. But I think you could use bluetooth, so a module like RN42XV could be conected to the arduino in the skate. Then through an app in an Android phone you will be able to control the skate.

     

    Just as an example:

    http://forcetronic.blogspot.com.es/2014/04/building-bluetooth-remote-control-car.html

    You could adapt the receiver part for your skate instead for an RC car.

    And for the transmitter just an app in an Android phone.

     

    Does it fit the idea?

     

    In fact, in this case, there is no receiver neither transmitter, both sides are transceiver, so you can get parameters, as for example, speed, battery status... from the skate to the app.

     

    One big inconvenience, do not fall down and hurt your mobile... image

     

    Hope that helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to gihu

    My kids break enough phones without being on a skate  board while trying to use it, I would definelty recommend a way cheaper controller ... I mean, think about it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to Robert Peter Oakes

    Jibx,

    I am more concerened about the handheld transmitter than the bluethoot stuff.

    Gihu,

    Thanks for the reply, exactly what I was looking fo but in a different menner. The one youposted was wide. I wanted something thin. For exampe, take your walkman/walking stick and hold it. That's how less thick it should be.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to royston02

    for a prototype what I proposed will work

     

    If it pans out then simply get a board made to the dimensions you need, with everything on the single board.

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to Robert Peter Oakes

    My irritation is what type of battery shall be used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to royston02

    Since power conumption is 5Vs and the battery should have a charging circuit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to royston02

    3v3 so a lithium ION battery of 4.2V max (3.7 nominal) therefore any usb charger as a source and a very inexpensive single cell LION charger chip / board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to Robert Peter Oakes

    It(transmitter) takes 5Vs and step up regulators are inefficient!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to royston02

    Funnily enough the Wireless Nintendo Wii Nunchuck, uses an internal Lipo battery and is 3v3 electronics.

    step up regulators are inefficient!

    And you base this how ??

    What does it matter, you're going to need to charge the skateboard, so the transmitter is another part of it.

     

    I suggest maybe YOU do the design and then ask for comments ...so far it seems everyone else is doing the design for you.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to mcb1

    This is a actual life skateboard, not a toy. The thing is that I only need help with the battery for tansmitter. I've chosen the transmitter. If you want to say step up regulators are efficient than give one which is effecient. Every Volt/Amp is needed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to royston02

    Ihave the design ready. A transmitter, atmega chip all that is remaining is battery and the smaller the better.