Arduino
  • Products
  • More
Arduino
Arduino Forum How to wire a transistor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 2178 views
  • Users 0 members are here
  • transistor
  • circuit
  • wiring
  • wire
  • Design
  • arduino
  • circuitry
Related

How to wire a transistor?

nschreiber0813
nschreiber0813 over 12 years ago

Dear: Element 14

Hello it is me Noah again as you may remember me from my last post I am trying to build an arduino rocket controller and I am at prototyping stage. First of all you should know that I am using transistors BD712 which a pnp transistor that I need to amplify a current. The reason I need it to amplify a current is because I need it to increase 5V to 7.5V and to then send the current to my fixed barrier terminal blocks where it will then detonate the rocket motors. You see first of all in order you need a base resistor that connects to ground. The reason you need that is to prevent the board from short circuiting. I have placed several base resistors at several points and according to wikipedia I think I am doing this right. It says on wikipedia that I should do this.

NPN_common_emitter.svg

And this is what I did.

image

Please can you help me because I am not even sure what a transistor is?

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 12 years ago +1
    It would be useful to know how much current you would need to actuate an ignitior, and if they melt open when actuated. If this is the case, you could use a thrystor. In the more general case of having…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Sure, thank you kindly for asking. I used to play with rockets when I was a kid, but feel free to enlighten me on the topic. A thrystor is a device such as a SCR or TRIAC. These devices turn on well, but…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Model rocket igniters are made with wires made from nichrome, or were when I was a kid. The electric burner on a stove is made out of the stuff AFIK. It is 50/50 nickel and chrome. Hard, low corrosive…
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    Try:

    Thyristor - Wikipedia, the free encyclopedia

    Silicon-controlled rectifier - Wikipedia, the free encyclopedia

    TRIAC - Wikipedia, the free encyclopedia

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 12 years ago

    Try:

    Thyristor - Wikipedia, the free encyclopedia

    Silicon-controlled rectifier - Wikipedia, the free encyclopedia

    TRIAC - Wikipedia, the free encyclopedia

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to D_Hersey

    Dear: Don

    I am very sorry to ask you so many questions but not to give you enough points for it but I might make this be a discussion, how are the following associated with my project and I don't get what you have in mind.

    • Thyristor
    • SCR
    • TRIAC

    Could please explain why and how they are associated with my project because I am not getting that.

    From: Noah

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 12 years ago in reply to nschreiber0813

    Well, just that you could use a SCR (for example) rather than a transistor as a power switch if the iginiters normally melt through.  It is a small matter.  NVM.  With a transistor, you have to turn off the current.  The thyristor version would keep juicin' 'til the filament melted.  You would probably want to throw a fuse in series with the load just-in-case the load didn't melt through for some reason.  Depends how your igniter works.  Some just heat up and ignite chemicals that the nichrome has been dipped in and don't melt through.  If you really wanted to dump tons of energy into the igniters, you could get a charge pumper and make a circuit like the one used to fire a photographic strobe.  Again, NVM.  These ideas just add more complexity than they are worth for a non-expert.  I was just musing.  Nowadays you would have trouble finding someone who could bias a MOSFET, much less know what an SCR is.