Arduino
  • Products
  • More
Arduino
Arduino Forum How to connect a cellular antenna?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 1486 views
  • Users 0 members are here
  • rover_5
  • bluetooth
  • connector
  • gps
  • cellular_antenna
  • wireless
  • arduino
Related

How to connect a cellular antenna?

nschreiber0813
nschreiber0813 over 12 years ago

Dear: Element 14

First of all you should know that I am currently working on my Rover 5 chassis. I would like my rover 5 chassis to have a GPS so it doesn't get lost and for it to also have a Bluetooth module so I can control it remotely and autonomously. But in order to do that I need an antenna. See the antennas on both modules aren't powerful enough to send a signal back and to receive it. That is why I am using part cel-0075 which you can find here. Good luck I could use all the help I can get.

From: Noahimage

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1 suggested
    Noah, I don't think this is going to work the way you expect. As I understand your question, you want to control your rover via bluetooth (which operates at 2.4 GHz) via a cellular antenna, which operates…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to nschreiber0813 +1
    Noah, You'll need a pigtail to connect the antenna to the board. Something like this: http://www.amazon.com/TP-LINK-TL-ANT24PT-RP-SMA-Pigtail-Cable/dp/B003U6825G/ref=sr_1_5?ie=UTF8&qid=1407111497&sr=8…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Noah What controller are you planning to use on this project, You should know that a lot of the Arduino's will not be able to talk to a USB Bluetooth dongle (adapter) like the one you linked in, you will…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Ariel length is a function of the frequency, most small devices try to go with about a 1/4 of the wavelength

     

    you can calculate what this is like this

     

    First the speed of electricity (Radio Wave) in free air = 300000000 Meters per Second

     

    Wavelength is the speed of travel in free air divided by the frequency

     

    ie.

    2.4Ghz/300,000M/S = 120mm so a quarter wavelength will be 30mm. this would be a good length. you could also go with 1/8 = 15mm but less effective

    900Mhz/300000       = 333mm, so almost 3 times longer and not an even divider of the 2.4Ghz length, even a                     1/8 = 41.6mm


    How far are you intending to control this from ?, a simple Bluetooth will give you 30-100ft, a cheap sub1Ghz radio will work to 300 feet or more

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to Robert Peter Oakes

    Dear: Peter

    You should know first of all I am using parts GTPA013 and CSR 4.0 which you can find here and here. and I would like it to have a decent range not much or not to little. I am really not sure how far I want it to go but as long as it has 4 bars little to almost all the time I am good.

    From: Noahimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to Robert Peter Oakes

    Dear: Peter

    You should know first of all I am using parts GTPA013 and CSR 4.0 which you can find here and here. and I would like it to have a decent range not much or not to little. I am really not sure how far I want it to go but as long as it has 4 bars little to almost all the time I am good.

    From: Noahimage