Arduino Forum ESP8266 arduino wireless.
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
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 404 subscribers
  • Views 606 views
  • Users 0 members are here
  • controll
  • wireless
  • arduino
  • remote
Related

ESP8266 arduino wireless.

anej
anej over 11 years ago

Hello.

I am planning to build a remote controled car with 2 arduinos - one arduino for the car and one for the controller... Now i found this ESP8266 Serial WIFI Wireless Transceiver Modules and i don't know if this is a good thing to use with my project. Can i use two those modules for serial communication between two arduinos ??

 

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 11 years ago +2 suggested
    Anej, As has been said the ESP8266 is a relatively new device and there is not a lot of information on its use yet. For your project I would use the CISECO wireless modules. CISECO do a wireless shield…
  • camuyano
    camuyano over 11 years ago +1 suggested
    Short answer yes with some notes: To use the ESP8266 you'll need to parse the strings you get from the device in order to get the data. The ESP will output different messages about status and things like…
  • scargill
    scargill over 11 years ago in reply to bobcroft +1
    I would tend to disagree - there is now a lot of information - there are several projects including the original ESPRESSIF AT code which now works as of the latest updates - the FRANKENSTEIN code and a…
Parents
  • amgalbu
    0 amgalbu over 11 years ago

    Hello

    I would use Aurel modules which have a very good quality-to-price ratio with the Arduino VirtualWire library

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to amgalbu

    Thanks amgalbu

     

    I was about to ask a similar question on here and was looking at either the XBee, the Laird PRM133, or the Aurel modules. Will give the Aurel modules a try now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scargill
    0 scargill over 11 years ago in reply to gadget.iom

    Not sure what you want to use these for but they are awfully simple and are easily blocked by any old radio remote control. Suggest RM22 or similar. NRF24L01 don’t have much range – but they are cheap.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • scargill
    0 scargill over 11 years ago in reply to gadget.iom

    Not sure what you want to use these for but they are awfully simple and are easily blocked by any old radio remote control. Suggest RM22 or similar. NRF24L01 don’t have much range – but they are cheap.