Arduino
  • Products
  • More
Arduino
Arduino Forum controlling 3.1 volt steppers with adafruit motorshields v 2.3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 999 views
  • Users 0 members are here
  • stepper
  • ohm's_law
  • motor_shield
  • adafruit
  • arduino
Related

controlling 3.1 volt steppers with adafruit motorshields v 2.3

e14 Contributor
e14 Contributor over 11 years ago

Hi.

 

I'm quite new to electronics and robotics.

 

I've got two adafruit motor shields and three steppers. The steppers has a rated current of 2.5 A and a phase resistance of 1.25 ohms.

 

I understand from adafruits documentation that it can control motors in a voltage range of 5-12 V dc.

 

My question is can I use my 3.125 V motors if I put a  3.55 Ohm resistor in serie in each phase of each motor?

I calculated the restistance using Ohm's law:

U = I * R

12 V = 2.5 A * (1.25 Ohm + 3.55 Ohm)

 

Have a nice Weekend image

 

- Roar

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to clem57 +3 verified
    In most stepper motor controllers (Modern ones), you do not limit the voltage by setting up a divider (R1, R2 ) as they manage the pulse width in the same way as driving an LED with PWM, it is more about…
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor +1
    The voltage divider is better way to go sending one end to ground. I have seen this for 5 volt connections to a 3.3 volt pins on Raspberry Pi. But Too much voltage does not divide well. 12 volts to 3 volts…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor +1
    See my other coment but in context to your comment, most motors have a rated current, not voltage and the controller takes care of the difference
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have tried to make a schematic:

    image

    The gray area represents the adafruit motor shield.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    If the voltage is not HIGH enough a resistor will not INCREASE the voltage as far as I can see. Let me refer you to Robert Peter Oakes

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    If the voltage is not HIGH enough a resistor will not INCREASE the voltage as far as I can see. Let me refer you to Robert Peter Oakes

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Hi Clem.

     

    The Idea is to decrease the voltage.

    My idea is, using calculations, that if:

     

    3.125 V = 2.5 A * 1.25 Ω

     

    Which gives the voltage of the stepper.

     

    My consideration is if I put a 3.55 resistor in serie, as in the schematic in a former post, will this resistor obtain the excess voltage?

     

    By calculation:

     

    12 V = 2.5 A * (1.25Ω + 3.55Ω)

    where the 3.55Ω resistor is the one I'm talking about.

     

    Is it possible to do it that way?

    Or will the resistor consume too much energy?

    Perhaps it's better to crate a voltage divider to reduce the voltage?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    The voltage divider is better way to go sending one end to ground. I have seen this for 5 volt connections to a 3.3 volt pins on Raspberry Pi. But Too much voltage does not divide well. 12 volts to 3 volts will heat up the circuit too much.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to clem57

    In most stepper motor controllers (Modern ones), you do not limit the voltage by setting up a divider (R1, R2 ) as they manage the pulse width in the same way as driving an LED with PWM, it is more about the current going through the Motor, its inductance will limit this automatically and is often set-up in the configuration of the controller

     

    So having a motor with only 1.25Ohms DC resistance means nothing to a pulse, its inductive reactance is what will matter and that to a pulse can be much higher than the DC Ohms

     

    It would be common to see a stepper like this having say a 12V supply but still driven directly from the controller with no additional limiting resistors, you can often have a current sense resistor that provides feedback to the controller so it can manage the average current / power through the motor

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    See my other coment but in context to your comment, most motors have a rated current, not voltage and the controller takes care of the difference

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to Robert Peter Oakes

    I always learn more with you Peter. Thanks for stepping in.

    Clem