Arduino Forum pls how do i go about communicating with 2 arduinos with the use of the tx/rx pin.
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
  • State Not Answered
  • Replies 17 replies
  • Subscribers 403 subscribers
  • Views 1799 views
  • Users 0 members are here
Related

pls how do i go about communicating with 2 arduinos with the use of the tx/rx pin.

Former Member
Former Member over 10 years ago

i have codes for pulse sensor, temp sensor, GPS  and i need the readings from the sensors and gps to be sent to the other arduino's LCD. i just dont know how to go about doing it and i was wondering if there is someone that could help guide me.

 

//sender

int inpin=A0;

int TEMP=0;

int heartratepin=A1;

int difference;

int newHeartReading = 0;

int lastHeartReading = 0;

int measurements[5] = {0,0,0,0,0};

int historySize = 5;

int recenttotal = 0;

int Index = 0;

boolean highChange = false;

int minimumdifference = 2;

int num[5];

int average=0;

 

 

// Heart rate timing

long lastHeartbeatTime = 0;

long debounceDelay = 150;       // the debounce time; increase if the output flickers

int currentHeartrate = 0;

int lastHeartrate = 0;

//Heart rate LED

//int ledState = LOW;

//long ledOnMillis = 0;

//long ledOnInterval = 50;

int slope = ((newHeartReading-lastHeartReading)/(debounceDelay-lastHeartrate));

 

 

 

 

 

 

// Debugging string

String debugOutput = "";

void setup() {

   // start serial port at 9600 bps:

   Serial.begin(9600);

    pinMode(heartratepin,INPUT);

   establishContact();

}

void establishContact() {

while (Serial.available() <= 0) {

      Serial.println("hello");   // send a starting message

      delay(300);

   }

}

void loop() {

   // read analog input, divide by 4 to make the range 0-255:

   int analogValue = analogRead(inpin);

   float millivolts = (analogValue/1024.0)*5000;

   float celsius = millivolts/10-50;

   Serial.println(analogValue);

   Serial.print(celsius);

   Serial.print("c");

   Serial.print((celsius*9)/5+32);

   Serial.print("F");

   newHeartReading = analogRead(heartratepin);

    //calculation

  difference = newHeartReading - lastHeartReading;

  lastHeartReading = newHeartReading;

 

  // Find new recent total

  recenttotal = recenttotal - measurements[Index] + difference;

  // replace indexed recent value

  measurements[Index] = difference;

   //index + 1 index = (index + 1) % historySize;

    for (int i=0; i<5; i=i+1){

               num[i]=0;        

   }

    

              if (Index>=5)

              Index=0;

              //calculating the average

              average=recenttotal/5;

              Serial.println(average);

              delay(10);

  if (recenttotal >= minimumdifference)

  {

    // possible heart rate check timing

    if (millis() - lastHeartbeatTime >= debounceDelay)   // whatever the reading is at, it's been there for longer

    // than the debounce delay, so take it as the actual current state:

 

 

    {

  // Heart rate

// digitalWrite(ledPin, HIGH);

  currentHeartrate = 60000 / (millis() - lastHeartbeatTime);

    lastHeartbeatTime = millis();

   Serial.println(newHeartReading);

      if (currentHeartrate <= 200)// && currentHeartrate > 20)

    { 

                 

                  Serial.print("Heart Rate =" + String(currentHeartrate) + "  ");

                  delay(10);

    }

            if (currentHeartrate <= 39 and currentHeartrate >= 0){

                

                  Serial.print("I Am Sick");

                }

                 delay(10);

          if (currentHeartrate<= 79 and currentHeartrate >= 70){

                

                  Serial.print("Night Mare");

                }

                delay(10);

            if (currentHeartrate <= 69 and currentHeartrate >= 40){

               

                  Serial.print("kid Is At Sleep");

          }

              delay(10);

              if (currentHeartrate <= 99 and currentHeartrate >= 80){

                 

                  Serial.print("Kid Is Resting");

             }

                delay(10);

                if (currentHeartrate <= 119 and currentHeartrate >= 100){

                

                  Serial.print("Kid Is Playing");

               }

             

                  if(currentHeartrate > 120){

                   

                    Serial.print(" The Kid Is Having ");

                    //lcd.setCursor(0,1);

                    //lcd.print(" A Heart Attack");

                }

  

  

 

 

   // print different formats:

   Serial.write(analogValue);  // Print the raw binary value

   Serial.print('\t');             // print a tab

   Serial.write(newHeartReading);  // Print the raw binary value

   Serial.print('\t');             // print a tab

 

}

  }

}

 

 

 

//receiver

#include <SPI.h>

#include <LiquidCrystal.h>

int heartratepin=A1;

int inpin=A0;

LiquidCrystal lcd(30,31,32,33,34,35);

void setup()

{

  lcd.begin(16,2);

  Serial.begin(9600);

}

void loop()

{

  if(Serial.available()>0)

  {

    int inByte=Serial.read();

    int analogValue=analogRead(inpin);

    lcd.print(analogValue);

    lcd.print(",");

   

    int newHeartReading=analogRead(heartratepin);

    lcd.print(newHeartReading);

    lcd.print(",");

   

   

 

 

  }

}

 

i dont know what i am doing wrong

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 10 years ago in reply to Former Member +2
    Richard, in order to see the Easy Transfer library just Google Arduino Easy Transfer library. There are informative notes and code examples. To answer your other question, yes you can display the data…
  • clem57
    clem57 over 10 years ago +1
    ricardo240 I cannot comment on the sender code since it has many things going on. But here are the things I would do: Make sure the pins are connected as TX to RX on the UART on sender and UART on receiver…
  • clem57
    clem57 over 10 years ago in reply to Former Member +1
    To understand: 1) the sensors are reading fine. 2) The UNO sends on UART to the MEGA UART but does not work. What pins are connected on each to the other? 3) The code you sent looks like snippets especially…
Parents
  • neilk
    0 neilk over 10 years ago

    ricardo240  Hi Richard,

     

    Your problem seems to me to be the classic one of "can't see the wood for the trees"

     

    I assume that you can read the sensors correctly AND display the results on the Serial Monitor of the UNO

    I assume that you can correctly display similar data on the LCD connected to your MEGA.

     

    So, if I were you I would start a NEW simple sketch to transmit a SIMPLE KNOWN item of data from the UNO to the MEGA, displaying the received item of data on the MEGA Serial Monitor.

     

    Once you have achieved this, using the help that clem57 has already offered you, then you can make the data more complex and so develop the code in a stepwise fashion..

     

    It's how I do all my development work - identify the most difficult component and solve that FIRST.

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • neilk
    0 neilk over 10 years ago

    ricardo240  Hi Richard,

     

    Your problem seems to me to be the classic one of "can't see the wood for the trees"

     

    I assume that you can read the sensors correctly AND display the results on the Serial Monitor of the UNO

    I assume that you can correctly display similar data on the LCD connected to your MEGA.

     

    So, if I were you I would start a NEW simple sketch to transmit a SIMPLE KNOWN item of data from the UNO to the MEGA, displaying the received item of data on the MEGA Serial Monitor.

     

    Once you have achieved this, using the help that clem57 has already offered you, then you can make the data more complex and so develop the code in a stepwise fashion..

     

    It's how I do all my development work - identify the most difficult component and solve that FIRST.

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to neilk

    i did but it still didnt display anything on the lcd

    this is the sample code that i decided to use as an experiment to get the communication working because i believe if this works then i can proceed to getting the rest of the things i need to do added to it.

    her is the code

     

    #include <SoftwareSerial.h>

    int inpin=A0;

    int TEMP=0;

    int sensorValue;

    SoftwareSerial mySerial(18,19);

     

     

    void setup() {

       // start serial port at 9600 bps:

       Serial.begin(9600);

     

       // pinMode(heartratepin,INPUT);

      // establishContact();

    }

    //void establishContact() {

    //while (Serial.available()== 1) {

         // Serial.println("hello");   // send a starting message

       //   delay(300);

      

     

    void loop() {

      if (mySerial.available())

      Serial.write(mySerial.read());

      if (Serial.available())

       int sensorValue = analogRead(inpin);

       float millivolts = (sensorValue/1024.0)*5000;

       float celsius = millivolts/10-50;

       Serial.println(sensorValue);

       Serial.print(celsius);

       Serial.print("c");

       Serial.print((celsius*9)/5+32);

       Serial.print("F");

       // print different formats:

      mySerial.write(sensorValue);  // Print the raw binary value

       Serial.print('\t');             // print a tab

    }

     

     

     

    #include <SoftwareSerial.h>

     

     

    //reciever

     

     

    #include <SPI.h>

    #include <LiquidCrystal.h>

    SoftwareSerial mySerial(1,0);

    int inpin=A0;

    LiquidCrystal lcd(30,31,32,33,34,35);

    void setup()

    {

      lcd.begin(16,2);

      Serial.begin(9600);

      //Serial1.begin(9600);

    establishContact();

    }

    void establishContact() {

    while (Serial.available()== 1) {

         // Serial.println("hello");   // send a starting message

          delay(300);

        }

    }

    void loop()

    {

      if(Serial.available()==1)

      {

        int inbyte =Serial.read();

        int sensorValue=analogRead(A0);

        lcd.print(sensorValue);

        lcd.print(",");

       

     

       

       

     

     

      }

    }