Hello,
I have RFID 13.56 MHz / NFC Module for Arduino from Cooking Hacks , I want to know how much time need a full read in a block process ?
I tried with millis () function and I get this :
I get 2196 ms . is that right ? I think it's so much
Rita
Hello,
I have RFID 13.56 MHz / NFC Module for Arduino from Cooking Hacks , I want to know how much time need a full read in a block process ?
I tried with millis () function and I get this :
I get 2196 ms . is that right ? I think it's so much
Rita
It does seem a little slow but I dont have one to try out so nothing to compare to
What is the code your using to time the read, can you please provide in here
Thanks
/* * RFID/NFC Modul for Arduino * Read a block */ uint8_t dataRX[35];//Receive buffer. uint8_t dataTX[35];//Transmit buffer. uint8_t _UID[4];// stores the UID (unique identifier) of a card. uint8_t keyAccess[] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF } ;// stores the key or password. uint8_t address = 0x04;//Address to read. uint8_t ATQ[2];//Answer to request uint8_t state;//state of the process uint8_t aux[16];//Auxiliar buffer. unsigned long time; void setup() { //Start serial port 115200 bps: Serial.begin(115200); delay(100); Serial.print("RFID/NFC @ 13.56 MHz module started"); delay(1000); //!It is needed to launch a simple command to sycnchronize getFirmware(); configureSAM(); } void loop() { Serial.print("\n"); Serial.print("Ready to read..."); ///////////////////////////////////////////////////////////// //Get the UID Identifier init(_UID, ATQ); Serial.print("\n"); Serial.print( "The UID : "); print(_UID , 4); time = millis();//prints time since program started Serial.print("Time:"); Serial.print(time); Serial.print(" "); Serial.write("ms"); //////////////////////////////////////////////////////////// //Auntenticate a block with his keyAccess state = authenticate(_UID, address, keyAccess); Serial.print("\n"); if ( state == 0) { Serial.println("Authentication block OK"); time = millis();//prints time since program started Serial.print("Time:"); Serial.print(time); Serial.print(" "); Serial.write("ms"); } else { Serial.println("Authentication failed"); } ///////////////////////////////////////////////////////////// //Read from address after authentication state = readData(address, aux); Serial.print("\n"); if (state == 0) { Serial.println("Read block OK"); } else { Serial.println("Read failed"); } Serial.print("\n"); Serial.print("Data readed : "); print(aux , 16); Serial.print("\n"); time = millis();//prints time since program started Serial.print("Time:"); Serial.print(time); Serial.print(" "); Serial.write("ms"); delay(2000); } //********************************************************************** //!The goal of this command is to detect as many targets (maximum MaxTg) // as possible in passive mode. uint8_t init(uint8_t *UID , uint8_t *ATQ) //! Request InListPassive { Serial.flush(); dataTX[0] = 0x04; // Length lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; dataTX[3] = 0x4A; // Code dataTX[4] = 0x01; //MaxTarget dataTX[5] = 0x00; //BaudRate = 106Kbps dataTX[6] = 0x00; // Clear checkSum position checkSum(dataTX); sendTX(dataTX , 7 ,23); for (int i = 17; i < (21) ; i++){ _UID[i-17] = dataRX[i]; UID[i-17] = _UID[i-17]; } ATQ[0] = dataRX[13]; ATQ[1] = dataRX[14]; if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x4B) & (dataRX[11] == 0x01)) { return 0; } else { return 1; } } //********************************************************************** //!A block must be authenticated before read and write operations uint8_t authenticate(uint8_t *UID, uint8_t blockAddress, uint8_t *keyAccess) { dataTX[0] = 0x0F; lengthCheckSum(dataTX); dataTX[2] = 0xD4; dataTX[3] = 0x40; // inDataEchange dataTX[4] = 0x01; //Number of targets dataTX[5] = 0x60; // Authentication code dataTX[6] = blockAddress; for (int i = 0; i < 6 ; i++) { dataTX[i + 7] = keyAccess[i]; } dataTX[13] = UID[0]; dataTX[14] = UID[1]; dataTX[15] = UID[2]; dataTX[16] = UID[3]; dataTX[17] = 0x00; checkSum(dataTX); sendTX(dataTX , 18 ,14); if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) { return 0; } else { return 1; } } //********************************************************************** //!Write 16 bytes in address . uint8_t writeData(uint8_t address, uint8_t *blockData) //!Writing { Serial.print(" "); dataTX[0] = 0x15; lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; dataTX[3] = 0x40;//inDataEchange CODE dataTX[4] = 0x01;//Number of targets dataTX[5] = 0xA0;//Write Command dataTX[6] = address; //Address for (int i = 0; i < 16; i++) { dataTX[i+7] = blockData[i]; } dataTX[23] = 0x00; checkSum(dataTX); sendTX(dataTX , 24 ,14); if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) { return 0; } else { return 1; } } //********************************************************************** //!Read 16 bytes from address . uint8_t readData(uint8_t address, uint8_t *readData) //!Reading { Serial.print(" "); dataTX[0] = 0x05; lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; // Code dataTX[3] = 0x40; // Code dataTX[4] = 0x01; // Number of targets dataTX[5] = 0x30; //ReadCode dataTX[6] = address; //Read address dataTX[7] = 0x00; checkSum(dataTX); sendTX(dataTX , 8, 30); memset(readData, 0x00, 16); if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) { for (int i = 12; i < 28; i++) { readData[i-12] = dataRX[i]; } return 0; } else { return 1; } } //********************************************************************** //!The PN532 sends back the version of the embedded firmware. bool getFirmware(void) //! It is needed to launch a simple command to sycnchronize { Serial.print(" "); memset(dataTX, 0x00, 35); dataTX[0] = 0x02; // Length lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; // CODE dataTX[3] = 0x02; //TFI checkSum(dataTX); //0x2A; //Checksum sendTX(dataTX , 5 , 17); Serial.print("\n"); Serial.print("Your Firmware version is : "); for (int i = 11; i < (15) ; i++){ Serial.print(dataRX[i], HEX); Serial.print(" "); } Serial.print("\n"); } //********************************************************************** //!Print data stored in vectors . void print(uint8_t * _data, uint8_t length) { for (int i = 0; i < length ; i++){ Serial.print(_data[i], HEX); Serial.print(" "); } Serial.print("\n"); } //********************************************************************** //!This command is used to set internal parameters of the PN532, bool configureSAM(void)//! Configure the SAM { Serial.print(" "); dataTX[0] = 0x05; //Length lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; dataTX[3] = 0x14; dataTX[4] = 0x01; // Normal mode dataTX[5] = 0x14; // TimeOUT dataTX[6] = 0x00; // IRQ dataTX[7] = 0x00; // Clean checkSum position checkSum(dataTX); sendTX(dataTX , 8, 13); } //********************************************************************** //!Send data stored in dataTX void sendTX(uint8_t *dataTX, uint8_t length, uint8_t outLength) { Serial.print(char(0x00)); Serial.print(char(0x00)); Serial.print(char(0xFF)); for (int i = 0; i < length; i++) { Serial.print(char(dataTX[i])); } Serial.print(char(0x00)); getACK(); waitResponse();// Receive response getData(outLength); } //********************************************************************** //!Wait for ACK response and stores it in the dataRX buffer void getACK(void) { delay(5); waitResponse(); for (int i = 0; i < 5 ; i++) { dataRX[i] = Serial.read(); } } //********************************************************************** //!Wait the response of the module void waitResponse(void) { int val = 0xFF; int cont = 0x00; while(val != 0x00) { //Wait for 0x00 response val = Serial.read(); delay(5); cont ++; } } //********************************************************************** //!Get data from the module void getData(uint8_t outLength) { for (int i=5; i < outLength; i++) { dataRX[i] = Serial.read();//read data from the module. } } //********************************************************************** //!Calculates the checksum and stores it in dataTX buffer void checkSum(uint8_t *dataTX) { for (int i = 0; i < dataTX[0] ; i++) { dataTX[dataTX[0] + 2] += dataTX[i + 2]; } byte(dataTX[dataTX[0] + 2]= - dataTX[dataTX[0] + 2]); } //********************************************************************** //!Calculates the length checksum and sotres it in the buffer. uint8_t lengthCheckSum(uint8_t *dataTX) { dataTX[1] = byte(0x100 - dataTX[0]); }
ok, try this
/* * RFID/NFC Modul for Arduino * Read a block */ uint8_t dataRX[35];//Receive buffer. uint8_t dataTX[35];//Transmit buffer. uint8_t _UID[4];// stores the UID (unique identifier) of a card. uint8_t keyAccess[] = { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF };// stores the key or password. uint8_t address = 0x04;//Address to read. uint8_t ATQ[2];//Answer to request uint8_t state;//state of the process uint8_t aux[16];//Auxiliar buffer. unsigned long time; unsigned long loop_time; // less the 2 second delay... dont forget unsigned long function_time; void setup() { //Start serial port 115200 bps: Serial.begin(115200); delay(100); Serial.println("RFID/NFC @ 13.56 MHz module started"); delay(1000); //!It is needed to launch a simple command to sycnchronize getFirmware(); configureSAM(); } void loop() { Serial.print("\nReady to read..."); // optimise the prints by putting the new lines in the same print as the actual print loop_time = 0; // reset the loop timer ///////////////////////////////////////////////////////////// //Get the UID Identifier function_time = millis(); // we already had a one second delay in setup that is not part of the timeing so lets start with a clean count init(_UID, ATQ); time = millis() - function_time; //prints time to get the UID loop_time += time; Serial.print("\nThe UID : "); print(_UID, 4); Serial.print("Time:"); Serial.print(time); Serial.println(" ms"); // dont need the space and the ms on seperate prints, just do it in one, also by using println you get the new line at the end automatically //////////////////////////////////////////////////////////// //Auntenticate a block with his keyAccess function_time = millis(); state = authenticate(_UID, address, keyAccess); time = millis() - function_time;//time the call loop_time += time; // add this call to the overall time Serial.print("\n"); if (state == 0) { Serial.println("Authentication block OK"); Serial.print("Time:"); Serial.print(time); Serial.println(" ms"); } else { Serial.println("Authentication failed"); } ///////////////////////////////////////////////////////////// //Read from address after authentication function_time = millis(); state = readData(address, aux); time = millis() - function_time; // time the call loop_time += time; // add this call to the overall time Serial.print("\n"); if (state == 0) { Serial.println("Read block OK"); } else { Serial.println("Read failed"); } Serial.print("\nData readed : "); print(aux, 16); Serial.print("\nTime:"); Serial.print(time); Serial.println(" ms"); Serial.print("\nTotal call time : "); Serial.print(loop_time); Serial.println(" ms"); delay(2000); // wait 2 seconds before we loop again } //********************************************************************** //!The goal of this command is to detect as many targets (maximum MaxTg) // as possible in passive mode. uint8_t init(uint8_t *UID, uint8_t *ATQ) //! Request InListPassive { Serial.flush(); dataTX[0] = 0x04; // Length lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; dataTX[3] = 0x4A; // Code dataTX[4] = 0x01; //MaxTarget dataTX[5] = 0x00; //BaudRate = 106Kbps dataTX[6] = 0x00; // Clear checkSum position checkSum(dataTX); sendTX(dataTX, 7, 23); for (int i = 17; i < (21); i++) { _UID[i - 17] = dataRX[i]; UID[i - 17] = _UID[i - 17]; } ATQ[0] = dataRX[13]; ATQ[1] = dataRX[14]; if ((dataRX[9] == 0xD5) & (dataRX[10] == 0x4B) & (dataRX[11] == 0x01)) { return 0; } else { return 1; } } //********************************************************************** //!A block must be authenticated before read and write operations uint8_t authenticate(uint8_t *UID, uint8_t blockAddress, uint8_t *keyAccess) { dataTX[0] = 0x0F; lengthCheckSum(dataTX); dataTX[2] = 0xD4; dataTX[3] = 0x40; // inDataEchange dataTX[4] = 0x01; //Number of targets dataTX[5] = 0x60; // Authentication code dataTX[6] = blockAddress; for (int i = 0; i < 6; i++) { dataTX[i + 7] = keyAccess[i]; } dataTX[13] = UID[0]; dataTX[14] = UID[1]; dataTX[15] = UID[2]; dataTX[16] = UID[3]; dataTX[17] = 0x00; checkSum(dataTX); sendTX(dataTX, 18, 14); if ((dataRX[9] == 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) { return 0; } else { return 1; } } //********************************************************************** //!Write 16 bytes in address . uint8_t writeData(uint8_t address, uint8_t *blockData) //!Writing { Serial.print(" "); dataTX[0] = 0x15; lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; dataTX[3] = 0x40;//inDataEchange CODE dataTX[4] = 0x01;//Number of targets dataTX[5] = 0xA0;//Write Command dataTX[6] = address; //Address for (int i = 0; i < 16; i++) { dataTX[i + 7] = blockData[i]; } dataTX[23] = 0x00; checkSum(dataTX); sendTX(dataTX, 24, 14); if ((dataRX[9] == 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) { return 0; } else { return 1; } } //********************************************************************** //!Read 16 bytes from address . uint8_t readData(uint8_t address, uint8_t *readData) //!Reading { Serial.print(" "); dataTX[0] = 0x05; lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; // Code dataTX[3] = 0x40; // Code dataTX[4] = 0x01; // Number of targets dataTX[5] = 0x30; //ReadCode dataTX[6] = address; //Read address dataTX[7] = 0x00; checkSum(dataTX); sendTX(dataTX, 8, 30); memset(readData, 0x00, 16); if ((dataRX[9] == 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) { for (int i = 12; i < 28; i++) { readData[i - 12] = dataRX[i]; } return 0; } else { return 1; } } //********************************************************************** //!The PN532 sends back the version of the embedded firmware. bool getFirmware(void) //! It is needed to launch a simple command to sycnchronize { Serial.print(" "); memset(dataTX, 0x00, 35); dataTX[0] = 0x02; // Length lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; // CODE dataTX[3] = 0x02; //TFI checkSum(dataTX); //0x2A; //Checksum sendTX(dataTX, 5, 17); Serial.print("Your Firmware version is : "); for (int i = 11; i < (15); i++) { Serial.print(dataRX[i], HEX); Serial.print(" "); } Serial.print("\n"); } //********************************************************************** //!Print data stored in vectors . void print(uint8_t * _data, uint8_t length) { for (int i = 0; i < length; i++) { Serial.print(_data[i], HEX); Serial.print(" "); } Serial.print("\n"); } //********************************************************************** //!This command is used to set internal parameters of the PN532, bool configureSAM(void)//! Configure the SAM { Serial.print(" "); dataTX[0] = 0x05; //Length lengthCheckSum(dataTX); // Length Checksum dataTX[2] = 0xD4; dataTX[3] = 0x14; dataTX[4] = 0x01; // Normal mode dataTX[5] = 0x14; // TimeOUT dataTX[6] = 0x00; // IRQ dataTX[7] = 0x00; // Clean checkSum position checkSum(dataTX); sendTX(dataTX, 8, 13); } //********************************************************************** //!Send data stored in dataTX void sendTX(uint8_t *dataTX, uint8_t length, uint8_t outLength) { Serial.print(char(0x00)); Serial.print(char(0x00)); Serial.print(char(0xFF)); for (int i = 0; i < length; i++) { Serial.print(char(dataTX[i])); } Serial.print(char(0x00)); getACK(); waitResponse();// Receive response getData(outLength); } //********************************************************************** //!Wait for ACK response and stores it in the dataRX buffer void getACK(void) { delay(5); waitResponse(); for (int i = 0; i < 5; i++) { dataRX[i] = Serial.read(); } } //********************************************************************** //!Wait the response of the module void waitResponse(void) { int val = 0xFF; int cont = 0x00; while (val != 0x00) { //Wait for 0x00 response val = Serial.read(); delay(5); cont++; } } //********************************************************************** //!Get data from the module void getData(uint8_t outLength) { for (int i = 5; i < outLength; i++) { dataRX[i] = Serial.read();//read data from the module. } } //********************************************************************** //!Calculates the checksum and stores it in dataTX buffer void checkSum(uint8_t *dataTX) { for (int i = 0; i < dataTX[0]; i++) { dataTX[dataTX[0] + 2] += dataTX[i + 2]; } byte(dataTX[dataTX[0] + 2] = -dataTX[dataTX[0] + 2]); } //********************************************************************** //!Calculates the length checksum and sotres it in the buffer. uint8_t lengthCheckSum(uint8_t *dataTX) { dataTX[1] = byte(0x100 - dataTX[0]); }
I took out some redundent print statements (Or not necessary as they can be optimised into single line), I hope this did not break the code
The main mistake you where doing is this
the main loop has a 2 second delay in it, you where not eliminating this from your timeing, second you had a one second delay in startup, this was also included in your time, then you also had all the print statements to the screen (Console) also included in your time
What I did and the main change in your code is introduce a seperate timer value "function_time" that is set to millis() just before a call to read the chips, then I subtract it from the new mills() once done, this tells us how long the function call actually took. The "loop_time" simply adds up all the funcrtion_time values to see what the total is without having to keep track with a calculator after a run
Hope this helps
good, that first one still seems a little slow but that may be its nature
Glad it helped
Peter
Hi Peter ,
is the first Time just to get the UID?
what reason can I give, that's the time so long is for UID ?
Regards ,
Rita
See http://electronics.howstuffworks.com/near-field-communication.htm . This explains some of what NFC does. To protect the transmission, a handshake is made to verify and encrypt later transmissions that will be made resulting in a UID. I can write a book here, but just say encryption is not cheap to set up both in processor and communication.
Clem