Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Reverse Footprint for Arduino Mega
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 22 replies
  • Subscribers 414 subscribers
  • Views 8704 views
  • Users 0 members are here
  • arduino
  • arduino projects
Related

Reverse Footprint for Arduino Mega

colporteur
colporteur over 4 years ago

How do you mount a Mega on a PCB?

I'm using a Arduino Mega for a project and wanted to use Fritzing to create a PCB layout. The footprint for the Mega reflects the pinout of the motherboard. If I create a pin pattern on the board to mount the Mega directly to the board, then the pins need to be reversed. The Mega is flipped over and mounted face down on the PCB reversing the pinout.

I cannot find a pinout that reflects the Mega face down on a PCB. I would assume that is the way to install the board and not have a collection of jumpers running from the Mega board back to the PCB. If anyone has an insight I would welcome the input?

image

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 4 years ago +2
    I assume the PCB is plated through-hole? Put the footprint on the reverse of the PCB but actually solder the MEGA (or headers) onto the front of the board. That would work wouldn’t it?
  • BigG
    BigG over 4 years ago in reply to colporteur +2
    I would change the background colour so that you can see the white font. I did a quick test to prove and it is quite straightforward. If this is what you need, then I can place the modified fritzing…
  • BigG
    BigG over 4 years ago +1
    In PCB mode, click on the footprint and then change "pcb layer" to bottom.
Parents
  • Andrew J
    0 Andrew J over 4 years ago

    I assume the PCB is plated through-hole?  Put the footprint on the reverse of the PCB but actually solder the MEGA (or headers) onto the front of the board.  That would work wouldn’t it?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 4 years ago in reply to Andrew J

    Thanks for the response. Your suggestion was my original thought. The Mega mounts on the backside of the PCB. Not a solution I have used before therefore it seemed strange. First time using a Mega in a project also.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 4 years ago in reply to colporteur

    Yes, that would work too!  Which side to solder the Mega too might get dictated by any encasement?  Specifically, how thick the case would be and access to the USB and Power ports once soldered; I was assuming you wanted to keep all parts on one side.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 4 years ago in reply to colporteur

    Yes, that would work too!  Which side to solder the Mega too might get dictated by any encasement?  Specifically, how thick the case would be and access to the USB and Power ports once soldered; I was assuming you wanted to keep all parts on one side.