Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Best practices for Arduino I/O selection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 414 subscribers
  • Views 5294 views
  • Users 0 members are here
  • arduino_development_environment
  • arduino
Related

Best practices for Arduino I/O selection

colporteur
colporteur over 4 years ago

I'm currently working on a project using an Arduino knock-off Mega board. I discovered during prototype board development and testing an issue using I/O' 0 and 1. I found I could not control the output within my script. From online research, I discovered if I was using serial communication then I should avoid using those two I/O's. I wonder what other gotcha's don't know about?

I confess I am way down the scale of Arduinos knowledge. I label myself more of a resurrectionist rather than a programmer. I adapt code and solutions I find to solve my problems. Rarely if ever, have I built from scratch. This leads me to the title line "Best Practices for Arduino I/O selection". Are there any resources that provide this type of guidance? Are there I/O's to avoid and others that are better for a specific function?

I realize some I/O's are for specific purposes. I'm just thinking are there best practices using I/O's. I read the review posted on the site of this new book and thought maybe that has some suggestions. I'm looking for member experience.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 4 years ago in reply to shabaz +7
    I use the same principles but the other way round. I first do the inflexible ones, like UART, i2c/SPI, pwm/timer , interrupt and analogue. Then sprinkle the easy ones across what's left over.
  • fmilburn
    fmilburn over 4 years ago +7
    I've been caught out with this type of problem when using the Arduino IDE with a board I'm unfamiliar with so I can relate. In your case, the pins with the labels 0 and 1 on the silkscreen will cause a…
  • shabaz
    shabaz over 4 years ago +5
    Hi Sean, The usual board pinout diagrams often indicate all functions available per pin, so they can be used for guidance, but the ultimate authority is the chip datasheet. Example snippet (found via…
Parents
  • dougw
    dougw over 4 years ago

    I always create a spreadsheet listing all the MCU pins and their possible functions, then I add peripherals or chips and all their pins opposite the MCU pins they will be connected to.

    There is an example here that provides an idea of what I do:

    /challenges-projects/design-challenges/sixth-sense-design-challenge/b/blog/posts/sixth-sense---interfaces---graffitibot-blog-4

    It might be  a bit confusing because the Nucleo has its native headers connected to Arduino headers, but this is a good reason to track it in a spreadsheet.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 4 years ago

    I always create a spreadsheet listing all the MCU pins and their possible functions, then I add peripherals or chips and all their pins opposite the MCU pins they will be connected to.

    There is an example here that provides an idea of what I do:

    /challenges-projects/design-challenges/sixth-sense-design-challenge/b/blog/posts/sixth-sense---interfaces---graffitibot-blog-4

    It might be  a bit confusing because the Nucleo has its native headers connected to Arduino headers, but this is a good reason to track it in a spreadsheet.