Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum LED Button push light up
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 38 replies
  • Subscribers 415 subscribers
  • Views 28140 views
  • Users 0 members are here
  • sequence
  • led
  • button
Related

LED Button push light up

Josephmbrandtii
Josephmbrandtii over 4 years ago

Attempting to make a Cornhole score board with 21 lights that light up at each button push.  At the end of the chain i want it to shut off the lights so there is none.  I am very new to this and have only gotten to the research part.  Any help i can get will be amazing.  Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 4 years ago +7
    Is the button to be controlled by a person or is the button controlled automatically by the cornsack/beanbag passing through the hole in the board ? What sort of lights are you planning on using ? Individual…
  • javagoza
    javagoza over 4 years ago +5
    Maybe you can use addressable LEDs https://www.makerguides.com/how-to-control-ws2812b-individually-addressable-leds-using-arduino/
  • geralds
    geralds over 4 years ago in reply to Josephmbrandtii +5
    Hi, here a suggestion: As I saw you have drawn it from the example from the datasheet. Now this is the complete circuit including the bypass capacitors and one of a possible method to make the…
Parents
  • dougw
    0 dougw over 4 years ago

    It sounds like you could just connect a 22 bit Johnson counter to 21 lights with a debounced button to count up. Three CD4017 chips (~$0.11 each) cascaded would could make a 21 bit Johnson counter. You would need a MOSFET on each output to drive each light.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 4 years ago in reply to dougw

    @dougw  @colporteur - would a transistor array chip work for that? I've never used them, but this ULN2004 chip available here on Newark seems to combine 7 transistors at 500mA each.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 4 years ago in reply to dougw

    @dougw  @colporteur - would a transistor array chip work for that? I've never used them, but this ULN2004 chip available here on Newark seems to combine 7 transistors at 500mA each.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 4 years ago in reply to ntewinkel

    Yes the ULN2004 should work great - they are often used to drive LEDs.