Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Does Arduino have a Dead Man switch?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 23 replies
  • Subscribers 410 subscribers
  • Views 5731 views
  • Users 0 members are here
  • arduino coding
  • arduino
Related

Does Arduino have a Dead Man switch?

colporteur
colporteur over 4 years ago

A dead man's switch is a device used as a fail-safe. These switches are usually used as a form of fail-safe where they stop a machine with no operator from a potentially dangerous action or incapacitate a device as a result of accident, malfunction, or misuse. 

I'm looking for some method to stop an Arduino to prevent harm. Is there an Arduino code sequence that will stop an Arduino and the only way to recover is to restart the device?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +10
    Watchdog circuits are the most common way to respond to serious system failure or software issues but there are a bunch of similar but subtly different concepts to clarify before a full answer... Fail…
  • robogary
    robogary over 4 years ago +5
    An ESTOP switch is a fail safe electro-mechanical device to provide fail-safe whether a machine is operating or not. A deadman switch is used when a machine is in operation to ensure the operator is…
  • javagoza
    javagoza over 4 years ago +5
    I recently faced a similar issue with the Arduino Nano 33 IoT. The Arduino Nano 33 IoT uses the 32-bit SAMD21 Arm Cortex-M0 processor so the solution would not work for all Arduino models. I had to activate…
Parents
  • Gough Lui
    0 Gough Lui over 4 years ago

    You could always drop into an infinite loop to stop an Arduino in its tracks.

    More often, watchdog timers are used to reboot an Arduino in case the sketch stops running for a certain length of time.

    But perhaps the safest and easiest depending on the application is to have a mechanical "dead-man's" that cuts power to the board entirely, e.g. a series power switch.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 4 years ago

    You could always drop into an infinite loop to stop an Arduino in its tracks.

    More often, watchdog timers are used to reboot an Arduino in case the sketch stops running for a certain length of time.

    But perhaps the safest and easiest depending on the application is to have a mechanical "dead-man's" that cuts power to the board entirely, e.g. a series power switch.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ntewinkel
    0 ntewinkel over 4 years ago in reply to Gough Lui

    I wonder if there’s a watchdog type power switch module? Ie, a module that shuts off after 1 second unless the timer is reset via a digital pin. Then in the Arduino code loop it has to pulse a digital pin or else the power gets cut.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 4 years ago in reply to ntewinkel

    I suppose you could combine WDT with reset cause to achieve this.

    Lets say your program begins by determining reset cause first - if it was WDT, then hang the program in a loop feeding the WDT. If the cause was anything else (e.g. cold boot, brownout), then continue execution.

    - Gough