Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Does Arduino have a Dead Man switch?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 23 replies
  • Subscribers 410 subscribers
  • Views 5752 views
  • Users 0 members are here
  • arduino coding
  • arduino
Related

Does Arduino have a Dead Man switch?

colporteur
colporteur over 4 years ago

A dead man's switch is a device used as a fail-safe. These switches are usually used as a form of fail-safe where they stop a machine with no operator from a potentially dangerous action or incapacitate a device as a result of accident, malfunction, or misuse. 

I'm looking for some method to stop an Arduino to prevent harm. Is there an Arduino code sequence that will stop an Arduino and the only way to recover is to restart the device?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +10
    Watchdog circuits are the most common way to respond to serious system failure or software issues but there are a bunch of similar but subtly different concepts to clarify before a full answer... Fail…
  • robogary
    robogary over 4 years ago +5
    An ESTOP switch is a fail safe electro-mechanical device to provide fail-safe whether a machine is operating or not. A deadman switch is used when a machine is in operation to ensure the operator is…
  • javagoza
    javagoza over 4 years ago +5
    I recently faced a similar issue with the Arduino Nano 33 IoT. The Arduino Nano 33 IoT uses the 32-bit SAMD21 Arm Cortex-M0 processor so the solution would not work for all Arduino models. I had to activate…
  • colporteur
    0 colporteur over 4 years ago in reply to javagoza

    J, your post on Arduino project just blow me away. I envy your knowledge level because it makes things sound so easy.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 4 years ago in reply to colporteur

    If you have enough control to be able to detect the issue and programmatically place the microcontroller into a sleep state, then it sounds as if you would also have enough control to take a slightly less drastic approach. Just stop all activity and if necessary, reinitialise back to the start-up state.

    If it requires physical intervention on the track, then stop all activity under program control, turn on a 'check engine light' and wait for an 'all clear' button press before continuing operation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 4 years ago in reply to beacon_dave

    To be honest, I don't have enough information at the moment to know whether my *** is punched or bored:) My deadman switch request was a lifeline to see if I could get the code to behave.

    I have some sensor reading reliability issues that are causing problems. I now know halogen floods lights are not good when you are working with IR sensors:( 

    I need to do some additional troubleshooting to isolate the issue or issues. I threw the sleep_mode in the code today as a hail mary and it did nothing. The relays still chattered like my teeth on a November Manitoba morning.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robogary
    0 robogary over 4 years ago in reply to colporteur

    Some cold maple syrup ought to muffle or even eliminate the chatter :-) 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 3 years ago in reply to colporteur

    Relays can chatter if their coils aren't getting enough voltage or current. Is it possible when both coils get energized, it loads the power supply enough to cause a local voltage drop?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to dougw

    The condition is two relays cycling one on the other off then flip. The relay control turnouts on the layout. Something in my code is owly causing the problem. I'm working on the problem hoping to uncover the cause.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 3 years ago in reply to colporteur

    In that case, your sleep mode code may not be working entirely as expected either, if the code is still toggling the relay outputs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to beacon_dave

    The troubleshooting session today was a disaster. I reversed the DC power input to the controller board and it no longer winky-blinky:(

    I failed to notice the two power wires had reversed themselves while I was doing some changes. My mind failed to register the labels and the colour coding of the wires. I hook them up and JASUS!

    Two hours later the buck-boost board has been replaced and a diode was installed to prevent the problem in the future. Fortunately, I installed a protection diode for the Arduino Mega so it wasn't taken out. Why I didn't install the diode for the other section on the board escapes me.

    Maybe tomorrow will be a better day.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 3 years ago in reply to colporteur

    Ouch!

    On a more philosophical note though, I guess it finally silenced those chattering relays?

    Perhaps more of a crowbar approach than a dead man's switch though...  

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to beacon_dave

    These are growth moments. Personally, and hardware-design-wise.

    also: Hugging

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>