Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Does Arduino have a Dead Man switch?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 23 replies
  • Subscribers 410 subscribers
  • Views 5755 views
  • Users 0 members are here
  • arduino coding
  • arduino
Related

Does Arduino have a Dead Man switch?

colporteur
colporteur over 4 years ago

A dead man's switch is a device used as a fail-safe. These switches are usually used as a form of fail-safe where they stop a machine with no operator from a potentially dangerous action or incapacitate a device as a result of accident, malfunction, or misuse. 

I'm looking for some method to stop an Arduino to prevent harm. Is there an Arduino code sequence that will stop an Arduino and the only way to recover is to restart the device?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +10
    Watchdog circuits are the most common way to respond to serious system failure or software issues but there are a bunch of similar but subtly different concepts to clarify before a full answer... Fail…
  • robogary
    robogary over 4 years ago +5
    An ESTOP switch is a fail safe electro-mechanical device to provide fail-safe whether a machine is operating or not. A deadman switch is used when a machine is in operation to ensure the operator is…
  • javagoza
    javagoza over 4 years ago +5
    I recently faced a similar issue with the Arduino Nano 33 IoT. The Arduino Nano 33 IoT uses the 32-bit SAMD21 Arm Cortex-M0 processor so the solution would not work for all Arduino models. I had to activate…
  • kmikemoo
    0 kmikemoo over 3 years ago

    colporteur  Owly when working with relays?  Don't forget the reverse biased anti-spike diodes across the relay coils.  That inductive kick can do some damage - or at least give you odd operating characteristics.

    As to the deadman... you can always supply power through the NO contacts on a relay.  Use a momentary switch to enable power to the Arduino and have the Arduino act as the seal-in contacts for the power relay.  If the watchdog timer drops out, so do the seal-in contacts.  Restart is manual.

    I keep meaning to make a 555 watchdog, but I haven't got around to it yet.  Sure there are chips that do this, but... I have this idea stuck in my brain. Laughing

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to kmikemoo

    Thanks for the input. Owly is a colloquialism from where I was raised. I have seen a similar relay arrangement in the past as a fail-safe.

    I'm licking my wounds from the stuff I burnt up. The model train is having some issues. Not running reliably. Kinda hard to test when it keeps introducing errors. I hope to get some real troubleshooting time this week.

    The missus is leaving town for a few days. Fresh fish is on the menu and the dog and myself are going to watch TV in our underwear.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 3 years ago in reply to colporteur
    colporteur said:
    The missus is leaving town for a few days. Fresh fish is on the menu and the dog and myself are going to watch TV in our underwear.

    That tends to suggest that you either a) don't normally wear any while watching TV, or b) that you normally wear someone else's... Scream

    Either way, after this week's incidents I'd strongly recommend going for the fire-proof variety...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<