Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Looking for a small display recommendation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 413 subscribers
  • Views 6698 views
  • Users 0 members are here
  • displays
  • model railroad
  • arduino projects
Related

Looking for a small display recommendation

colporteur
colporteur over 3 years ago

Does any member have a recommendation for a small display that is appropriate for scrolling from right to left?

After an hour culling the adafruit website with few returns, I have come to the E14 community hopefully to get a recommendation. I've been asked to build a two signs, one that scrolls "Welcome to Snow Island"  and the other "Thank you for Visiting Snow" Island. The signs will be positioned on top of a bridge on an HO scale model railroad layout.

I had hoped to use a MAX7219 Dot led Matrix MCU 8x32 but it is way to large for the foot print I have to work with. The bridge has a large flat surface about 4X4 inches to hold the sign.

Like any model railroad project cost is a factor. I don't have a big budget. I'm hoping to combine the display with an Nano Arduino to simulate a continuous text scrolling road sign to message visitors.

If your suggestions could contain the source for the part that would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +5
    Thank you for the input folks. Here are two displays I have ordered. If the displays on the left work it should be fairly simple to finish the project. Very little work on my part. The display on the right…
  • colporteur
    colporteur over 3 years ago in reply to colporteur +4
    community.element14.com/.../IMG_5F00_2289.MOV Do I buy or do I build? The S1144 (far left) displays arrived today. After installing the configuration software the display I wanted was working. At $10…
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave +3
    Just saw these, look quite nice, just under 3.7" wide, available in many colors, and very cheap! However they either work for the use-case, or don't, since the behaviour of them is only configurable…
  • charlieo21
    charlieo21 over 3 years ago

    Previously I worked with this one, it's really easy to use it. Adafruit FeatherWing OLED - 128x64 OLED Add-on For Feather [STEMMA QT / Qwiic] : ID 4650 : $14.95 : Adafruit Industries, Unique & fun DIY electronics and kits

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago

    4 X 4 is a tough nut to crack for alphanumerics, the aspect ratio doesnt fit the usual. Could a 1602 LCD do the job ?  https://www.amazon.com/NOYITO-Yellow-Green-Backlight-Interface-MEGA2560/dp/B07SZV1MK8/ref=sr_1_13?crid=73DPEGA7PT9Q&keywords=lcd+1602+module&qid=1677080223&sprefix=lcd+1602%2Caps%2C151&sr=8-13

     https://www.amazon.com/Qunqi-Serial-Backlight-Arduino-MEGA2560/dp/B01E4YUT3K/ref=sr_1_11?crid=2DZB5X1BBJQTT&keywords=iic+%2F+i2c+1602+blue+backlight+lcd+display+screen+module&qid=1677080327&sprefix=lcd+1602+module%2Caps%2C287&sr=8-11

    SSD1306 displays work well, but they are 1.3 inches square at best. There are some bigger TFT screens, but I hadnt worked with them to say how easy they are, and of course they start to get pricey as the size increases. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago

    I recommend a small OLED. Not sure if it supports scrolling though. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 3 years ago

    I suppose the question to ask yourself is, how small can the text font be before it becomes illegible.

    OLED's are small and the text font is tiny. As the text display crisp and clear it's fine for close viewing but at the distance it's not much use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 3 years ago

    I have used one like this before in an E14presents  project: https://export.farnell.com/midas/mdob128032gv-wi/oled-display-cob-128-x-32-pixel/dp/3407291?st=oled
    it works with adafruits GFX library. so scrolling should work. they are very wel lreadable. the only issue is you need to tinker around a bit with adressing the pixels, 0,0 is not where one expect them to be, that common for all midas oleds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago
    colporteur said:
    I had hoped to use a MAX7219 Dot led Matrix MCU 8x32 but it is way to large for the foot print I have to work with. The bridge has a large flat surface about 4X4 inches to hold the sign.

    How about a 4x4 assembly of these 0.1" pitch miniature LED matrix displays 

    https://www.adafruit.com/product/956

    which will give you just under 4" x 4" so enough for a filter and bezel to tidy it up.

    Drive them with your MAX7219

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago

    image

    Thanks for the response folks.

    Some of your offerings I have looked at and others didn't come up on my radar. I need to do some further research under the heading of EASY. I hoping to avoid investing countless hours in the build.

    In my head I have this idea of soldering some sockets to a breadboard to hold a Nano with a few connections to a display. Bang out some code and the message is flowing. I like the idea of building a shroud around the blue display but the 8X8 was what appealed to me in the beginning. I just don't think the screens would be long enough without adding at least six.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to colporteur

    I also had the thought that a really REALLY cool train marquee would be a persistence of Vision display like amgalbu built for  Santa Tracker , of course scaled down and use 8 normal LEDs packed together rather than programmable LEDs. 

    This is the HARD way  :-)  but for sure would be eye catching. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago

    There are low cost composite input monitors

    image

    But I have no clue how easy or reliably they would function with a raspberry pi...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to scottiebabe

    Using a Mini PAL/NTSC Display with a Raspberry Pi
    By Simon Monk

    https://learn.adafruit.com/using-a-mini-pal-ntsc-display-with-a-raspberry-pi/parts

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>