Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Coding with else{}...what are the cost benefits analysis?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 413 subscribers
  • Views 3928 views
  • Users 0 members are here
  • arduino_code
  • arduino
Related

Coding with else{}...what are the cost benefits analysis?

colporteur
colporteur over 3 years ago

if (digitalRead(ButtonPin) == LOW) {  //}

OR

if (digitalRead(ButtonPin) == HIGH) {  //
  return HIGH;
} else {  //}

I came across these two methods of testing a button. They both accomplish the same thing. 

Why would a coder use one over the other? What are advantages/disadvantages to using either?

I am a code resurrectionist not a programmer or coder. I usually cut and paste code parts to develop a working project. I have code that use both methods. I'm curious what falls into best practice? Does one provide better performance?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +4
    Hi Sean, There's not much difference, one might be a fraction faster or slower but it's negligible. It also depends on if the push-button is wired to ground or to the supply. Everyone does it in different…
  • javagoza
    javagoza over 3 years ago +4
    If it is a button I try not to read and compare the state in the if statement but to compare against a state variable of the button. In this way I can add logic to prevent button click bounces or have…
  • Fred27
    Fred27 over 3 years ago +4
    Code readability and maintainability will trump any minor performance differences in almost all cases. Make sure your code is easy to follow, debug, and extend and all will be good. Exactly what code…
Parents
  • colporteur
    colporteur over 3 years ago

    My understanding is by using the second conditional statement provides more flexibility. With the else, you provide the option to take action on both a HIGH and LOW value of the button. The first conditional statement doesn't provide that. 

    The Best practice for a coder would be to provide flexibility without causing overhead. By using the conditional statement with else the code is more flexible to expand. If never needed nothing lost.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to colporteur

    Those of us who are used to programming with object-oriented languages try to program without using conditional statements (if, case) to minimize branching. A conditional statement generates several paths and therefore when testing you have to test all those paths. This complicates the tests. In object-oriented programming, this is not your case, a good practice is to replace branching by polymorphism.

    See: https://www.refactoring.com/catalog/replaceConditionalWithPolymorphism.html

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to javagoza

    Interesting, that makes sense, but I find I have trouble keeping it pure like that. For example, how would you deal with an api call that returns a bird in json, wouldn’t you still need some way of iterating through the field names? And how do you go from a bird to a specific bird?

    I might need to take some refresher courses!

    Course, in Arduino it’s just a heck of a lot quicker to be messy Laughing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 3 years ago in reply to javagoza

    Interesting, that makes sense, but I find I have trouble keeping it pure like that. For example, how would you deal with an api call that returns a bird in json, wouldn’t you still need some way of iterating through the field names? And how do you go from a bird to a specific bird?

    I might need to take some refresher courses!

    Course, in Arduino it’s just a heck of a lot quicker to be messy Laughing