Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Coding with else{}...what are the cost benefits analysis?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 413 subscribers
  • Views 3916 views
  • Users 0 members are here
  • arduino_code
  • arduino
Related

Coding with else{}...what are the cost benefits analysis?

colporteur
colporteur over 3 years ago

if (digitalRead(ButtonPin) == LOW) {  //}

OR

if (digitalRead(ButtonPin) == HIGH) {  //
  return HIGH;
} else {  //}

I came across these two methods of testing a button. They both accomplish the same thing. 

Why would a coder use one over the other? What are advantages/disadvantages to using either?

I am a code resurrectionist not a programmer or coder. I usually cut and paste code parts to develop a working project. I have code that use both methods. I'm curious what falls into best practice? Does one provide better performance?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +4
    Hi Sean, There's not much difference, one might be a fraction faster or slower but it's negligible. It also depends on if the push-button is wired to ground or to the supply. Everyone does it in different…
  • javagoza
    javagoza over 3 years ago +4
    If it is a button I try not to read and compare the state in the if statement but to compare against a state variable of the button. In this way I can add logic to prevent button click bounces or have…
  • Fred27
    Fred27 over 3 years ago +4
    Code readability and maintainability will trump any minor performance differences in almost all cases. Make sure your code is easy to follow, debug, and extend and all will be good. Exactly what code…
Parents
  • Andrew J
    Andrew J over 3 years ago

    I came across a situation today which is essentially the reverse of what you have found: a ‘hanging’ if:

    if (aTestForTrue) [
       // do nothing
    else {
       some code;
       some more code;
       ...
    }

    I’ve seen this quite a few times and used it myself a few times, including today.  It’s done this way because the logic test is much clearer to write and understand than it’s inverse would be, and it’s a nod to the future where someone would have to maintain it.  It looks weird, and some purists and/or corporate standards would argue against it;  also, it’s unlikely the compiler would optimise his out as it isn’t as simple a case as the ‘hanging else’ would be.  But the code is more readable, speed of execution isn’t critical and the author (me) knows what they are doing!!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 3 years ago

    I came across a situation today which is essentially the reverse of what you have found: a ‘hanging’ if:

    if (aTestForTrue) [
       // do nothing
    else {
       some code;
       some more code;
       ...
    }

    I’ve seen this quite a few times and used it myself a few times, including today.  It’s done this way because the logic test is much clearer to write and understand than it’s inverse would be, and it’s a nod to the future where someone would have to maintain it.  It looks weird, and some purists and/or corporate standards would argue against it;  also, it’s unlikely the compiler would optimise his out as it isn’t as simple a case as the ‘hanging else’ would be.  But the code is more readable, speed of execution isn’t critical and the author (me) knows what they are doing!!