Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum What is your go to DC motor driver for Arduino projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 410 subscribers
  • Views 8667 views
  • Users 0 members are here
  • motor control
  • arduino
Related

What is your go to DC motor driver for Arduino projects

colporteur
colporteur over 3 years ago

My post  Raising the Bridge...Automation with Arduino: Failure reconciliation  details some of my failures with the L293N & L298N motor drivers.

Now I find myself looking for another DC motor driver. What DC motor driver do you use in Arduino projects? Why is it you motor driver of choice? Is there a Arduino library for the module or do you roll your own.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +3
    Another advantage of trying something new: Although I initially searched around for a reliable H-bridge to help colporteur it ended up helping me too. It turned out to make a nice little AC driver for…
  • shabaz
    shabaz over 3 years ago +2
    I don't know if I ever posted a photo of it, but that H450 driver (which was described here: Using H450 (Toshiba TB67H450) Motor Driver Boards with Arduino ) PCB arrived a while back. It appears to work…
  • shabaz
    shabaz over 3 years ago in reply to colporteur +2
    Hi Sean, The KiCad files, and the zip Arduino library file are here: https://github.com/shabaz123/h450 If you download that repository, then the KiCad project is in the motor_pcb folder. It is a KiCad…
Parents
  • rachna34
    rachna34 over 3 years ago

    I can suggest popular DC motor drivers often used in Arduino projects:

    1. L298N: This is a widely used dual H-bridge motor driver that can control two DC motors. It's affordable and works well for small to medium-sized projects.

    2. L293D: Another dual H-bridge motor driver that's compatible with Arduino. It's suitable for controlling two motors bidirectionally.

    3. Adafruit Motor Shield: This is a shield designed for Arduino boards that can control up to 4 DC motors or 2 stepper motors. It offers more advanced features and is great for larger projects.

    4. TB6612FNG: This is a compact and efficient motor driver that can control one DC motor or a stepper motor. It's a good choice for smaller projects with space constraints.

    5. DRV8833: A small and low-cost motor driver that can control one DC motor. It's suitable for basic motor control needs.

    Your choice of motor driver depends on your project's specific requirements, such as the number of motors you need to control, the power requirements, and any additional features you may need. Be sure to check compatibility with your Arduino board and the motor specifications before selecting a motor driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to rachna34

    LOL ChatGPT suggests the same as you:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • javagoza
    javagoza over 3 years ago in reply to rachna34

    LOL ChatGPT suggests the same as you: