Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Why does my Arduino switch Debounce routine bounce?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 411 subscribers
  • Views 6383 views
  • Users 0 members are here
  • arduino_code
  • arduino coding
  • arduino
Related

Why does my Arduino switch Debounce routine bounce?

colporteur
colporteur over 3 years ago

Why does the LED flash twice with one push and release of the button?

#include <Servo.h>

Servo Stop_servo;  // create servo object to control a servo

// Buttons with Pull-Ups are "backwards"
// Some DEFINEs to make reading code easier
#define PUSHED false
#define NOT_PUSHED true
#define WATCH_BUTTON true
#define IGNORE_BUTTON false

// Time to wait for bounce, in MICROsconds
const int buttonWaitInterval = 6000;
// Pins for LED and Button
const int LEDpin = 5;
const int BUTTONpin = 2;
float Minpos = 0;    // variable to store the servo position
float Maxpos = 255;  //greatest travel of servo

// Used to track how long between "bounces"
unsigned long previousMicros = 0;

// Used to track state of button (high or low)
boolean previousButtonState = NOT_PUSHED;

// Variable reporting de-bounced state.
boolean debouncedButtonState = NOT_PUSHED;

// Tracks if we are waiting for a "bounce" event
boolean bounceState = false;

// Nothing surprising here
void setup() {
  pinMode(LEDpin, OUTPUT);
  pinMode(BUTTONpin, INPUT_PULLUP);
  digitalWrite(LEDpin, LOW);
  Stop_servo.attach(3);  // attaches the servo on pin 3 to the servo object
  Stop_servo.write(0);

  Serial.begin(9600);
  Serial.println(F("Serial Initialized"));
}

void loop() {

  // This needs to be called periodically to
  // update the timers and button status
  updateButton();
  // This replaces: digitalRead(BUTTONpin);
  //digitalWrite(LEDpin, debouncedButtonState);
  if (debouncedButtonState == LOW) {
    digitalWrite(LEDpin, HIGH);
    delay(500);
    digitalWrite(LEDpin, LOW);
    delay(500);
    Stop_servo.write(255);
    delay(5000);
    Stop_servo.write(0);
    Serial.println(F("servo cycled"));
  }
}

// All of the magic happens here
void updateButton() {
  // We are waiting for any activity on the button
  if (bounceState == WATCH_BUTTON) {
    // Get and store current button state
    boolean currentButtonState = digitalRead(BUTTONpin);
    // Check to see if a transition has occured (and only one)
    if (previousButtonState != currentButtonState) {
      // A transition was detected, ignore the others for a while
      bounceState = IGNORE_BUTTON;
      // Store current time (start the clock)
      previousMicros = micros();
    }
    // Keep storing existing button state, if we're watching
    previousButtonState = currentButtonState;
  }
  // We are waiting for the buttonWaitInterval to elapse
  if (bounceState == IGNORE_BUTTON) {
    // Compare current value of micros to previously stored, enough time yet?
    unsigned long currentMicros = micros();
    if ((unsigned long)(currentMicros - previousMicros) >= buttonWaitInterval) {
      // Store the state of the button/pin to debouncedButtonState, which "reports"
      // the correct value. This allows for the code to handle active high or low inputs
      debouncedButtonState = digitalRead(BUTTONpin);
      // Go back to watching the button again.
      bounceState = WATCH_BUTTON;
    }
  }
}

I'm trying to use Baldengineer debounce code to read a button and take an action. Each press of the button causes the LED to flash twice. The serial output reflects the routine running twice. 

I have failed in my code changes to get the result I hope. I have looked at Internet and have found no hints to help.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago in reply to scottiebabe +4
    Technical forums are great, so many great tidbits of knowledge shared in this thread! One more demonstration showing why a schmitt trigger is an important part of the solution. I wrote a simple PIO…
  • dougw
    dougw over 3 years ago +3
    Debouncing may be good practice, but it would seem you don't need it here. If you start your LED and servo cycle as soon as a button push is first detected, all button bouncing will be long over before…
  • shabaz
    shabaz over 3 years ago +3
    Hi Sean, I've not looked in detail, but it seems that you wish to move a servo just once, if a button is pressed. Your delay() functions are actually already performing a button-pushed-down debounce…
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

     colporteur Hi, personally   I do not like soft debounce. I much prefer to get it over with a Schmitt Trigger (IC) you can use CD40106 (CMOS) or my favorite SN7414N, it is ubiquitous, and has many families.  you can look here for how it's done.  there is more info on this page:  if you wish to see the full article there is linked under one of the photos. This works ALL THE TIME, rain, snow whatever.. LOL

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to phoenixcomm

    Agree..

    The software debounce is now just moving the problem, especially because of the comment "controlled by a button some distance away from the Arduino Mega. The 26 gauge copper pair acts like an antenna for picking up noise".

    Now if a software debounce library is used, the question becomes, what sort of debounce to do in software? The debounce library can be configured with about 3 options, and not all will work if the issue is noise pickup (which is unrelated to button debounce).

    At some point, the issue needs to be understood, for the best configuration of code, regardless of whether a library is used or not. I too would have gone with hardware fix, although to augment the software debounce, i.e. an approach that uses both software and hardware.

    Also, one really needs to look at the code, and learn how the debounce works, and where and why it is needed, otherwise one will never move forward at learning how to marry up code to the underlying problem or task at hand,

    I sketched this, just as a discrete version. It can tolerate a lot of noise. The resistors could be about 2.2k ohm, for the collector one, and the base-to-emitter one could've 2.2k ohm too. Maybe 10 k ohm for the resistor connected to the switch. And a capacitor will help, maybe 100nF. This would all cost just $0.20 perhaps.

    image

    And for the logic IC version, I'd do the same as phoenixcomm recommends. A resistor can be added to prevent the input floating. This circuit expects the switch to be connected between positive supply and the Schmitt trigger input, but it could be rearranged if it's preferred to have the switch to ground.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to phoenixcomm

    Agree..

    The software debounce is now just moving the problem, especially because of the comment "controlled by a button some distance away from the Arduino Mega. The 26 gauge copper pair acts like an antenna for picking up noise".

    Now if a software debounce library is used, the question becomes, what sort of debounce to do in software? The debounce library can be configured with about 3 options, and not all will work if the issue is noise pickup (which is unrelated to button debounce).

    At some point, the issue needs to be understood, for the best configuration of code, regardless of whether a library is used or not. I too would have gone with hardware fix, although to augment the software debounce, i.e. an approach that uses both software and hardware.

    Also, one really needs to look at the code, and learn how the debounce works, and where and why it is needed, otherwise one will never move forward at learning how to marry up code to the underlying problem or task at hand,

    I sketched this, just as a discrete version. It can tolerate a lot of noise. The resistors could be about 2.2k ohm, for the collector one, and the base-to-emitter one could've 2.2k ohm too. Maybe 10 k ohm for the resistor connected to the switch. And a capacitor will help, maybe 100nF. This would all cost just $0.20 perhaps.

    image

    And for the logic IC version, I'd do the same as phoenixcomm recommends. A resistor can be added to prevent the input floating. This circuit expects the switch to be connected between positive supply and the Schmitt trigger input, but it could be rearranged if it's preferred to have the switch to ground.