Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino UNO R4 WiFi LED Demo
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 413 subscribers
  • Views 7469 views
  • Users 0 members are here
  • dougw
  • LED demo
  • arduino uno r4 wifi
Related

Arduino UNO R4 WiFi LED Demo

dougw
dougw over 3 years ago

element14 sent me an Arduino UNO R4 WiFi, which features a Renesas RA4M1 MCU. (Arm Cortex M4 48MHz).

This is a major upgrade over the original UNO. It is also a lot of fun to play with since it comes with a 12x8 LED matrix.

This is a quick demo of the LEDs in action...

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Thank you element14 for this excellent MCU module.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +7
    I think I posted this in the wrong area - I can't edit it. I worked out the graphics with a spreadsheet that shows the graphic as you enter ones in cells and computes the 32 bit hex numbers for the program…
  • javagoza
    javagoza over 3 years ago +2
    Great! You can also use the online LED matrix editor ledmatrix-editor.arduino.cc/
  • dougw
    dougw over 3 years ago in reply to robogary +2
    I didn't measure performance, although I had it scrolling so fast it was just a blur. This LED matrix is more capable than the micro:bit, the spacing also is tighter which makes the graphics more readable…
Parents
  • dougw
    dougw over 3 years ago

    Note - I have covered the LEDs with dark window tint film to hide the unlit LEDs.

    I also made a demo using the Arduino UNO R4 Minima which I received at the same time. That demo, linked here, is a much bigger display.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago

    Note - I have covered the LEDs with dark window tint film to hide the unlit LEDs.

    I also made a demo using the Arduino UNO R4 Minima which I received at the same time. That demo, linked here, is a much bigger display.