Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino UNO R4 WiFi LED Demo
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 413 subscribers
  • Views 7468 views
  • Users 0 members are here
  • dougw
  • LED demo
  • arduino uno r4 wifi
Related

Arduino UNO R4 WiFi LED Demo

dougw
dougw over 3 years ago

element14 sent me an Arduino UNO R4 WiFi, which features a Renesas RA4M1 MCU. (Arm Cortex M4 48MHz).

This is a major upgrade over the original UNO. It is also a lot of fun to play with since it comes with a 12x8 LED matrix.

This is a quick demo of the LEDs in action...

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Thank you element14 for this excellent MCU module.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +7
    I think I posted this in the wrong area - I can't edit it. I worked out the graphics with a spreadsheet that shows the graphic as you enter ones in cells and computes the 32 bit hex numbers for the program…
  • javagoza
    javagoza over 3 years ago +2
    Great! You can also use the online LED matrix editor ledmatrix-editor.arduino.cc/
  • dougw
    dougw over 3 years ago in reply to robogary +2
    I didn't measure performance, although I had it scrolling so fast it was just a blur. This LED matrix is more capable than the micro:bit, the spacing also is tighter which makes the graphics more readable…
  • dougw
    dougw over 3 years ago in reply to robogary

    I didn't measure performance, although I had it scrolling so fast it was just a blur. This LED matrix is more capable than the micro:bit, the spacing also is tighter which makes the graphics more readable. And I got the LEDs to be viewable by my camera - the micro:bit multiplexing makes that display tough to video.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to cstanton

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    Note - I have covered the LEDs with dark window tint film to hide the unlit LEDs.

    I also made a demo using the Arduino UNO R4 Minima which I received at the same time. That demo, linked here, is a much bigger display.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    Thank you for posting this, dougw .Mine arrived a few days ago but I haven't made the time to fire it up yet.  I'm excited to give it a whirl.  I love Arduinos.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • navadeepganeshu
    navadeepganeshu over 3 years ago

    Great! Thanks for sharing about this. I was looking at the features of this board and a comparison table of memory, RAM and peripherals with an earlier UNO version - just amazing.

    Renesas somehow has a very good MCU product line and application specific veraints in a family all at a relatively lower pricepoint.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 3 years ago

    Nice, I look forward to seeing you put it to use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 3 years ago in reply to dougw

    We had to use this approach when we were putting text and symbols on displays in the 1980's.

    You still have to understand the bits and bytes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bidrohini
    bidrohini over 3 years ago in reply to cstanton

    Thank you so much. I am confused about which one will be more convenient. Wifi or Minima?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to bidrohini

    if you just want an mcu board, go minima, if wifi and the matrix are features you need go wifi, I got both, so I can use whatever feels apropriate depending on  the project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<