Arduino
  • Products
  • More
Arduino
Arduino Forum Need help building a jet turbine sound module.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 409 subscribers
  • Views 4186 views
  • Users 0 members are here
Related

Need help building a jet turbine sound module.

akashthakur0305
akashthakur0305 over 2 years ago

Hi All,
I've been trying to make a Jet engine sound module,
I want to 3d print a turbine model and have a potentiometer control the turbine startup/ spooling up/ spooling down / shutdown sound.
Can't seem to find any Arduino code for playing these sounds.
Either on the board or on a MP3 module.

youtu.be/xpAWZPsR82E

I found a old video on YouTube, no tutorials though,
Can anyone help.


Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 2 years ago +3
    JQ6500 MP3 Player the sequel I use a JQ6500 sound module with my Arduino projects for sound. You can load the JQ6500 with up to 2M of mp3 and play them individually. The module can be used standalone…
  • rsc
    rsc over 2 years ago +2
    Do a search for RC jet engine sound module and you'll find several devices that you can operate using a PWM channel from the arduino.
  • phoenixcomm
    phoenixcomm over 2 years ago +2 suggested
    akashthakur0305 Ok, I bite, first a sound file is sort of universal. I was a crew chief in the USAF, and when you started you thing it sounded terrible. I suggest, that you don't mess about and print the…
  • akashthakur0305
    0 akashthakur0305 over 2 years ago in reply to fskrzycki

    Hi,

    This is not for a RC plane,

    Im 3d printing a turbojet engine model which I can keep on my desktop,

    Printing the file is easy, making a motor run the turbine with a potentiometer is also figured out,

    But it would be cool if there was background noise of the engine starting up and spooling up along with the turning turbine,

    Controlled with the same potentiometer.

    There are RC engine simulators with esp32 and Arduino, but I can't sleep to modify them for my use, plus they are a little complicated as people have integrated turn signals,headlights and stuff.

    Regards 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fskrzycki
    0 fskrzycki over 2 years ago in reply to akashthakur0305

    If all you want is the turbine spinning why not use a simple circuit with a small electric engine? You can connect the potentiometer to the power supply. I don't see the need to even use a program.. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 1 year ago

    Check out the audio section in this project - it simplifies triggering arbitrary sound files:

    (+) The Proverbial Black Box - element14 Community

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 1 year ago in reply to dougw

    I think they may be after seamless looping of a section of a sound file based upon the current position of the potentiometer.

    increase from 0% to 10%
    hold at 10% percent
    increase from 10% to 50%
    hold at 50%
    decrease from 50% to 25%
    hold at 25%

    Perhaps need two recordings - one for increasing speed and one for reducing, synchronised to RPM. Use the left and right channel in one stereo file perhaps so when changing direction cross fade to the other channel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<