Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino IDE 2.3.3 hangs when trying to download boards package_index.json
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 411 subscribers
  • Views 7302 views
  • Users 0 members are here
  • arduino ide
  • serial monitor interaction
  • package_index.json download
Related

Arduino IDE 2.3.3 hangs when trying to download boards package_index.json

ralphjy
ralphjy over 1 year ago

I just ran into an unexpected issue when I was trying to update code for a project.  When I had previously closed the IDE yesterday I had the Serial Monitor open.  Today when I opened the code in a fresh instance of the IDE it got stuck trying to download the first package_index.json that I have in my Additional Boards Manager URLs.

I discovered that it is possibly a known issue with the IDE - Exceptionally long duration of "Downloading index: ....  What fixed it for me was closing the Serial Monitor and reopening it after the IDE finished startup.  I am using IDE version 2.3.3 and there isn't any released update available so I guess the problem is not fixed yet.

Just thought I'd mention it here as it surprised me because I hadn't updated either the code or IDE and would never have expected an interaction with the Serial Monitor.  Maybe I'll just remember to close it when I shutdown.

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 1 year ago +1
    I've been experiencing the same problem for the past two weeks working with Espressif boards, the only solution that works for me is reinstalling the ESP32 board package. I've already read about closing…
  • ralphjy
    ralphjy over 1 year ago in reply to javagoza +1
    I don't update the IDE that frequently so I don't know when this issue started (it appears that it might have been 2.3.x). I'm glad that the workaround didn't require downgrading the IDE version. I have…
Parents
  • bidrohini
    bidrohini over 1 year ago

    It will be worth keeping an eye on release notes or bug reports for future updates of Arduino IDE to see if they address this specific issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bidrohini
    bidrohini over 1 year ago

    It will be worth keeping an eye on release notes or bug reports for future updates of Arduino IDE to see if they address this specific issue.