Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Can Someone Review my Schematic for Android GPIO?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 410 subscribers
  • Views 2074 views
  • Users 0 members are here
  • android
  • arduino nano
  • mcp2200
  • arduino
Related

Can Someone Review my Schematic for Android GPIO?

mjones517
mjones517 over 1 year ago

Okay, so I want to access Arduino GPIO pins via Android. My plan is to access them via a serial connection using an MCP2200. I can read / write to the serial port on Android, which can then interact with the Arduino.

The problem is I also want to be able to plug in the phone and have it charging while still being able to access the Arduino. I came up with this, but am pretty new to the electronics side of things and want to avoid blowing things up. Will this do what I want?

It's essentially two USB ports. One goes to the charger, the other to the phone. The Arduino and MCP2200 sit in the middle.

image

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 1 year ago +2
    Short answer is: No this will not work in the current form. Long answer: The basics: Connect all GND pins on both USB connectors, Arduino+ VSS and a schematic GND symbol Connect all VBUS on both…
  • shabaz
    shabaz over 1 year ago +2
    Hi, I agree with everything Wolfgang mentioned. If you want to make life easier, it is possible for a few $ to obtain a ready-made USB OTG cable with extra port for charging. It will contain the electronics…
  • wolfgangfriedrich
    wolfgangfriedrich over 1 year ago in reply to mjones517 +2
    I agree with everything shabaz mentioned. But if you want to go the fun route and design your own solution,here we go. Even as a USB device you need the 12 MHz crystal. The chip needs some sort of…
Parents
  • mjones517
    0 mjones517 over 1 year ago

    Today was interesting and I've learned some stuff.

    I decided step 1 was just getting the MCP2200 to register as a serial device. I could not get this to work for the life of me, not even on my laptop. I suspect wolfgangfriedrich is correct and I need to add the 12 Mhz crystal. I don't have one, so I can't test for sure.

    Out of frustration I plugged my Arduino directly into my Pixel 6 and opened a serial monitor app. I was able to directly connect, no intermediate chip required. I even got an LED to turn on / off.

    I think the solution I'm going to take is to do that and also buy the USB OTG cable shabaz suggested. That will accomplish everything I need to make this project work.

    My last project used a Raspberry Pi. I realized at the end the only thing I needed the Pi for was GPIO, and that the rest of the project would have been cheaper / easier if I could have just used an Android tablet. Now that I know I can control an Arduino using serial commands, I can skip the bloodbath of trying to find / use a Pi.

    Thanks again for everyone's help! As you've figured out I'm a raw newbie.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mjones517
    0 mjones517 over 1 year ago

    Today was interesting and I've learned some stuff.

    I decided step 1 was just getting the MCP2200 to register as a serial device. I could not get this to work for the life of me, not even on my laptop. I suspect wolfgangfriedrich is correct and I need to add the 12 Mhz crystal. I don't have one, so I can't test for sure.

    Out of frustration I plugged my Arduino directly into my Pixel 6 and opened a serial monitor app. I was able to directly connect, no intermediate chip required. I even got an LED to turn on / off.

    I think the solution I'm going to take is to do that and also buy the USB OTG cable shabaz suggested. That will accomplish everything I need to make this project work.

    My last project used a Raspberry Pi. I realized at the end the only thing I needed the Pi for was GPIO, and that the rest of the project would have been cheaper / easier if I could have just used an Android tablet. Now that I know I can control an Arduino using serial commands, I can skip the bloodbath of trying to find / use a Pi.

    Thanks again for everyone's help! As you've figured out I'm a raw newbie.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • wolfgangfriedrich
    0 wolfgangfriedrich over 1 year ago in reply to mjones517

    Thanks for reporting back, mjones517 . Awesome to hear that you found a solution, that is even more elegant than what we have suggested to you. Getting to blinky is always a huge step. You are less of a newbie now, the bag of experience is filling up. Well done.

    Good luck with your project.