Arduino Forum X-BEE module
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
  • Replies 5 replies
  • Subscribers 394 subscribers
  • Views 523 views
  • Users 0 members are here
  • arduino:
  • arduino rf
  • diy
  • arduino
Related

X-BEE module

Former Member
Former Member over 9 years ago

Hello,

 

I want to use the x-bee  for wireless serial comm. between two arduinos. How do i configure the X-bee modules.

Also, what are the possible uses of the X-bee. I am a beginner and do not have enough experience with wireless comm. How does the X-Bee work??

 

if i configure the X bee modules for just wireless serial comm, will i be able to send data wirelessly to the other device. will it work just like it would have worked, if the system was wired?.

 

 

reply would be greatly appreciated.

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2
    Hi Anshuman, I do not know if it will be of help but Jeremy Blum in his great book "Exploring Arduino" ISBN: 978-1-118-54936-0 devotes the entire chapter 11 to Wireless Communication with X-Bee Radios…
  • shabaz
    shabaz over 9 years ago +1
    We had this question about a week ago. The answer is no, they won't work the same. You need to check the datasheets for the various xbee models, they are all different. But, in general, if there is no…
  • tonyboubady
    tonyboubady over 9 years ago +1
    Get this 2.5GHz wireless transceiver called nrf24l01, it's inexpensive, easy to use to start with wireless communication, loads of tutorials on web, you can connect 2 microcontrollers wirelessly which…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Anshuman,

    I do not know if it will be of help but Jeremy Blum in his great book "Exploring Arduino" ISBN: 978-1-118-54936-0 devotes the entire chapter 11 to Wireless Communication with X-Bee Radios. You can google the book and check out the sub-listings in chapter 11 to see if any of the topics would answer your needs.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 9 years ago in reply to jw0752

    This is another nice book on wireless transmission using xbee.  Building Wireless Sensor Networks: with ZigBee, XBee, Arduino, and Processing: Robert Faludi: 9780596807733: Amazon.com:…

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Nate1616
    Nate1616 over 9 years ago in reply to jw0752

    This is another nice book on wireless transmission using xbee.  Building Wireless Sensor Networks: with ZigBee, XBee, Arduino, and Processing: Robert Faludi: 9780596807733: Amazon.com:…

     

    Nate