Arduino Forum Sensor
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
  • Replies 8 replies
  • Subscribers 393 subscribers
  • Views 653 views
  • Users 0 members are here
Related

Sensor

Former Member
Former Member over 9 years ago

I would like to ask if there are any sensors that I could use in detecting the level of powder in a case while reloading. The only thing I can find commercially only tell you when a case is empty or over full. I want to know if it has a level between those two.

1. the level I want

2. anything short of that level

3. anything above that level.

 

any advice would be great thanks

Keith

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago +1
    Traditionally the most accurate linear position sensor is an LVDT (linear variable differential transducer) but they can be expensive. A linear potentiometer is a pretty good low-cost alternative. Maybe…
Parents
  • shabaz
    shabaz over 9 years ago

    Hi Keith,

     

    If you scroll down to the section titled Linear Travel on this page: Keysight U1282A Vehicle/Automotive and Industrial Applications

    you'll see a sensor that can resolve to about a millimetre or better. It is like a plunger without a spring (a spring could be added with some modification). The shaft is light, doesn't need much force. The end is a screw thread, perhaps it could be fitted to something the diameter of the case you refer to.

    It's just an idea, I don't really know if it is suitable or not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 9 years ago

    Hi Keith,

     

    If you scroll down to the section titled Linear Travel on this page: Keysight U1282A Vehicle/Automotive and Industrial Applications

    you'll see a sensor that can resolve to about a millimetre or better. It is like a plunger without a spring (a spring could be added with some modification). The shaft is light, doesn't need much force. The end is a screw thread, perhaps it could be fitted to something the diameter of the case you refer to.

    It's just an idea, I don't really know if it is suitable or not.